<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX93 DSI: failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX93-DSI-failed-to-attach-bridge-soc-0-dsi-4ae10000-to-encoder/m-p/2001564#M231187</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;You're encountering (failed to attach bridge: -517) typically indicates that a required component or dependency is not ready during the device initialization process. This is often related to probe order issues in the Linux kernel device tree or missing configurations.&lt;/P&gt;&lt;P&gt;-517 corresponds to -EPROBE_DEFER, which indicates that the kernel driver is deferring its initialization because a dependency (e.g., another device or resource) is not ready.&lt;BR /&gt;The common reasons for this error include:&lt;BR /&gt;Missing or incorrect configuration in the device tree.&lt;BR /&gt;Drivers for dependent components are not loaded or initialized in the correct order.&lt;/P&gt;&lt;P&gt;Ensure that the panel and dsi nodes are correctly defined and match the bindings expected by the driver. Based on your device tree examples:&lt;BR /&gt;Confirm that the compatible strings ("startek,kd050fwfia019" and "ili9806e") match those in the kernel drivers.&lt;BR /&gt;Validate that the reset-gpios, vdd-supply, and vccio-supply properties are correctly defined and available.&lt;/P&gt;&lt;P&gt;Confirm that the dw-mipi-dsi and ili9806e drivers are being initialized in the correct order. Use dmesg to check for related logs:&amp;nbsp;dmesg | grep -i dsi&amp;nbsp;If the panel driver (panel-ilitek-ili9806e.c) is being probed before the DSI controller is ready, you may need to ensure the controller initializes earlier.&amp;nbsp;Move the panel node to be a sub-node of the dsi controller node. This ensures that the panel is registered as part of the DSI controller's initialization.&amp;nbsp;The panel-ilitek-ili9806e.c file should contain a valid initialization sequence for the ili9806e panel. Double-check the init_sequence function in your driver for any missing steps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Enable debug logs for DRM and DSI:&lt;/P&gt;&lt;P&gt;Add the following kernel parameters:&amp;nbsp;&lt;/P&gt;&lt;P&gt;drm.debug=0x1f&lt;/P&gt;&lt;P&gt;This provides detailed information about DRM and DSI initialization.&lt;BR /&gt;Use these logs to identify whether the panel or DSI controller is failing to probe.&lt;/P&gt;&lt;P&gt;Ensure that the regulators (vdd and vccio) and GPIOs are defined and active.&lt;BR /&gt;Verify that the backlight node is properly defined and linked in the device tree.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are still encountering issues, consider checking the driver documentation or&amp;nbsp;&lt;FONT size="1 2 3 4 5 6 7" color="#FFFFFF"&gt;&lt;A href="https://www.ingresosolidario.com.co" target="_self"&gt;consultar ingreso solidario&lt;/A&gt;&lt;/FONT&gt; similar device examples in the kernel source.&amp;nbsp;You can also try using CONFIG_DRM_PANEL_SIMPLE as a temporary panel driver for basic testing.&lt;BR /&gt;loglevel=8&lt;/P&gt;</description>
    <pubDate>Tue, 26 Nov 2024 03:54:00 GMT</pubDate>
    <dc:creator>harold07douglas</dc:creator>
    <dc:date>2024-11-26T03:54:00Z</dc:date>
    <item>
      <title>IMX93 DSI: failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX93-DSI-failed-to-attach-bridge-soc-0-dsi-4ae10000-to-encoder/m-p/1999957#M231110</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I'm working on IMX93 board with mipi screen named "&lt;/SPAN&gt;&lt;SPAN&gt;startek,kd050fwfia019" driven by "ili9806e"&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;for a while, and still stucked.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;There is no display output while encountering the following message from booting up.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[    2.089408] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[    2.097386] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517
[    2.107483] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517
[    2.117351] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried two cases of kernel divice tree, both end up with the same error mentioned above.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;test case 1 ：&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;&amp;amp;dsi {
	status = "okay";

	panel@0 {
		compatible = "startek,kd050fwfia019";
		pinctrl-names = "default";
		pinctrl-0 = &amp;lt;&amp;amp;pinctrl_panel0_gpios&amp;gt;;
	  	vdd-supply = &amp;lt;&amp;amp;reg_vdd_3v3&amp;gt;;
	 	vccio-supply = &amp;lt;&amp;amp;reg_vddio_1v8&amp;gt;;
        reset-gpios = &amp;lt;&amp;amp;gpio2 16 GPIO_ACTIVE_LOW&amp;gt;;
		backlight = &amp;lt;&amp;amp;dsi_backlight&amp;gt;;
		rotation = &amp;lt;90&amp;gt;;
		status = "okay";

		port {
			panel_in: endpoint {
				remote-endpoint = &amp;lt;&amp;amp;dsi_out&amp;gt;;
			};
		};
	};

	ports{
 		#address-cells = &amp;lt;1&amp;gt;;
 		#size-cells = &amp;lt;0&amp;gt;;

		port@1 {
			reg = &amp;lt;1&amp;gt;;

			dsi_out: endpoint {
				remote-endpoint = &amp;lt;&amp;amp;panel_in&amp;gt;;
			};
		};
	};
};&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;test case 2：&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;/ {
        dsi_panel {
		compatible = "startek,kd050fwfia019";
		pinctrl-names = "default";
		pinctrl-0 = &amp;lt;&amp;amp;pinctrl_panel0_gpios&amp;gt;;
	  	vdd-supply = &amp;lt;&amp;amp;reg_vdd_3v3&amp;gt;;
	 	vccio-supply = &amp;lt;&amp;amp;reg_vddio_1v8&amp;gt;;
        reset-gpios = &amp;lt;&amp;amp;gpio2 16 GPIO_ACTIVE_LOW&amp;gt;;
		backlight = &amp;lt;&amp;amp;dsi_backlight&amp;gt;;
		rotation = &amp;lt;90&amp;gt;;
		status = "okay";

		port {
			panel_in: endpoint {
				remote-endpoint = &amp;lt;&amp;amp;dsi_out&amp;gt;;
			};
		};
	};
};

&amp;amp;dsi {
	status = "okay";

	ports{
 		#address-cells = &amp;lt;1&amp;gt;;
 		#size-cells = &amp;lt;0&amp;gt;;

		port@1 {
			reg = &amp;lt;1&amp;gt;;

			dsi_out: endpoint {
				remote-endpoint = &amp;lt;&amp;amp;panel_in&amp;gt;;
			};
		};
	};
};&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;panel-ilitek-ili9806e.c ：&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;// SPDX-License-Identifier: GPL-2.0

#include &amp;lt;linux/delay.h&amp;gt;
#include &amp;lt;linux/device.h&amp;gt;
#include &amp;lt;linux/err.h&amp;gt;
#include &amp;lt;linux/errno.h&amp;gt;
#include &amp;lt;linux/gpio/consumer.h&amp;gt;
#include &amp;lt;linux/kernel.h&amp;gt;
#include &amp;lt;linux/mod_devicetable.h&amp;gt;
#include &amp;lt;linux/module.h&amp;gt;
#include &amp;lt;linux/property.h&amp;gt;
#include &amp;lt;linux/regulator/consumer.h&amp;gt;

#include &amp;lt;drm/drm_mipi_dsi.h&amp;gt;
#include &amp;lt;drm/drm_modes.h&amp;gt;
#include &amp;lt;drm/drm_panel.h&amp;gt;
#include &amp;lt;drm/drm_probe_helper.h&amp;gt;

#include &amp;lt;video/mipi_display.h&amp;gt;

struct ili9806e_panel;

struct panel_desc {
	const struct drm_display_mode *display_mode;
	unsigned long mode_flags;
	enum mipi_dsi_pixel_format format;
	unsigned int lanes;
	int (*init_sequence)(struct ili9806e_panel *ctx);
};

struct ili9806e_panel {
	struct drm_panel panel;
	struct mipi_dsi_device *dsi;
	struct gpio_desc *reset_gpio;
	struct regulator_bulk_data supplies[2];
	const struct panel_desc *desc;
	enum drm_panel_orientation orientation;
};

static const char * const regulator_names[] = {
	"vdd",
	"vccio",
};

static inline struct ili9806e_panel *to_ili9806e_panel(struct drm_panel *panel)
{
	return container_of(panel, struct ili9806e_panel, panel);
}

static int ili9806e_power_on(struct ili9806e_panel *ctx)
{
	struct mipi_dsi_device *dsi = ctx-&amp;gt;dsi;
	int ret;

	gpiod_set_value(ctx-&amp;gt;reset_gpio, 1);

	ret = regulator_bulk_enable(ARRAY_SIZE(ctx-&amp;gt;supplies), ctx-&amp;gt;supplies);
	if (ret &amp;lt; 0) {
		dev_err(&amp;amp;dsi-&amp;gt;dev, "regulator bulk enable failed: %d\n", ret);
		return ret;
	}

	usleep_range(10000, 20000);
	gpiod_set_value(ctx-&amp;gt;reset_gpio, 0);
	usleep_range(10000, 20000);

	return 0;
}

static int ili9806e_power_off(struct ili9806e_panel *ctx)
{
	struct mipi_dsi_device *dsi = ctx-&amp;gt;dsi;
	int ret;

	gpiod_set_value(ctx-&amp;gt;reset_gpio, 1);

	ret = regulator_bulk_disable(ARRAY_SIZE(ctx-&amp;gt;supplies), ctx-&amp;gt;supplies);
	if (ret)
		dev_err(&amp;amp;dsi-&amp;gt;dev, "regulator bulk disable failed: %d\n", ret);

	return ret;
}

static int ili9806e_on(struct ili9806e_panel *ctx)
{
    int ret = 0;
	if (ctx-&amp;gt;desc-&amp;gt;init_sequence) {
		ret = ctx-&amp;gt;desc-&amp;gt;init_sequence(ctx);
    }

    if (ret != 0) {
        return ret;
    }

	return mipi_dsi_dcs_exit_sleep_mode(ctx-&amp;gt;dsi);
}

static int ili9806e_enable(struct drm_panel *panel)
{
	struct ili9806e_panel *ctx = to_ili9806e_panel(panel);

	usleep_range(100000, 120000);

	return mipi_dsi_dcs_set_display_on(ctx-&amp;gt;dsi);
}

static int ili9806e_off(struct ili9806e_panel *ctx)
{
	return mipi_dsi_dcs_enter_sleep_mode(ctx-&amp;gt;dsi);
}

static int ili9806e_disable(struct drm_panel *panel)
{
	struct ili9806e_panel *ctx = to_ili9806e_panel(panel);

	return mipi_dsi_dcs_set_display_off(ctx-&amp;gt;dsi);
}

static int ili9806e_prepare(struct drm_panel *panel)
{
	struct ili9806e_panel *ctx = to_ili9806e_panel(panel);
	int ret;

	ret = ili9806e_power_on(ctx);
	if (ret &amp;lt; 0)
		return ret;

	ret = ili9806e_on(ctx);
	if (ret &amp;lt; 0) {
		ili9806e_power_off(ctx);
		return ret;
	}

	return 0;
}

static int ili9806e_unprepare(struct drm_panel *panel)
{
	struct ili9806e_panel *ctx = to_ili9806e_panel(panel);
	struct mipi_dsi_device *dsi = ctx-&amp;gt;dsi;
	int ret;

	ili9806e_off(ctx);

	ret = ili9806e_power_off(ctx);
	if (ret &amp;lt; 0)
		dev_err(&amp;amp;dsi-&amp;gt;dev, "power off failed: %d\n", ret);

	return ret;
}

static int ili9806e_get_modes(struct drm_panel *panel,
			      struct drm_connector *connector)
{
	struct ili9806e_panel *ctx = to_ili9806e_panel(panel);
	const struct drm_display_mode *mode = ctx-&amp;gt;desc-&amp;gt;display_mode;

	return drm_connector_helper_get_modes_fixed(connector, mode);
}

static enum drm_panel_orientation ili9806e_get_orientation(struct drm_panel *panel)
{
	struct ili9806e_panel *ctx = to_ili9806e_panel(panel);

	return ctx-&amp;gt;orientation;
}

static const struct drm_panel_funcs ili9806e_funcs = {
	.prepare = ili9806e_prepare,
	.unprepare = ili9806e_unprepare,
    .enable = ili9806e_enable,
    .disable = ili9806e_disable,
	.get_modes = ili9806e_get_modes,
	.get_orientation = ili9806e_get_orientation,
};

static int ili9806e_dsi_probe(struct mipi_dsi_device *dsi)
{
	struct device *dev = &amp;amp;dsi-&amp;gt;dev;
	struct ili9806e_panel *ctx;
	int i, ret;

	ctx = devm_kzalloc(dev, sizeof(*ctx), GFP_KERNEL);
	if (!ctx)
		return -ENOMEM;

	ctx-&amp;gt;desc = device_get_match_data(dev);

	for (i = 0; i &amp;lt; ARRAY_SIZE(ctx-&amp;gt;supplies); i++)
		ctx-&amp;gt;supplies[i].supply = regulator_names[i];

	ret = devm_regulator_bulk_get(dev, ARRAY_SIZE(ctx-&amp;gt;supplies),
				      ctx-&amp;gt;supplies);
	if (ret &amp;lt; 0)
		return ret;

	ctx-&amp;gt;reset_gpio = devm_gpiod_get(dev, "reset", GPIOD_OUT_LOW);
	if (IS_ERR(ctx-&amp;gt;reset_gpio))
		return dev_err_probe(dev, PTR_ERR(ctx-&amp;gt;reset_gpio),
				     "Failed to get reset-gpios\n");

	mipi_dsi_set_drvdata(dsi, ctx);
	ctx-&amp;gt;dsi = dsi;

	dsi-&amp;gt;mode_flags = ctx-&amp;gt;desc-&amp;gt;mode_flags;
	dsi-&amp;gt;format = ctx-&amp;gt;desc-&amp;gt;format;
	dsi-&amp;gt;lanes = ctx-&amp;gt;desc-&amp;gt;lanes;

	drm_panel_init(&amp;amp;ctx-&amp;gt;panel, dev, &amp;amp;ili9806e_funcs,
		       DRM_MODE_CONNECTOR_DSI);

	ret = of_drm_get_panel_orientation(dev-&amp;gt;of_node, &amp;amp;ctx-&amp;gt;orientation);
	if (ret)
		return dev_err_probe(dev, ret, "Failed to get orientation\n");

	ret = drm_panel_of_backlight(&amp;amp;ctx-&amp;gt;panel);
	if (ret)
		return dev_err_probe(dev, ret, "Failed to get backlight\n");

	drm_panel_add(&amp;amp;ctx-&amp;gt;panel);

	ret = mipi_dsi_attach(dsi);
	if (ret &amp;lt; 0) {
		dev_err_probe(dev, ret, "Failed to attach to DSI host\n");
		drm_panel_remove(&amp;amp;ctx-&amp;gt;panel);
		return ret;
	}

	return 0;
}

static void ili9806e_dsi_remove(struct mipi_dsi_device *dsi)
{
	struct ili9806e_panel *ctx = mipi_dsi_get_drvdata(dsi);

	mipi_dsi_detach(dsi);
	drm_panel_remove(&amp;amp;ctx-&amp;gt;panel);
}

static int ili9806e_switch_page(struct ili9806e_panel *ctx, u8 page)
{
	u8 buf[7] = { 0xff, 0xff, 0x98, 0x81, 0x06, 0x04, page };
	int ret;

	ret = mipi_dsi_dcs_write_buffer(ctx-&amp;gt;dsi, buf, sizeof(buf));
	if (ret &amp;lt; 0)
		return ret;

	return 0;
}

static int ili9806e_send_cmd_data(struct ili9806e_panel *ctx, u8 cmd, u8 data)
{
	u8 buf[2] = { cmd, data };
	int ret;

	ret = mipi_dsi_dcs_write_buffer(ctx-&amp;gt;dsi, buf, sizeof(buf));
	if (ret &amp;lt; 0)
		return ret;

	return 0;
}

static int ili9806e_send_cmd(struct ili9806e_panel *ctx, u8 cmd)
{
	u8 buf[1] = { cmd };
	int ret;

	ret = mipi_dsi_dcs_write_buffer(ctx-&amp;gt;dsi, buf, sizeof(buf));
	if (ret &amp;lt; 0)
		return ret;

	return 0;
}

static int kd050fwfia019_init(struct ili9806e_panel *ctx)
{
    // Change to Page 1
    ili9806e_switch_page(ctx, 0x01);
    //Output    SDA
    ili9806e_send_cmd_data(ctx, 0x08, 0x10);
    //set DE/VSYNC mode
    ili9806e_send_cmd_data(ctx, 0x20, 0x00);
    //DE = 1 Active
    ili9806e_send_cmd_data(ctx, 0x21, 0x01);
    //Resolution setting 480 X 854
    ili9806e_send_cmd_data(ctx, 0x30, 0x01);
    //Inversion setting 2-dot
    ili9806e_send_cmd_data(ctx, 0x31, 0x00);
    //BT  AVDD,AVDD
    ili9806e_send_cmd_data(ctx, 0x40, 0x16);
    //22
    ili9806e_send_cmd_data(ctx, 0x41, 0x33);
    //VGL=DDVDH+VCIP -DDVDL,VGH=2DDVDL-VCIP
    ili9806e_send_cmd_data(ctx, 0x42, 0x03);
    //SET VGH clamp level
    ili9806e_send_cmd_data(ctx, 0x43, 0x09);
    //SET VGL clamp level
    ili9806e_send_cmd_data(ctx, 0x44, 0x06);
    //VREG1
    ili9806e_send_cmd_data(ctx, 0x50, 0x88);
    //VREG2
    ili9806e_send_cmd_data(ctx, 0x51, 0x88);
    //Flicker MSB
    ili9806e_send_cmd_data(ctx, 0x52, 0x00);
    //Flicker LSB
    ili9806e_send_cmd_data(ctx, 0x53, 0x49);
    //Flicker
    ili9806e_send_cmd_data(ctx, 0x55, 0x49);

    ili9806e_send_cmd_data(ctx, 0x60, 0x07);
    ili9806e_send_cmd_data(ctx, 0x61, 0x00);
    ili9806e_send_cmd_data(ctx, 0x62, 0x07);
    ili9806e_send_cmd_data(ctx, 0x63, 0x00);

    //++++++++++++++++++ Gamma Setting ++++++++++++++++++//
    //Positive Gamma
    ili9806e_send_cmd_data(ctx, 0xA0, 0x00);
    ili9806e_send_cmd_data(ctx, 0xA1, 0x09);
    ili9806e_send_cmd_data(ctx, 0xA2, 0x11);
    ili9806e_send_cmd_data(ctx, 0xA3, 0x0B);
    ili9806e_send_cmd_data(ctx, 0xA4, 0x05);
    ili9806e_send_cmd_data(ctx, 0xA5, 0x08);
    ili9806e_send_cmd_data(ctx, 0xA6, 0x06);
    ili9806e_send_cmd_data(ctx, 0xA7, 0x04);
    ili9806e_send_cmd_data(ctx, 0xA8, 0x09);
    ili9806e_send_cmd_data(ctx, 0xA9, 0x0C);
    ili9806e_send_cmd_data(ctx, 0xAA, 0x15);
    ili9806e_send_cmd_data(ctx, 0xAB, 0x08);
    ili9806e_send_cmd_data(ctx, 0xAC, 0x0F);
    ili9806e_send_cmd_data(ctx, 0xAD, 0x12);
    ili9806e_send_cmd_data(ctx, 0xAE, 0x09);
    ili9806e_send_cmd_data(ctx, 0xAF, 0x00);
    //Negative Gamma
    ili9806e_send_cmd_data(ctx, 0xC0, 0x00);
    ili9806e_send_cmd_data(ctx, 0xC1, 0x09);
    ili9806e_send_cmd_data(ctx, 0xC2, 0x10);
    ili9806e_send_cmd_data(ctx, 0xC3, 0x0C);
    ili9806e_send_cmd_data(ctx, 0xC4, 0x05);
    ili9806e_send_cmd_data(ctx, 0xC5, 0x08);
    ili9806e_send_cmd_data(ctx, 0xC6, 0x06);
    ili9806e_send_cmd_data(ctx, 0xC7, 0x04);
    ili9806e_send_cmd_data(ctx, 0xC8, 0x08);
    ili9806e_send_cmd_data(ctx, 0xC9, 0x0C);
    ili9806e_send_cmd_data(ctx, 0xCA, 0x14);
    ili9806e_send_cmd_data(ctx, 0xCB, 0x08);
    ili9806e_send_cmd_data(ctx, 0xCC, 0x0F);
    ili9806e_send_cmd_data(ctx, 0xCD, 0x11);
    ili9806e_send_cmd_data(ctx, 0xCE, 0x09);
    ili9806e_send_cmd_data(ctx, 0xCF, 0x00);

    // Change to Page 6 CMD for GIP timing
    ili9806e_switch_page(ctx, 0x06);
    ili9806e_send_cmd_data(ctx, 0x00, 0x20);
    ili9806e_send_cmd_data(ctx, 0x01, 0x0A);
    ili9806e_send_cmd_data(ctx, 0x02, 0x00);
    ili9806e_send_cmd_data(ctx, 0x03, 0x00);
    ili9806e_send_cmd_data(ctx, 0x04, 0x01);
    ili9806e_send_cmd_data(ctx, 0x05, 0x01);
    ili9806e_send_cmd_data(ctx, 0x06, 0x98);
    ili9806e_send_cmd_data(ctx, 0x07, 0x06);
    ili9806e_send_cmd_data(ctx, 0x08, 0x01);
    ili9806e_send_cmd_data(ctx, 0x09, 0x80);
    ili9806e_send_cmd_data(ctx, 0x0A, 0x00);
    ili9806e_send_cmd_data(ctx, 0x0B, 0x00);
    ili9806e_send_cmd_data(ctx, 0x0C, 0x01);
    ili9806e_send_cmd_data(ctx, 0x0D, 0x01);
    ili9806e_send_cmd_data(ctx, 0x0E, 0x05);
    ili9806e_send_cmd_data(ctx, 0x0F, 0x00);
    ili9806e_send_cmd_data(ctx, 0x10, 0xF0);
    ili9806e_send_cmd_data(ctx, 0x11, 0xF4);
    ili9806e_send_cmd_data(ctx, 0x12, 0x01);
    ili9806e_send_cmd_data(ctx, 0x13, 0x00);
    ili9806e_send_cmd_data(ctx, 0x14, 0x00);
    ili9806e_send_cmd_data(ctx, 0x15, 0xC0);
    ili9806e_send_cmd_data(ctx, 0x16, 0x08);
    ili9806e_send_cmd_data(ctx, 0x17, 0x00);
    ili9806e_send_cmd_data(ctx, 0x18, 0x00);
    ili9806e_send_cmd_data(ctx, 0x19, 0x00);
    ili9806e_send_cmd_data(ctx, 0x1A, 0x00);
    ili9806e_send_cmd_data(ctx, 0x1B, 0x00);
    ili9806e_send_cmd_data(ctx, 0x1C, 0x00);
    ili9806e_send_cmd_data(ctx, 0x1D, 0x00);
    ili9806e_send_cmd_data(ctx, 0x20, 0x01);
    ili9806e_send_cmd_data(ctx, 0x21, 0x23);
    ili9806e_send_cmd_data(ctx, 0x22, 0x45);
    ili9806e_send_cmd_data(ctx, 0x23, 0x67);
    ili9806e_send_cmd_data(ctx, 0x24, 0x01);
    ili9806e_send_cmd_data(ctx, 0x25, 0x23);
    ili9806e_send_cmd_data(ctx, 0x26, 0x45);
    ili9806e_send_cmd_data(ctx, 0x27, 0x67);
    ili9806e_send_cmd_data(ctx, 0x30, 0x11);
    ili9806e_send_cmd_data(ctx, 0x31, 0x11);
    ili9806e_send_cmd_data(ctx, 0x32, 0x00);
    ili9806e_send_cmd_data(ctx, 0x33, 0xEE);
    ili9806e_send_cmd_data(ctx, 0x34, 0xFF);
    ili9806e_send_cmd_data(ctx, 0x35, 0xBB);
    ili9806e_send_cmd_data(ctx, 0x36, 0xAA);
    ili9806e_send_cmd_data(ctx, 0x37, 0xDD);
    ili9806e_send_cmd_data(ctx, 0x38, 0xCC);
    ili9806e_send_cmd_data(ctx, 0x39, 0x66);
    ili9806e_send_cmd_data(ctx, 0x3A, 0x77);
    ili9806e_send_cmd_data(ctx, 0x3B, 0x22);
    ili9806e_send_cmd_data(ctx, 0x3C, 0x22);
    ili9806e_send_cmd_data(ctx, 0x3D, 0x22);
    ili9806e_send_cmd_data(ctx, 0x3E, 0x22);
    ili9806e_send_cmd_data(ctx, 0x3F, 0x22);
    ili9806e_send_cmd_data(ctx, 0x40, 0x22);

    // Change to Page 7 CMD for GIP timing
    ili9806e_switch_page(ctx, 0x07);
    ili9806e_send_cmd_data(ctx, 0x17, 0x22);
    ili9806e_send_cmd_data(ctx, 0x02, 0x77);
    ili9806e_send_cmd_data(ctx, 0x26, 0xB2);

    // Change to Page 0 CMD for Normal command
    ili9806e_switch_page(ctx, 0x00);
    //TE ON
    ili9806e_send_cmd(ctx, 0x35);
    //24BIT
    ili9806e_send_cmd_data(ctx, 0x3A, 0x70);

    // exit sleep
    ili9806e_send_cmd(ctx, 0x11);
    usleep_range(120, 140);
    ili9806e_send_cmd(ctx, 0x29);
    usleep_range(25, 30);

    // enter sleep
    // ili9806e_send_cmd(ctx, 0x28);
    // usleep_range(10, 20);
    // ili9806e_send_cmd(ctx, 0x10);
    // usleep_range(25, 30);

    return 0;
}

static const struct drm_display_mode kd050fwfia019_default_mode = {
	.clock		= 29000,    /* 29000kHz, fps: 60hZ */

	.hdisplay	= 480,
	.hsync_start	= 480 + 30,     /* h + hbp */
	.hsync_end	= 480 + 30 + 4,     /* h + hbp + hspw */
	.htotal		= 480 + 30 + 4 + 18,     /* h + hbp + hspw + hfp = 532 */

	.vdisplay	= 854,
	.vsync_start	= 854 + 30,     /* h + hbp */
	.vsync_end	= 854 + 30 + 4,     /* h + hbp + vspw */
	.vtotal		= 854 + 30 + 4 + 20,     /* h + hbp + vspw + vfp = 908 */

	.width_mm	= 62,
	.height_mm	= 110,

	.flags		= DRM_MODE_FLAG_NHSYNC | DRM_MODE_FLAG_NVSYNC,
	.type		= DRM_MODE_TYPE_DRIVER | DRM_MODE_TYPE_PREFERRED,
};

static const struct panel_desc kd050fwfia019_desc = {
	.init_sequence = kd050fwfia019_init,
	.display_mode = &amp;amp;kd050fwfia019_default_mode,
	.mode_flags = MIPI_DSI_MODE_VIDEO | MIPI_DSI_MODE_VIDEO_BURST |
		      MIPI_DSI_MODE_LPM,
	.format = MIPI_DSI_FMT_RGB888,
	.lanes = 2,
};

static const struct of_device_id ili9806e_of_match[] = {
	{ .compatible = "startek,kd050fwfia019", .data = &amp;amp;kd050fwfia019_desc },
	{ }
};
MODULE_DEVICE_TABLE(of, ili9806e_of_match);

static struct mipi_dsi_driver ili9806e_dsi_driver = {
	.driver = {
		.name = "ili9806e-dsi",
		.of_match_table = ili9806e_of_match,
	},
	.probe = ili9806e_dsi_probe,
	.remove = ili9806e_dsi_remove,
};
module_mipi_dsi_driver(ili9806e_dsi_driver);

MODULE_AUTHOR("Author &amp;lt;author@example.com&amp;gt;");
MODULE_DESCRIPTION("Ilitek ILI9806E Controller Driver");
MODULE_LICENSE("GPL");&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Hope someone can help me figure it out. Thanks&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Nov 2024 09:23:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX93-DSI-failed-to-attach-bridge-soc-0-dsi-4ae10000-to-encoder/m-p/1999957#M231110</guid>
      <dc:creator>Satan</dc:creator>
      <dc:date>2024-11-22T09:23:52Z</dc:date>
    </item>
    <item>
      <title>Re: IMX93 DSI: failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX93-DSI-failed-to-attach-bridge-soc-0-dsi-4ae10000-to-encoder/m-p/2001450#M231181</link>
      <description>&lt;P&gt;refer to your driver, do you attach 480x854 display, the clock is 29Mhz, right? then I checked the clock driver, current driver doesn't support this, so you should add the new clock in the&amp;nbsp;fracn_tbl&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/drivers/clk/imx/clk-fracn-gppll.c" target="_blank"&gt;linux-imx/drivers/clk/imx/clk-fracn-gppll.c at lf-6.6.y · nxp-imx/linux-imx · GitHub&lt;/A&gt;&lt;/P&gt;
&lt;DIV class="Box-sc-g0xbh4-0 kRmGAS"&gt;
&lt;DIV class="Box-sc-g0xbh4-0 code-navigation-cursor" aria-hidden="true" data-testid="navigation-cursor"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;DIV class="Box-sc-g0xbh4-0 kRmGAS"&gt;
&lt;DIV class="Box-sc-g0xbh4-0 code-navigation-cursor" aria-hidden="true" data-testid="navigation-cursor"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;/DIV&gt;</description>
      <pubDate>Tue, 26 Nov 2024 01:14:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX93-DSI-failed-to-attach-bridge-soc-0-dsi-4ae10000-to-encoder/m-p/2001450#M231181</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2024-11-26T01:14:41Z</dc:date>
    </item>
    <item>
      <title>Re: IMX93 DSI: failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX93-DSI-failed-to-attach-bridge-soc-0-dsi-4ae10000-to-encoder/m-p/2001564#M231187</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;You're encountering (failed to attach bridge: -517) typically indicates that a required component or dependency is not ready during the device initialization process. This is often related to probe order issues in the Linux kernel device tree or missing configurations.&lt;/P&gt;&lt;P&gt;-517 corresponds to -EPROBE_DEFER, which indicates that the kernel driver is deferring its initialization because a dependency (e.g., another device or resource) is not ready.&lt;BR /&gt;The common reasons for this error include:&lt;BR /&gt;Missing or incorrect configuration in the device tree.&lt;BR /&gt;Drivers for dependent components are not loaded or initialized in the correct order.&lt;/P&gt;&lt;P&gt;Ensure that the panel and dsi nodes are correctly defined and match the bindings expected by the driver. Based on your device tree examples:&lt;BR /&gt;Confirm that the compatible strings ("startek,kd050fwfia019" and "ili9806e") match those in the kernel drivers.&lt;BR /&gt;Validate that the reset-gpios, vdd-supply, and vccio-supply properties are correctly defined and available.&lt;/P&gt;&lt;P&gt;Confirm that the dw-mipi-dsi and ili9806e drivers are being initialized in the correct order. Use dmesg to check for related logs:&amp;nbsp;dmesg | grep -i dsi&amp;nbsp;If the panel driver (panel-ilitek-ili9806e.c) is being probed before the DSI controller is ready, you may need to ensure the controller initializes earlier.&amp;nbsp;Move the panel node to be a sub-node of the dsi controller node. This ensures that the panel is registered as part of the DSI controller's initialization.&amp;nbsp;The panel-ilitek-ili9806e.c file should contain a valid initialization sequence for the ili9806e panel. Double-check the init_sequence function in your driver for any missing steps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Enable debug logs for DRM and DSI:&lt;/P&gt;&lt;P&gt;Add the following kernel parameters:&amp;nbsp;&lt;/P&gt;&lt;P&gt;drm.debug=0x1f&lt;/P&gt;&lt;P&gt;This provides detailed information about DRM and DSI initialization.&lt;BR /&gt;Use these logs to identify whether the panel or DSI controller is failing to probe.&lt;/P&gt;&lt;P&gt;Ensure that the regulators (vdd and vccio) and GPIOs are defined and active.&lt;BR /&gt;Verify that the backlight node is properly defined and linked in the device tree.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are still encountering issues, consider checking the driver documentation or&amp;nbsp;&lt;FONT size="1 2 3 4 5 6 7" color="#FFFFFF"&gt;&lt;A href="https://www.ingresosolidario.com.co" target="_self"&gt;consultar ingreso solidario&lt;/A&gt;&lt;/FONT&gt; similar device examples in the kernel source.&amp;nbsp;You can also try using CONFIG_DRM_PANEL_SIMPLE as a temporary panel driver for basic testing.&lt;BR /&gt;loglevel=8&lt;/P&gt;</description>
      <pubDate>Tue, 26 Nov 2024 03:54:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX93-DSI-failed-to-attach-bridge-soc-0-dsi-4ae10000-to-encoder/m-p/2001564#M231187</guid>
      <dc:creator>harold07douglas</dc:creator>
      <dc:date>2024-11-26T03:54:00Z</dc:date>
    </item>
  </channel>
</rss>