<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX8QM USB Role Swap Problems in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-USB-Role-Swap-Problems/m-p/1998909#M231085</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm having a difficulty implementing the role swap process between the i.MX8M evaluation board and an iPhone. The two are connected via a Lightning-to-USB-C cable and the kernel version is&amp;nbsp; 6.1.36-imx8qm+gdd01990ad5ea.&lt;/P&gt;&lt;P&gt;When I try modify the /sys/bus/platform/devices/ci_hdrc.0/role, from host to device, I encounter a write error stating that it is forbidden to write that file (even though write permission is enabled for root). Checking the events with dmesg, I see the log "ci_hdrc.0: Current configuration is not dual-role, quit".&lt;/P&gt;&lt;P&gt;The dr_mode file inside the directory /sys/firmware/devicetree/base/bus@5b000000/usb@5b110000/usb@5b120000/ has the "otg" value.&lt;/P&gt;&lt;P&gt;What should I do to make an effective role swap process? Additionaly, should I also operate on the i2c pins for the role-swap process?&lt;BR /&gt;I'm doing my first embedded project so I'm a complete beginner at this.&lt;/P&gt;&lt;P&gt;Any pointers or advice will be would be greatly appreciated.&lt;/P&gt;</description>
    <pubDate>Thu, 21 Nov 2024 13:26:04 GMT</pubDate>
    <dc:creator>Bitlorenz</dc:creator>
    <dc:date>2024-11-21T13:26:04Z</dc:date>
    <item>
      <title>iMX8QM USB Role Swap Problems</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-USB-Role-Swap-Problems/m-p/1998909#M231085</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm having a difficulty implementing the role swap process between the i.MX8M evaluation board and an iPhone. The two are connected via a Lightning-to-USB-C cable and the kernel version is&amp;nbsp; 6.1.36-imx8qm+gdd01990ad5ea.&lt;/P&gt;&lt;P&gt;When I try modify the /sys/bus/platform/devices/ci_hdrc.0/role, from host to device, I encounter a write error stating that it is forbidden to write that file (even though write permission is enabled for root). Checking the events with dmesg, I see the log "ci_hdrc.0: Current configuration is not dual-role, quit".&lt;/P&gt;&lt;P&gt;The dr_mode file inside the directory /sys/firmware/devicetree/base/bus@5b000000/usb@5b110000/usb@5b120000/ has the "otg" value.&lt;/P&gt;&lt;P&gt;What should I do to make an effective role swap process? Additionaly, should I also operate on the i2c pins for the role-swap process?&lt;BR /&gt;I'm doing my first embedded project so I'm a complete beginner at this.&lt;/P&gt;&lt;P&gt;Any pointers or advice will be would be greatly appreciated.&lt;/P&gt;</description>
      <pubDate>Thu, 21 Nov 2024 13:26:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-USB-Role-Swap-Problems/m-p/1998909#M231085</guid>
      <dc:creator>Bitlorenz</dc:creator>
      <dc:date>2024-11-21T13:26:04Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM USB Role Swap Problems</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-USB-Role-Swap-Problems/m-p/2000160#M231118</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I think you should modify the hardware there is a resistor in line USB+ you need to change to operate a host device.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 22 Nov 2024 14:15:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-USB-Role-Swap-Problems/m-p/2000160#M231118</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-11-22T14:15:09Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM USB Role Swap Problems</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-USB-Role-Swap-Problems/m-p/2002677#M231267</link>
      <description>&lt;P&gt;Hi, Thank you for your response.&lt;/P&gt;&lt;P&gt;The resistor that you're talking about is the D1+ or D2+ in the U27/U55/U56 block that are connected to the usb type c port? How can I programmatically change that ? I should change it after the request of control swap?&lt;/P&gt;&lt;P&gt;I've found in this forum a question ("USB role switch with chipidea on i.MX8QXP") &lt;SPAN&gt;with a control transfer that can disconnect the otg device but then i don't see it as the host.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Nov 2024 08:47:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-USB-Role-Swap-Problems/m-p/2002677#M231267</guid>
      <dc:creator>Bitlorenz</dc:creator>
      <dc:date>2024-11-27T08:47:34Z</dc:date>
    </item>
  </channel>
</rss>