<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Dram retention mode in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Dram-retention-mode/m-p/1998617#M231062</link>
    <description>Hi,&lt;BR /&gt;&lt;BR /&gt;I recently trying the API that you provided in the SDK (board.c)&lt;BR /&gt;&lt;BR /&gt;The test is quite simple.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;1) Create a timer about 30s&lt;BR /&gt;2)&amp;nbsp;Call BOARD_DramEnterRetention + WFI()&lt;BR /&gt;3) when timer expired, trigger the interrupt and call BOARD_DramExitRetention()&lt;BR /&gt;&lt;BR /&gt;I could see some current changes when in retention mode. However, it seems not able to exit.&lt;BR /&gt;&lt;BR /&gt;May I know why when calling BOARD_DramExitRetention(), the A core is not wake up and the M Core is dead?</description>
    <pubDate>Thu, 21 Nov 2024 07:23:15 GMT</pubDate>
    <dc:creator>abdrhmn</dc:creator>
    <dc:date>2024-11-21T07:23:15Z</dc:date>
    <item>
      <title>Dram retention mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dram-retention-mode/m-p/1995014#M230878</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on imx8ulp power optimization.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am interested to know more on the dram_enter_retention mode and dram_exit_retention mode.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1) Other than observing the current usage, How to know that it is already in retention mode?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2) Is the retention mode only work in shared ram?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3) If calling the retention mode causing the system hang, what would be the culprit?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;4) If calling the dram_exit_retention mode causing the current a bit higher (than before calling it), what is the reason?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Nov 2024 00:06:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dram-retention-mode/m-p/1995014#M230878</guid>
      <dc:creator>abdrhmn</dc:creator>
      <dc:date>2024-11-15T00:06:39Z</dc:date>
    </item>
    <item>
      <title>Re: Dram retention mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dram-retention-mode/m-p/1995360#M230889</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;Q1:&lt;SPAN&gt;&amp;nbsp;Other than observing the current usage, How to know that it is already in retention mode?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;--&amp;gt;There is no other way to make observations, these functions are tested and there is no need to worry about it not being triggered correctly.&lt;/P&gt;
&lt;P&gt;Q2:&amp;nbsp;&lt;SPAN&gt;Is the retention mode only work in shared ram?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;--&amp;gt;Yes&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Q3:&amp;nbsp;&lt;SPAN&gt;If calling the retention mode causing the system hang, what would be the culprit?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;--&amp;gt;Have you made any changes to the code for this feature?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Q4 :&amp;nbsp;&lt;SPAN&gt;If calling the dram_exit_retention mode causing the current a bit higher (than before calling it), what is the reason?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;--&amp;gt;&lt;SPAN&gt;dram_exit_retention will recover DDR clocks and enable DDR PHY, so the current going to high is&amp;nbsp;reasonable&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Fri, 15 Nov 2024 09:41:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dram-retention-mode/m-p/1995360#M230889</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-11-15T09:41:15Z</dc:date>
    </item>
    <item>
      <title>Re: Dram retention mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dram-retention-mode/m-p/1996832#M230965</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;If the system I'm working on using lpddr. How can I make this work?&lt;/P&gt;</description>
      <pubDate>Tue, 19 Nov 2024 06:10:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dram-retention-mode/m-p/1996832#M230965</guid>
      <dc:creator>abdrhmn</dc:creator>
      <dc:date>2024-11-19T06:10:28Z</dc:date>
    </item>
    <item>
      <title>Re: Dram retention mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dram-retention-mode/m-p/1997557#M231006</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The functions in&amp;nbsp;plat/imx/imx8ulp/dram.c(imx-atf) have been done for different DRAMs, LPDDR4 &amp;amp; LPDDR3. There are still some spaces to&amp;nbsp;o&lt;SPAN class="fontstyle0"&gt;ptimize power consumption&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;SPAN class="fontstyle0"&gt;&amp;nbsp;please refer&amp;nbsp; &lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN13951.pdf" target="_self"&gt;AN13951&amp;nbsp;&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Wed, 20 Nov 2024 00:42:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dram-retention-mode/m-p/1997557#M231006</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-11-20T00:42:26Z</dc:date>
    </item>
    <item>
      <title>Re: Dram retention mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dram-retention-mode/m-p/1998617#M231062</link>
      <description>Hi,&lt;BR /&gt;&lt;BR /&gt;I recently trying the API that you provided in the SDK (board.c)&lt;BR /&gt;&lt;BR /&gt;The test is quite simple.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;1) Create a timer about 30s&lt;BR /&gt;2)&amp;nbsp;Call BOARD_DramEnterRetention + WFI()&lt;BR /&gt;3) when timer expired, trigger the interrupt and call BOARD_DramExitRetention()&lt;BR /&gt;&lt;BR /&gt;I could see some current changes when in retention mode. However, it seems not able to exit.&lt;BR /&gt;&lt;BR /&gt;May I know why when calling BOARD_DramExitRetention(), the A core is not wake up and the M Core is dead?</description>
      <pubDate>Thu, 21 Nov 2024 07:23:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dram-retention-mode/m-p/1998617#M231062</guid>
      <dc:creator>abdrhmn</dc:creator>
      <dc:date>2024-11-21T07:23:15Z</dc:date>
    </item>
    <item>
      <title>Re: Dram retention mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dram-retention-mode/m-p/1998637#M231065</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;To test&amp;nbsp;Dram retention and exit, please use&amp;nbsp;power_mode_switch demo and refer the api in&amp;nbsp;power_mode_switch.c.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Thu, 21 Nov 2024 07:49:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dram-retention-mode/m-p/1998637#M231065</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-11-21T07:49:25Z</dc:date>
    </item>
  </channel>
</rss>