<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic maaxboard mickledore branch kernel patch can not be applied in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/maaxboard-mickledore-branch-kernel-patch-can-not-be-applied/m-p/1997453#M230996</link>
    <description>&lt;P&gt;HI&lt;BR /&gt;I used langdale branch for maaxboard-mini (maaxboard-zeus sumo)&lt;BR /&gt;especially langdale branch for maaxboard-mini ,the source code are almost are same.&lt;/P&gt;&lt;P&gt;I add my M41T93 spi rtc kernel patch at meta-maaxboard/recipes-kernel/linux/linux-maaxboard-src.inc&lt;/P&gt;&lt;P&gt;the content is below:&lt;BR /&gt;KERNEL_SRC:maaxboardbase = "${MAAXBOARD_GIT_HOST_MIRROR}/linux-imx.git;${MAAXBOARD_GIT_PROTOCOL}"&lt;BR /&gt;KERNEL_BRANCH:maaxboardbase = "maaxboard_lf-6.1.22-2.0.0"&lt;BR /&gt;SRC_URI:maaxboardbase = "${KERNEL_SRC};branch=${KERNEL_BRANCH};${MAAXBOARD_GIT_USER}&lt;BR /&gt;file://002-rtc-m41t93.patch&lt;BR /&gt;"&lt;/P&gt;&lt;P&gt;SRCREV:maaxboardbase = "${AUTOREV}"&lt;/P&gt;&lt;P&gt;FILESEXTRAPATHS:prepend := "${THISDIR}/files:"&lt;BR /&gt;SRC_URI:maaxboardbase += "file://rtcm41t93.cfg"&lt;/P&gt;&lt;P&gt;do_configure:append() {&lt;BR /&gt;cat ${WORKDIR}/rtcm41t93.cfg &amp;gt;&amp;gt; ${B}/.config&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;--&lt;BR /&gt;anyway, use do_configure:append() .config can be changed forcely (before not use like this ,I worked before like this:&lt;BR /&gt;SRC_URI:maaxboardbase = "${KERNEL_SRC};branch=${KERNEL_BRANCH};${MAAXBOARD_GIT_USER}&lt;BR /&gt;file://002-rtc-m41t93.patch&lt;BR /&gt;file://rtcm41t93.cfg&lt;BR /&gt;"&lt;BR /&gt;but currently I need to use do_configure:append() to work. anyway it works. that's fine.&lt;/P&gt;&lt;P&gt;but patch file file://002-rtc-m41t93.patch NOT applied ,&lt;BR /&gt;kernel can be compiled ,but no patch applied&lt;/P&gt;&lt;P&gt;I need to patc h the file ./tmp/work/armv8a-mx8m-poky-linux/linux-imx-headers/6.1-r0/git/arch/arm64/boot/dts/freescale/maaxboard/ext-spi1.dts&lt;BR /&gt;but after the compilation finished. the file is same as the original, not changed.&lt;BR /&gt;I find the patch file 002-rtc-m41t93.patch was copied to ./tmp/work/maaxboard-poky-linux/linux-imx/6.1.22+gitAUTOINC+78ce688d5a-r0/&lt;BR /&gt;but NOT applied!&lt;/P&gt;&lt;P&gt;any help?&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;I also post the issue here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/Avnet/meta-maaxboard/issues/10" target="_blank"&gt;https://github.com/Avnet/meta-maaxboard/issues/10&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 19 Nov 2024 20:21:10 GMT</pubDate>
    <dc:creator>gonewithwind-peter</dc:creator>
    <dc:date>2024-11-19T20:21:10Z</dc:date>
    <item>
      <title>maaxboard mickledore branch kernel patch can not be applied</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/maaxboard-mickledore-branch-kernel-patch-can-not-be-applied/m-p/1997453#M230996</link>
      <description>&lt;P&gt;HI&lt;BR /&gt;I used langdale branch for maaxboard-mini (maaxboard-zeus sumo)&lt;BR /&gt;especially langdale branch for maaxboard-mini ,the source code are almost are same.&lt;/P&gt;&lt;P&gt;I add my M41T93 spi rtc kernel patch at meta-maaxboard/recipes-kernel/linux/linux-maaxboard-src.inc&lt;/P&gt;&lt;P&gt;the content is below:&lt;BR /&gt;KERNEL_SRC:maaxboardbase = "${MAAXBOARD_GIT_HOST_MIRROR}/linux-imx.git;${MAAXBOARD_GIT_PROTOCOL}"&lt;BR /&gt;KERNEL_BRANCH:maaxboardbase = "maaxboard_lf-6.1.22-2.0.0"&lt;BR /&gt;SRC_URI:maaxboardbase = "${KERNEL_SRC};branch=${KERNEL_BRANCH};${MAAXBOARD_GIT_USER}&lt;BR /&gt;file://002-rtc-m41t93.patch&lt;BR /&gt;"&lt;/P&gt;&lt;P&gt;SRCREV:maaxboardbase = "${AUTOREV}"&lt;/P&gt;&lt;P&gt;FILESEXTRAPATHS:prepend := "${THISDIR}/files:"&lt;BR /&gt;SRC_URI:maaxboardbase += "file://rtcm41t93.cfg"&lt;/P&gt;&lt;P&gt;do_configure:append() {&lt;BR /&gt;cat ${WORKDIR}/rtcm41t93.cfg &amp;gt;&amp;gt; ${B}/.config&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;--&lt;BR /&gt;anyway, use do_configure:append() .config can be changed forcely (before not use like this ,I worked before like this:&lt;BR /&gt;SRC_URI:maaxboardbase = "${KERNEL_SRC};branch=${KERNEL_BRANCH};${MAAXBOARD_GIT_USER}&lt;BR /&gt;file://002-rtc-m41t93.patch&lt;BR /&gt;file://rtcm41t93.cfg&lt;BR /&gt;"&lt;BR /&gt;but currently I need to use do_configure:append() to work. anyway it works. that's fine.&lt;/P&gt;&lt;P&gt;but patch file file://002-rtc-m41t93.patch NOT applied ,&lt;BR /&gt;kernel can be compiled ,but no patch applied&lt;/P&gt;&lt;P&gt;I need to patc h the file ./tmp/work/armv8a-mx8m-poky-linux/linux-imx-headers/6.1-r0/git/arch/arm64/boot/dts/freescale/maaxboard/ext-spi1.dts&lt;BR /&gt;but after the compilation finished. the file is same as the original, not changed.&lt;BR /&gt;I find the patch file 002-rtc-m41t93.patch was copied to ./tmp/work/maaxboard-poky-linux/linux-imx/6.1.22+gitAUTOINC+78ce688d5a-r0/&lt;BR /&gt;but NOT applied!&lt;/P&gt;&lt;P&gt;any help?&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;I also post the issue here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/Avnet/meta-maaxboard/issues/10" target="_blank"&gt;https://github.com/Avnet/meta-maaxboard/issues/10&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Nov 2024 20:21:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/maaxboard-mickledore-branch-kernel-patch-can-not-be-applied/m-p/1997453#M230996</guid>
      <dc:creator>gonewithwind-peter</dc:creator>
      <dc:date>2024-11-19T20:21:10Z</dc:date>
    </item>
    <item>
      <title>Re: maaxboard mickledore branch kernel patch can not be applied</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/maaxboard-mickledore-branch-kernel-patch-can-not-be-applied/m-p/1998066#M231033</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;you need contact you vendor since patches are for EVK and linux BSP. if it can not apply please check with you vendor.&lt;/P&gt;
&lt;P&gt;Rregards&lt;/P&gt;</description>
      <pubDate>Wed, 20 Nov 2024 14:42:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/maaxboard-mickledore-branch-kernel-patch-can-not-be-applied/m-p/1998066#M231033</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-11-20T14:42:22Z</dc:date>
    </item>
    <item>
      <title>Re: maaxboard mickledore branch kernel patch can not be applied</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/maaxboard-mickledore-branch-kernel-patch-can-not-be-applied/m-p/2000204#M231121</link>
      <description>&lt;P&gt;sorry, the new branch&amp;nbsp; put the patched files in different folders. it works.&lt;/P&gt;</description>
      <pubDate>Fri, 22 Nov 2024 14:55:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/maaxboard-mickledore-branch-kernel-patch-can-not-be-applied/m-p/2000204#M231121</guid>
      <dc:creator>gonewithwind-peter</dc:creator>
      <dc:date>2024-11-22T14:55:09Z</dc:date>
    </item>
  </channel>
</rss>