<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DHCP DORA Process stucks at DISCOVER/OFFER in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DHCP-DORA-Process-stucks-at-DISCOVER-OFFER/m-p/1996471#M230945</link>
    <description>Hi,&lt;BR /&gt;&lt;BR /&gt;I have not tried with the latest BSP, as this issue is occurring with units already deployed in the field. We need to address this problem without changing the BSP version.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Muthyam D.</description>
    <pubDate>Mon, 18 Nov 2024 14:21:23 GMT</pubDate>
    <dc:creator>Muthyam</dc:creator>
    <dc:date>2024-11-18T14:21:23Z</dc:date>
    <item>
      <title>DHCP DORA Process stucks at DISCOVER/OFFER</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DHCP-DORA-Process-stucks-at-DISCOVER-OFFER/m-p/1996345#M230934</link>
      <description>&lt;DIV class=""&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;I’m using the Apalis iMX8 QuadPlus with Yocto Dunfell on our custom board. While the unit generally functions well, there are times when it fails to obtain an IP address from the DHCP server. We’ve used &lt;EM&gt;tcpdump&lt;/EM&gt; on both the server and client sides for analysis. The client continuously sends DHCP Discover packets, which the server receives and responds to with DHCP Offer packets. However, these Offer packets are not visible on the client side. As a result, the client keeps sending additional Discover packets, causing the process to stall and preventing it from acquiring an IP address. This situation persists until the unit is power-cycled or the &lt;EM&gt;eth0&lt;/EM&gt; interface is brought down and then back up.&lt;/P&gt;&lt;P&gt;Client Side&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class=""&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Muthyam_0-1731931817079.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/311035i704C5944FE4A2302/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Muthyam_0-1731931817079.png" alt="Muthyam_0-1731931817079.png" /&gt;&lt;/span&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class=""&gt;&lt;SPAN class=""&gt;Client_Broadcasting_DISCOVER_Message&lt;/SPAN&gt;&lt;SPAN class=""&gt;1366×768 69.4 KB&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Server Side&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class=""&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Muthyam_1-1731931817202.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/311036i07235D81B5897CF6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Muthyam_1-1731931817202.png" alt="Muthyam_1-1731931817202.png" /&gt;&lt;/span&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class=""&gt;&lt;SPAN class=""&gt;Server_Replying2Discover_OfferWithUnicast&lt;/SPAN&gt;&lt;SPAN class=""&gt;719×678 15.1 KB&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any guidance on resolving this issue promptly would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you,&lt;BR /&gt;Muthyam D.&lt;/P&gt;&lt;/DIV&gt;</description>
      <pubDate>Mon, 18 Nov 2024 12:09:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DHCP-DORA-Process-stucks-at-DISCOVER-OFFER/m-p/1996345#M230934</guid>
      <dc:creator>Muthyam</dc:creator>
      <dc:date>2024-11-18T12:09:17Z</dc:date>
    </item>
    <item>
      <title>Re: DHCP DORA Process stucks at DISCOVER/OFFER</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DHCP-DORA-Process-stucks-at-DISCOVER-OFFER/m-p/1996467#M230944</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;Have you tried to replicate with the latest BSP for your board? Is the issue still present?&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 18 Nov 2024 14:12:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DHCP-DORA-Process-stucks-at-DISCOVER-OFFER/m-p/1996467#M230944</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-11-18T14:12:26Z</dc:date>
    </item>
    <item>
      <title>Re: DHCP DORA Process stucks at DISCOVER/OFFER</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DHCP-DORA-Process-stucks-at-DISCOVER-OFFER/m-p/1996471#M230945</link>
      <description>Hi,&lt;BR /&gt;&lt;BR /&gt;I have not tried with the latest BSP, as this issue is occurring with units already deployed in the field. We need to address this problem without changing the BSP version.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Muthyam D.</description>
      <pubDate>Mon, 18 Nov 2024 14:21:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DHCP-DORA-Process-stucks-at-DISCOVER-OFFER/m-p/1996471#M230945</guid>
      <dc:creator>Muthyam</dc:creator>
      <dc:date>2024-11-18T14:21:23Z</dc:date>
    </item>
    <item>
      <title>Re: DHCP DORA Process stucks at DISCOVER/OFFER</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DHCP-DORA-Process-stucks-at-DISCOVER-OFFER/m-p/1997472#M231000</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214675"&gt;@Muthyam&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The workaround you can use is to add the following line to your /etc/network/interfaces:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;auto eth0
iface eth0 inet dhcp
dhclient_opts -nw&lt;/LI-CODE&gt;
&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Tue, 19 Nov 2024 21:46:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DHCP-DORA-Process-stucks-at-DISCOVER-OFFER/m-p/1997472#M231000</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-11-19T21:46:41Z</dc:date>
    </item>
    <item>
      <title>Re: DHCP DORA Process stucks at DISCOVER/OFFER</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DHCP-DORA-Process-stucks-at-DISCOVER-OFFER/m-p/1998047#M231030</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442"&gt;@JosephAtNXP&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;As far as I know, the /etc/network/interfaces file is used when NetworkManager manages the network interfaces. However, the Toradex BSP provides two utilities for network configuration: &lt;STRONG&gt;ConnMan&lt;/STRONG&gt; and &lt;STRONG&gt;systemd-networkd&lt;/STRONG&gt;. By default:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;The Ethernet port is managed by &lt;STRONG&gt;ConnMan&lt;/STRONG&gt;.&lt;/LI&gt;&lt;LI&gt;The USB RNDIS interface is managed by &lt;STRONG&gt;systemd-networkd&lt;/STRONG&gt;.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;In our setup, there was no /etc/network/interfaces file by default. After encountering this issue, we disabled the &lt;STRONG&gt;ConnMan&lt;/STRONG&gt; service and assigned control of the eth0 interface to &lt;STRONG&gt;systemd-networkd&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Even after manually adding an interfaces file at /etc/network, the issue still persists.&lt;/P&gt;&lt;P&gt;Thank you,&lt;BR /&gt;Muthyam D.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Nov 2024 13:55:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DHCP-DORA-Process-stucks-at-DISCOVER-OFFER/m-p/1998047#M231030</guid>
      <dc:creator>Muthyam</dc:creator>
      <dc:date>2024-11-20T13:55:35Z</dc:date>
    </item>
  </channel>
</rss>