<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: LG Air Conditioning Controller (based on i.MX5)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LG-Air-Conditioning-Controller-based-on-i-MX5/m-p/1995530#M230898</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I can not seen the reason of panic but it looks like a bad programming, burn again your board and restart.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Fri, 15 Nov 2024 14:24:49 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-11-15T14:24:49Z</dc:date>
    <item>
      <title>LG Air Conditioning Controller (based on i.MX5)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LG-Air-Conditioning-Controller-based-on-i-MX5/m-p/1994887#M230873</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm a newbie about these boards but I'm here to ask you, experts, an hand recovering my controller which is based on a Freescale i.MX5 board.&lt;BR /&gt;&lt;BR /&gt;The appliance commercial name is AC SMART IV by LG and his main purpouse is to manage all air conditioning units attached to an external unit. The board is equipped with an MMC partitioned in 2 slices to contain root filesystem (ext2).&lt;BR /&gt;&lt;BR /&gt;My board now stucks booting saying "kernel panic" because he cannot locate any filesystem on root partition.&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;Someone can help me recovering boot partition?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Running some commands from the boot menu I have:&lt;BR /&gt;&lt;STRONG&gt;BBG U-Boot &amp;gt;&lt;/STRONG&gt; mmcinfo&lt;BR /&gt;Device: FSL_ESDHC&lt;BR /&gt;Manufacturer ID: 45&lt;BR /&gt;OEM: 100&lt;BR /&gt;Name: SEM04&lt;BR /&gt;Tran Speed: 25000000&lt;BR /&gt;Rd Block Len: 512&lt;BR /&gt;MMC version 4.0&lt;BR /&gt;High Capacity: Yes&lt;BR /&gt;Capacity: 3959422976&lt;BR /&gt;Bus Width: 4-bit&lt;/P&gt;&lt;P&gt;BBG U-Boot &amp;gt; fatinfo mmc&lt;BR /&gt;Interface: MMC&lt;BR /&gt;Device 0: Vendor: Man 450100 Snr 90232720 Rev: 4.7 Prod: SEM04&lt;BR /&gt;Type: Removable Hard Disk&lt;BR /&gt;Capacity: 3776.0 MB = 3.6 GB (7733248 x 512)&lt;/P&gt;&lt;P&gt;No valid FAT fs found&lt;/P&gt;&lt;P&gt;BBG U-Boot &amp;gt; iminfo&lt;/P&gt;&lt;P&gt;## Checking Image at 90800000 ...&lt;BR /&gt;Unknown image format!&lt;/P&gt;&lt;P&gt;BBG U-Boot &amp;gt; bdinfo&lt;BR /&gt;arch_number = 0x0000084D&lt;BR /&gt;env_t = 0x00000000&lt;BR /&gt;boot_params = 0x90000100&lt;BR /&gt;DRAM bank = 0x00000000&lt;BR /&gt;-&amp;gt; start = 0x90000000&lt;BR /&gt;-&amp;gt; size = 0x20000000&lt;BR /&gt;ethaddr = 00:E0:91:0F:09:8B&lt;BR /&gt;ip_addr = 192.168.10.13&lt;BR /&gt;baudrate = 115200 bps&lt;/P&gt;&lt;P&gt;At boot I have:&lt;/P&gt;&lt;P&gt;pmic_rtc pmic_rtc.1: setting system clock to 1970-01-24 09:23:28 UTC (2021008)&lt;BR /&gt;List of all partitions:&lt;BR /&gt;b300 3866624 mmcblk0 driver: mmcblk&lt;BR /&gt;b301 819232 mmcblk0p1&lt;BR /&gt;b302 2893824 mmcblk0p2&lt;BR /&gt;No filesystem could mount root, tried: ext3 ext2 ext4 cramfs vfat msdos&lt;BR /&gt;[&amp;lt;800c54ac&amp;gt;] (unwind_backtrace+0x0/0xf0) from [&amp;lt;804a2dfc&amp;gt;] (panic+0x6c/0xe0)9,1)&lt;BR /&gt;[&amp;lt;804a2dfc&amp;gt;] (panic+0x6c/0xe0) from [&amp;lt;80008ef8&amp;gt;] (mount_block_root+0x1cc/0x20c)&lt;BR /&gt;+0x160/0x1b8)(mount_block_root+0x1cc/0x20c) from [&amp;lt;80009188&amp;gt;] (prepare_namespace&lt;BR /&gt;0/0x168)88&amp;gt;] (prepare_namespace+0x160/0x1b8) from [&amp;lt;80008480&amp;gt;] (kernel_init+0x12&lt;BR /&gt;/0x8)08480&amp;gt;] (kernel_init+0x120/0x168) from [&amp;lt;800c19c0&amp;gt;] (kernel_thread_exit+0x0&lt;/P&gt;</description>
      <pubDate>Thu, 14 Nov 2024 19:12:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LG-Air-Conditioning-Controller-based-on-i-MX5/m-p/1994887#M230873</guid>
      <dc:creator>FilippoAdessi</dc:creator>
      <dc:date>2024-11-14T19:12:52Z</dc:date>
    </item>
    <item>
      <title>Re: LG Air Conditioning Controller (based on i.MX5)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LG-Air-Conditioning-Controller-based-on-i-MX5/m-p/1995530#M230898</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I can not seen the reason of panic but it looks like a bad programming, burn again your board and restart.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 15 Nov 2024 14:24:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LG-Air-Conditioning-Controller-based-on-i-MX5/m-p/1995530#M230898</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-11-15T14:24:49Z</dc:date>
    </item>
    <item>
      <title>Re: LG Air Conditioning Controller (based on i.MX5)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LG-Air-Conditioning-Controller-based-on-i-MX5/m-p/1995598#M230902</link>
      <description>&lt;P&gt;Sure! The board, in my humble opinion, is ok but I miss the code to flash. Kernel was compiled by LG which distributes (sell) this product. I've asked to their "specialistic support" but the only answer I had was: "we dunno".&lt;BR /&gt;&lt;BR /&gt;Is someone so human to give me some hints on how to recover partitions or how to check and find why the system is unable to find a valid filesystem on root partition?&lt;BR /&gt;&lt;BR /&gt;Is there an utility as fsck to check and repair filesystem corrupted?&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;Filippo&lt;/P&gt;</description>
      <pubDate>Fri, 15 Nov 2024 18:03:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LG-Air-Conditioning-Controller-based-on-i-MX5/m-p/1995598#M230902</guid>
      <dc:creator>FilippoAdessi</dc:creator>
      <dc:date>2024-11-15T18:03:06Z</dc:date>
    </item>
  </channel>
</rss>