<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックThreadX NetX Duo Multithreading</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ThreadX-NetX-Duo-Multithreading/m-p/1993716#M230820</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;DIV class=""&gt;&lt;P&gt;I'm wondering if there are any restrictions on using NetX Duo resources from multiple threads? E.g. assuming that an NX_IP object has been created using nx_ip_create (which looks to be thread safe as it disables interrupts when placing the create NX_IP object in the IP control block), can this object be passed to other API functions without explicit synchronization from the user application?&lt;/P&gt;&lt;P&gt;I'm investigating an issue where a call to nx_web_http_client_response_body_get sporadically fails with NX_SECURE_TLS_INVALID_STATE, which comes from the fact that the TLS socket seems to have been reset, and its type is NX_SECURE_TLS_SESSION_TYPE_NONE. Removing the other threads that share the network resources of the thread in question seems to resolve the issue, but I can't find anything in the NetX Duo documentation specifying whether multithreading is inherently supported.&lt;/P&gt;&lt;P&gt;Kind regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/DIV&gt;</description>
    <pubDate>Wed, 13 Nov 2024 12:38:46 GMT</pubDate>
    <dc:creator>dafela</dc:creator>
    <dc:date>2024-11-13T12:38:46Z</dc:date>
    <item>
      <title>ThreadX NetX Duo Multithreading</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ThreadX-NetX-Duo-Multithreading/m-p/1993716#M230820</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;DIV class=""&gt;&lt;P&gt;I'm wondering if there are any restrictions on using NetX Duo resources from multiple threads? E.g. assuming that an NX_IP object has been created using nx_ip_create (which looks to be thread safe as it disables interrupts when placing the create NX_IP object in the IP control block), can this object be passed to other API functions without explicit synchronization from the user application?&lt;/P&gt;&lt;P&gt;I'm investigating an issue where a call to nx_web_http_client_response_body_get sporadically fails with NX_SECURE_TLS_INVALID_STATE, which comes from the fact that the TLS socket seems to have been reset, and its type is NX_SECURE_TLS_SESSION_TYPE_NONE. Removing the other threads that share the network resources of the thread in question seems to resolve the issue, but I can't find anything in the NetX Duo documentation specifying whether multithreading is inherently supported.&lt;/P&gt;&lt;P&gt;Kind regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 13 Nov 2024 12:38:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ThreadX-NetX-Duo-Multithreading/m-p/1993716#M230820</guid>
      <dc:creator>dafela</dc:creator>
      <dc:date>2024-11-13T12:38:46Z</dc:date>
    </item>
    <item>
      <title>Re: ThreadX NetX Duo Multithreading</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ThreadX-NetX-Duo-Multithreading/m-p/1993768#M230827</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;there is no restriction to use multithread and multiprocessing on i.MX8, mabe someone of&amp;nbsp;@threadx could help with this.&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Wed, 13 Nov 2024 14:08:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ThreadX-NetX-Duo-Multithreading/m-p/1993768#M230827</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-11-13T14:08:00Z</dc:date>
    </item>
    <item>
      <title>Re: ThreadX NetX Duo Multithreading</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ThreadX-NetX-Duo-Multithreading/m-p/1994327#M230859</link>
      <description>&lt;P&gt;Do you have direct contact with the developers of ThreadX, are they available to answer in this forum?&lt;/P&gt;</description>
      <pubDate>Thu, 14 Nov 2024 06:16:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ThreadX-NetX-Duo-Multithreading/m-p/1994327#M230859</guid>
      <dc:creator>dafela</dc:creator>
      <dc:date>2024-11-14T06:16:40Z</dc:date>
    </item>
    <item>
      <title>Re: ThreadX NetX Duo Multithreading</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ThreadX-NetX-Duo-Multithreading/m-p/1994637#M230863</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;No,They should be available trough this forum but you can send an email:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://rtosx.com/threadx-tech-support/" target="_blank"&gt;https://rtosx.com/threadx-tech-support/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 14 Nov 2024 12:37:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ThreadX-NetX-Duo-Multithreading/m-p/1994637#M230863</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-11-14T12:37:15Z</dc:date>
    </item>
  </channel>
</rss>