<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: AVB Demos, AVDECC entity definition, create custom</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/AVB-Demos-AVDECC-entity-definition-create-custom/m-p/1992902#M230768</link>
    <description>&lt;P&gt;Hi, Joseph,&lt;/P&gt;&lt;P&gt;Thanks for responding.&amp;nbsp; Have you tried what you're suggesting?&amp;nbsp; When I run the Hive controller, I can see the configurations, and the Dynamic Info-&amp;gt;Stream Format, but I cannot change the stream format.&amp;nbsp; The only selection offered is the one that is set.&amp;nbsp; For demo #22, that's AAF, 48kHz, PCM-INT-32, 2 channels.&amp;nbsp; I was hoping to configure a profile as having an 8 channel stream, rather than 4 streams of 2 channels (or, in the case of profile #22, 2 streams of 2 channels).&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Having said that, I have been able to configure ALSA's plug-ins to divide my 8 channel device into 4 2-channel devices, and they work, at least with aplay and arecord.&amp;nbsp; When I use one of the pairs as the alsa device for this demo (#22 or #9/11), I get no errors that I recognize, but also no sound.&amp;nbsp; More precisely, I get no sound that is related to the signal being put into the alsa device.&amp;nbsp; When I make the connection in the Hive controller, I DO hear a faint high-pitched noise, so it's trying to do something.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've attached the /var/log/avb and /var/log/avb_media_app logs from the talker and listener in case someone can see something I cannot.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 12 Nov 2024 14:21:41 GMT</pubDate>
    <dc:creator>jpa</dc:creator>
    <dc:date>2024-11-12T14:21:41Z</dc:date>
    <item>
      <title>AVB Demos, AVDECC entity definition, create custom</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AVB-Demos-AVDECC-entity-definition-create-custom/m-p/1991144#M230683</link>
      <description>&lt;P&gt;As I understand it, in the AVB demos, there are binary .aem files that define the AVDECC stream configurations.&amp;nbsp; &amp;nbsp;I'm trying to use those demos on custom i.MX8MP hardware, and the ADC/DAC that is available has limited format and channel support.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a binary .aem file that supports 8 channels, 32 bit LE at 48 kHz?&amp;nbsp; If not, is there documentation for that file format or a utility that can be used to create such a configuration file (or some other approach that I should be considering) ?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is "Hive Controller binaries and scrounging up a Windows PC"&amp;nbsp; an answer, the only answer, the best answer?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;</description>
      <pubDate>Fri, 08 Nov 2024 14:34:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AVB-Demos-AVDECC-entity-definition-create-custom/m-p/1991144#M230683</guid>
      <dc:creator>jpa</dc:creator>
      <dc:date>2024-11-08T14:34:00Z</dc:date>
    </item>
    <item>
      <title>Re: AVB Demos, AVDECC entity definition, create custom</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AVB-Demos-AVDECC-entity-definition-create-custom/m-p/1991982#M230724</link>
      <description>&lt;P&gt;Well, I think I can answer that last piece, myself, at this point.&amp;nbsp; The Hive controller does not allow me to change the configurations.&amp;nbsp; There are drop-downs that make it seem like it might, but the drop-downs are only populated with the current setting.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Nov 2024 13:00:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AVB-Demos-AVDECC-entity-definition-create-custom/m-p/1991982#M230724</guid>
      <dc:creator>jpa</dc:creator>
      <dc:date>2024-11-11T13:00:04Z</dc:date>
    </item>
    <item>
      <title>Re: AVB Demos, AVDECC entity definition, create custom</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AVB-Demos-AVDECC-entity-definition-create-custom/m-p/1992186#M230733</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;What defines the stream configurations are the profiles that both sides set, quoting from AVB spec:&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;The vendor shall notify the certification facility of the range of format variants (for example, audio channels, video resolution and profile, etc.)&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;For your tests, you need to refer to the AVB demos by NXP which can be &lt;A href="https://www.nxp.com/docs/en/user-guide/GENAVBTSNUG.pdf" target="_self"&gt;found here&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Your channel requirement is solved in this chapter:&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;10.3.2 Connect audio streams with different channel count&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;The avdecc entity model supports multiple stream formats with different channel counts (1, 2, 4, 6 and 8 channels) for the stream inputs/outputs. To change the stream inputs/outputs format, use the Hive controller to set the desired stream format on both talker and listener.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JosephAtNXP_0-1731351100866.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/309832i055A29C2B8ADA4B1/image-size/large?v=v2&amp;amp;px=999" role="button" title="JosephAtNXP_0-1731351100866.png" alt="JosephAtNXP_0-1731351100866.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 11 Nov 2024 18:51:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AVB-Demos-AVDECC-entity-definition-create-custom/m-p/1992186#M230733</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-11-11T18:51:56Z</dc:date>
    </item>
    <item>
      <title>Re: AVB Demos, AVDECC entity definition, create custom</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AVB-Demos-AVDECC-entity-definition-create-custom/m-p/1992902#M230768</link>
      <description>&lt;P&gt;Hi, Joseph,&lt;/P&gt;&lt;P&gt;Thanks for responding.&amp;nbsp; Have you tried what you're suggesting?&amp;nbsp; When I run the Hive controller, I can see the configurations, and the Dynamic Info-&amp;gt;Stream Format, but I cannot change the stream format.&amp;nbsp; The only selection offered is the one that is set.&amp;nbsp; For demo #22, that's AAF, 48kHz, PCM-INT-32, 2 channels.&amp;nbsp; I was hoping to configure a profile as having an 8 channel stream, rather than 4 streams of 2 channels (or, in the case of profile #22, 2 streams of 2 channels).&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Having said that, I have been able to configure ALSA's plug-ins to divide my 8 channel device into 4 2-channel devices, and they work, at least with aplay and arecord.&amp;nbsp; When I use one of the pairs as the alsa device for this demo (#22 or #9/11), I get no errors that I recognize, but also no sound.&amp;nbsp; More precisely, I get no sound that is related to the signal being put into the alsa device.&amp;nbsp; When I make the connection in the Hive controller, I DO hear a faint high-pitched noise, so it's trying to do something.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've attached the /var/log/avb and /var/log/avb_media_app logs from the talker and listener in case someone can see something I cannot.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Nov 2024 14:21:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AVB-Demos-AVDECC-entity-definition-create-custom/m-p/1992902#M230768</guid>
      <dc:creator>jpa</dc:creator>
      <dc:date>2024-11-12T14:21:41Z</dc:date>
    </item>
  </channel>
</rss>