<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic u-boot splash screen (no command line messages) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-splash-screen-no-command-line-messages/m-p/1991148#M230685</link>
    <description>&lt;P&gt;hello guys,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am pretty new to this u-boot environment and customization and using i.mx 8mp board.&lt;/P&gt;&lt;P&gt;I need some inputs or help or some steps(actually elaborated) in order to create a minimal u-boot with custom splash screen(image on entire screen) with no command line logs while booting. I have this .bmp image which I have created by following some external links. but no idea how to proceed further from there.&lt;/P&gt;&lt;P&gt;Any help or inputs on this is highly appreciated as I know I am asking you guys a bigger chunk of help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anil Kumar&lt;/P&gt;</description>
    <pubDate>Fri, 08 Nov 2024 14:44:50 GMT</pubDate>
    <dc:creator>anilkandikonda</dc:creator>
    <dc:date>2024-11-08T14:44:50Z</dc:date>
    <item>
      <title>u-boot splash screen (no command line messages)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-splash-screen-no-command-line-messages/m-p/1991148#M230685</link>
      <description>&lt;P&gt;hello guys,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am pretty new to this u-boot environment and customization and using i.mx 8mp board.&lt;/P&gt;&lt;P&gt;I need some inputs or help or some steps(actually elaborated) in order to create a minimal u-boot with custom splash screen(image on entire screen) with no command line logs while booting. I have this .bmp image which I have created by following some external links. but no idea how to proceed further from there.&lt;/P&gt;&lt;P&gt;Any help or inputs on this is highly appreciated as I know I am asking you guys a bigger chunk of help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anil Kumar&lt;/P&gt;</description>
      <pubDate>Fri, 08 Nov 2024 14:44:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-splash-screen-no-command-line-messages/m-p/1991148#M230685</guid>
      <dc:creator>anilkandikonda</dc:creator>
      <dc:date>2024-11-08T14:44:50Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot splash screen (no command line messages)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-splash-screen-no-command-line-messages/m-p/1992922#M230771</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/240445"&gt;@anilkandikonda&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing very well.&lt;/P&gt;
&lt;P&gt;You can take a look to the&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13709.pdf" target="_self"&gt;AN13709&lt;/A&gt; that is about of&amp;nbsp;Linux Boot Time Optimizations for i.MX8M Family.&lt;/P&gt;
&lt;P&gt;In chapter 4 is mentioned the possible Bootloader optimizations.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope this information can helps to you.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Nov 2024 15:20:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-splash-screen-no-command-line-messages/m-p/1992922#M230771</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2024-11-12T15:20:13Z</dc:date>
    </item>
  </channel>
</rss>