<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 imx93 DSI send command fail in some case</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx93-DSI-send-command-fail-in-some-case/m-p/1988909#M230574</link>
    <description>&lt;P&gt;HI experts:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I got a problem when intergrade a mipi panel to imx93 board ,&amp;nbsp; the log is:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;"dw-mipi-dsi-imx 4ae10000.dsi:failed to write command FIFo"&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; and the function "mipi_dsi_device_transfer" return with error=-110.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;After more research,&amp;nbsp; and found that not all commands fail, but some command with too much parameters will fail, for example: the driver send the following commands:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jiangyaqiang_0-1730901400423.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/308956iE35FA41CA55D6E3B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jiangyaqiang_0-1730901400423.png" alt="jiangyaqiang_0-1730901400423.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;it will fail at command : 0xB4 , 0xD3, 0xD5 , 0xD6.&lt;/P&gt;&lt;P&gt;&amp;nbsp; If I don't send the commands failed, the panel can show picture , but the picture position is&amp;nbsp; &amp;nbsp;offset,&amp;nbsp; and I have confirmed the board is ok wit DSI TO HDMI,&amp;nbsp; and the panel is ok with imx8mini.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Dose anyone has any suggestion ?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Best Regards .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 06 Nov 2024 14:04:15 GMT</pubDate>
    <dc:creator>jiangyaqiang</dc:creator>
    <dc:date>2024-11-06T14:04:15Z</dc:date>
    <item>
      <title>imx93 DSI send command fail in some case</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-DSI-send-command-fail-in-some-case/m-p/1988909#M230574</link>
      <description>&lt;P&gt;HI experts:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I got a problem when intergrade a mipi panel to imx93 board ,&amp;nbsp; the log is:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;"dw-mipi-dsi-imx 4ae10000.dsi:failed to write command FIFo"&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; and the function "mipi_dsi_device_transfer" return with error=-110.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;After more research,&amp;nbsp; and found that not all commands fail, but some command with too much parameters will fail, for example: the driver send the following commands:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jiangyaqiang_0-1730901400423.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/308956iE35FA41CA55D6E3B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jiangyaqiang_0-1730901400423.png" alt="jiangyaqiang_0-1730901400423.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;it will fail at command : 0xB4 , 0xD3, 0xD5 , 0xD6.&lt;/P&gt;&lt;P&gt;&amp;nbsp; If I don't send the commands failed, the panel can show picture , but the picture position is&amp;nbsp; &amp;nbsp;offset,&amp;nbsp; and I have confirmed the board is ok wit DSI TO HDMI,&amp;nbsp; and the panel is ok with imx8mini.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Dose anyone has any suggestion ?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Best Regards .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 14:04:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-DSI-send-command-fail-in-some-case/m-p/1988909#M230574</guid>
      <dc:creator>jiangyaqiang</dc:creator>
      <dc:date>2024-11-06T14:04:15Z</dc:date>
    </item>
    <item>
      <title>Re: imx93 DSI send command fail in some case</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-DSI-send-command-fail-in-some-case/m-p/1989640#M230593</link>
      <description>&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;The DSI controller in i.MX93 is different from i.MX8MM.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Please refer Table 526. Error Cause and Recover&amp;nbsp; in i.MX93 RM. For pld_w_err, the controller can send such long packet at one time.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Zhiming_Liu_1-1730944309000.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/309047iDA0B9C60370E6A8A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Zhiming_Liu_1-1730944309000.png" alt="Zhiming_Liu_1-1730944309000.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please check with your panel vendor to see if you can split these long cmd lists.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Best Regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Zhiming&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Nov 2024 02:09:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-DSI-send-command-fail-in-some-case/m-p/1989640#M230593</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-11-07T02:09:23Z</dc:date>
    </item>
    <item>
      <title>Re: imx93 DSI send command fail in some case</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-DSI-send-command-fail-in-some-case/m-p/1990165#M230616</link>
      <description>&lt;P&gt;Hi Zhiming:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;And finally I found that add more timeout or don't send command in LPM will fix the problem.&lt;/P&gt;</description>
      <pubDate>Thu, 07 Nov 2024 11:57:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-DSI-send-command-fail-in-some-case/m-p/1990165#M230616</guid>
      <dc:creator>jiangyaqiang</dc:creator>
      <dc:date>2024-11-07T11:57:20Z</dc:date>
    </item>
  </channel>
</rss>