<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic running the /usr/bin binary using the systemd service. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/running-the-usr-bin-binary-using-the-systemd-service/m-p/1982961#M230186</link>
    <description>&lt;P&gt;Hi NXP Team,&lt;BR /&gt;&lt;BR /&gt;I want to run the binary with the help of service as soon as the device is booted and get the logs on the console prompt.&lt;BR /&gt;&lt;BR /&gt;For that, I've created the recipe and I can see that the service is enabled and also active but I don't get logs on the console.&lt;BR /&gt;&lt;BR /&gt;Use case of binary: The binary should print logs continuously on the console.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Could you please help me with this?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Mon, 28 Oct 2024 12:42:08 GMT</pubDate>
    <dc:creator>sbmd_1234</dc:creator>
    <dc:date>2024-10-28T12:42:08Z</dc:date>
    <item>
      <title>running the /usr/bin binary using the systemd service.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/running-the-usr-bin-binary-using-the-systemd-service/m-p/1982961#M230186</link>
      <description>&lt;P&gt;Hi NXP Team,&lt;BR /&gt;&lt;BR /&gt;I want to run the binary with the help of service as soon as the device is booted and get the logs on the console prompt.&lt;BR /&gt;&lt;BR /&gt;For that, I've created the recipe and I can see that the service is enabled and also active but I don't get logs on the console.&lt;BR /&gt;&lt;BR /&gt;Use case of binary: The binary should print logs continuously on the console.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Could you please help me with this?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Mon, 28 Oct 2024 12:42:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/running-the-usr-bin-binary-using-the-systemd-service/m-p/1982961#M230186</guid>
      <dc:creator>sbmd_1234</dc:creator>
      <dc:date>2024-10-28T12:42:08Z</dc:date>
    </item>
    <item>
      <title>Re: running the /usr/bin binary using the systemd service.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/running-the-usr-bin-binary-using-the-systemd-service/m-p/1983187#M230202</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229463"&gt;@sbmd_1234&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing very well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Enable-WIFI-on-Ubuntu-22-04-and-Linux-BSPs-in-iMX8-Family/ta-p/1665223" target="_self"&gt;here&lt;/A&gt; to the Step 1 and 2. There is mentioned how to make boot scripts to run a service while the device is running.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
      <pubDate>Mon, 28 Oct 2024 19:11:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/running-the-usr-bin-binary-using-the-systemd-service/m-p/1983187#M230202</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2024-10-28T19:11:13Z</dc:date>
    </item>
  </channel>
</rss>