<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What are Host1, 2, 3 and OTG2 in IMX_REFERENCE_MANUAL.pdf of imx8mm? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/What-are-Host1-2-3-and-OTG2-in-IMX-REFERENCE-MANUAL-pdf-of/m-p/1980756#M230080</link>
    <description>&lt;P&gt;The imx8mm have nothing to do with Hos1, 2 and 3?&lt;/P&gt;</description>
    <pubDate>Thu, 24 Oct 2024 04:14:40 GMT</pubDate>
    <dc:creator>takeshi100</dc:creator>
    <dc:date>2024-10-24T04:14:40Z</dc:date>
    <item>
      <title>What are Host1, 2, 3 and OTG2 in IMX_REFERENCE_MANUAL.pdf of imx8mm?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-are-Host1-2-3-and-OTG2-in-IMX-REFERENCE-MANUAL-pdf-of/m-p/1977944#M229906</link>
      <description>&lt;P&gt;What are Host1, 2, 3 and OTG2 in IMX_REFERENCE_MANUAL.pdf of imx8mm?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;【&lt;SPAN&gt;applicable parts&lt;/SPAN&gt;】&lt;/P&gt;&lt;P&gt;• High-speed Host Only core (Host1), high-speed, full speed, and low devices are supported&lt;BR /&gt;• High-speed Inter-Chip core (Host2 &amp;amp; Host3)&lt;BR /&gt;• High-speed Host Only core (OTG2), high-speed, full speed, and low devices are supported. A USB2Pci bridge&lt;BR /&gt;is connected to OTG2 by default. Therefore, users may not be able to connect other USB devices on this port.&lt;BR /&gt;• High-speed Inter-Chip core (Host2)&lt;/P&gt;</description>
      <pubDate>Mon, 21 Oct 2024 08:06:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-are-Host1-2-3-and-OTG2-in-IMX-REFERENCE-MANUAL-pdf-of/m-p/1977944#M229906</guid>
      <dc:creator>takeshi100</dc:creator>
      <dc:date>2024-10-21T08:06:49Z</dc:date>
    </item>
    <item>
      <title>Re: What are Host1, 2, 3 and OTG2 in IMX_REFERENCE_MANUAL.pdf of imx8mm?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-are-Host1-2-3-and-OTG2-in-IMX-REFERENCE-MANUAL-pdf-of/m-p/1980609#M230068</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There are two USB 2.0 controller cores in this chip:&lt;BR /&gt;• Controller Core 0 is also named 'OTG1 Core'; its connected port is named 'OTG1&lt;BR /&gt;port'.&lt;BR /&gt;• Controller Core 1 is also named 'OTG2 Core'; its connected port is named 'OTG2&lt;BR /&gt;port'.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For details, please refer to the Chapter 11 in the Reference Manual.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Oct 2024 01:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-are-Host1-2-3-and-OTG2-in-IMX-REFERENCE-MANUAL-pdf-of/m-p/1980609#M230068</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2024-10-24T01:27:29Z</dc:date>
    </item>
    <item>
      <title>Re: What are Host1, 2, 3 and OTG2 in IMX_REFERENCE_MANUAL.pdf of imx8mm?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-are-Host1-2-3-and-OTG2-in-IMX-REFERENCE-MANUAL-pdf-of/m-p/1980756#M230080</link>
      <description>&lt;P&gt;The imx8mm have nothing to do with Hos1, 2 and 3?&lt;/P&gt;</description>
      <pubDate>Thu, 24 Oct 2024 04:14:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-are-Host1-2-3-and-OTG2-in-IMX-REFERENCE-MANUAL-pdf-of/m-p/1980756#M230080</guid>
      <dc:creator>takeshi100</dc:creator>
      <dc:date>2024-10-24T04:14:40Z</dc:date>
    </item>
  </channel>
</rss>