<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックwriting an ALSA driver</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/writing-an-ALSA-driver/m-p/1980602#M230066</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I've been tasked with writing an ALSA soundcard driver for IMX8/Yocto build system. This isn't a tradidional driver which wraps an SAI port or controls a Hardware codec or other hardware but like a bridge which transfers audio from another domain in the system running under a hypervisor to the Linux world, where it can be used by LInux applications, saved/played back from files, etc.&lt;/P&gt;&lt;P&gt;I'm very new to Linux and IMX (but not to device programming and audio). I've found a "sound-dummy" example LInux driver which I'm working to probe and reverse-engineer but I wondered if there were any documentation or examples specifically for the IMX? (I've tried the search engine but haven't turned up much, except for the SAI port wrapper)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Thu, 24 Oct 2024 01:14:33 GMT</pubDate>
    <dc:creator>sgordon777</dc:creator>
    <dc:date>2024-10-24T01:14:33Z</dc:date>
    <item>
      <title>writing an ALSA driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/writing-an-ALSA-driver/m-p/1980602#M230066</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I've been tasked with writing an ALSA soundcard driver for IMX8/Yocto build system. This isn't a tradidional driver which wraps an SAI port or controls a Hardware codec or other hardware but like a bridge which transfers audio from another domain in the system running under a hypervisor to the Linux world, where it can be used by LInux applications, saved/played back from files, etc.&lt;/P&gt;&lt;P&gt;I'm very new to Linux and IMX (but not to device programming and audio). I've found a "sound-dummy" example LInux driver which I'm working to probe and reverse-engineer but I wondered if there were any documentation or examples specifically for the IMX? (I've tried the search engine but haven't turned up much, except for the SAI port wrapper)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 24 Oct 2024 01:14:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/writing-an-ALSA-driver/m-p/1980602#M230066</guid>
      <dc:creator>sgordon777</dc:creator>
      <dc:date>2024-10-24T01:14:33Z</dc:date>
    </item>
  </channel>
</rss>