<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Failed to Start Network Configuration on iMX8MP in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-Start-Network-Configuration-on-iMX8MP/m-p/1980384#M230056</link>
    <description>&lt;P&gt;Hi Clay,&lt;/P&gt;&lt;P&gt;Thanks for the follow up. Unfortunately neither using the generic target nor setting up a clean environment worked. Could I be missing something in the process? Or perhaps there is something wrong with the board I have?&lt;/P&gt;&lt;P&gt;I now completely deleted the directory with my Yocto environment and set a fresh one up, using the latest scarthgap manifest (repo init -u &lt;A href="https://github.com/nxp-imx/imx-manifest" target="_blank"&gt;https://github.com/nxp-imx/imx-manifest&lt;/A&gt; -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml) and target&amp;nbsp;imx8mp-lpddr4-evk (MACHINE=imx8mp-lpddr4-evk DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh -b bld-xwayland).&lt;/P&gt;&lt;P&gt;The build succeeds (bitbake imx-image-core), but when I run the device it once again doesn't show any network interface.&lt;/P&gt;&lt;PRE&gt;root@imx8mp-lpddr4-evk:~# ifconfig&lt;BR /&gt;lo Link encap:Local Loopback&lt;BR /&gt;inet addr:127.0.0.1 Mask:255.0.0.0&lt;BR /&gt;inet6 addr: ::1/128 Scope:Host&lt;BR /&gt;UP LOOPBACK RUNNING MTU:65536 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;I attached a log file with all the boot messages, in case that can be helpful.&lt;/P&gt;&lt;P&gt;Thank you for the support,&lt;BR /&gt;Alex&lt;/P&gt;</description>
    <pubDate>Wed, 23 Oct 2024 17:13:25 GMT</pubDate>
    <dc:creator>amosercq</dc:creator>
    <dc:date>2024-10-23T17:13:25Z</dc:date>
    <item>
      <title>Failed to Start Network Configuration on iMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-Start-Network-Configuration-on-iMX8MP/m-p/1964586#M229133</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am having issues connecting my iMX8MP-EVK to the network when using a Yocto build. In particular, when booting the board the console output prints several FAILED operations (most of them are repeated and I only included one for each below):&lt;/P&gt;&lt;PRE&gt;Starting Network Name Resolution...&lt;BR /&gt;[FAILED] Failed to start Network Time Synchronization.&lt;BR /&gt;See 'systemctl status systemd-timesyncd.service' for details.&lt;BR /&gt;[FAILED] Failed to start Network Name Resolution.&lt;BR /&gt;See 'systemctl status systemd-resolved.service' for details.&lt;BR /&gt; Starting Network Configuration...&lt;BR /&gt;[FAILED] Failed to start Avahi mDNS/DNS-SD Stack.&lt;BR /&gt;See 'systemctl status avahi-daemon.service' for details.&lt;BR /&gt;[ OK ] Started Telephony service.&lt;BR /&gt;[FAILED] Failed to start Network Configuration.&lt;BR /&gt;See 'systemctl status systemd-networkd.service' for details.&lt;BR /&gt;[DEPEND] Dependency failed for Wait for Network to be Configured.&lt;/PRE&gt;&lt;P&gt;I originally blamed it on the fact that I was using an older nanbield environment, so decided to update to scarthgap, but unfortunately that didn't resolve the issue.&lt;/P&gt;&lt;P&gt;So far I have tried both the 6.6.23 and 6.6.36 releases, with the same result (I even tried the imx-image-multimedia and imx-image-full recipes). Interestingly, if I use the pre-built image downloadable from the website&amp;nbsp;(&lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=L6.6.36_2.1.0_MX8MP&amp;amp;appType=file1&amp;amp;DOWNLOAD_ID=null" target="_self"&gt;L6.6.36_2.1.0_MX8MP&lt;/A&gt;) there doesn't seem to be any issues.&lt;/P&gt;&lt;P&gt;Checking the status of the systemd services shows the following:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;systemd-networkd&lt;/STRONG&gt;&lt;/P&gt;&lt;PRE&gt;root@imx8mp-lpddr4-evk:~# systemctl status systemd-networkd.service&lt;BR /&gt;x systemd-networkd.service - Network Configuration&lt;BR /&gt;Loaded: loaded (/usr/lib/systemd/system/systemd-networkd.service; enabled; preset: enabled)&lt;BR /&gt;Active: failed (Result: exit-code) since Tue 2024-02-27 17:26:11 UTC; 23s ago&lt;BR /&gt;TriggeredBy: x systemd-networkd.socket&lt;BR /&gt;Docs: man:systemd-networkd.service(8)&lt;BR /&gt;man:org.freedesktop.network1(5)&lt;BR /&gt;Process: 785 ExecStart=/usr/lib/systemd/systemd-networkd (code=exited, status=203/EXEC)&lt;BR /&gt;Main PID: 785 (code=exited, status=203/EXEC)&lt;BR /&gt;FD Store: 0 (limit: 512)&lt;BR /&gt;CPU: 74ms&lt;BR /&gt;Feb 27 17:26:11 imx8mp-lpddr4-evk systemd[1]: systemd-networkd.service: Scheduled restart job, restart counter is at 5.&lt;BR /&gt;Feb 27 17:26:11 imx8mp-lpddr4-evk systemd[1]: systemd-networkd.service: Start request repeated too quickly.&lt;BR /&gt;Feb 27 17:26:11 imx8mp-lpddr4-evk systemd[1]: systemd-networkd.service: Failed with result 'exit-code'.&lt;BR /&gt;Feb 27 17:26:11 imx8mp-lpddr4-evk systemd[1]: Failed to start Network Configuration.&lt;/PRE&gt;&lt;P&gt;&lt;STRONG&gt;systemd-resolved&lt;/STRONG&gt;&lt;/P&gt;&lt;PRE&gt;root@imx8mp-lpddr4-evk:~# systemctl status systemd-resolved.service&lt;BR /&gt;x systemd-resolved.service - Network Name Resolution&lt;BR /&gt;Loaded: loaded (/usr/lib/systemd/system/systemd-resolved.service; enabled; preset: enabled)&lt;BR /&gt;Active: failed (Result: exit-code) since Tue 2024-02-27 17:26:09 UTC; 20min ago&lt;BR /&gt;Docs: man:systemd-resolved.service(8)&lt;BR /&gt;man:org.freedesktop.resolve1(5)&lt;BR /&gt;https://www.freedesktop.org/wiki/Software/systemd/writing-network-configuration-managers&lt;BR /&gt;https://www.freedesktop.org/wiki/Software/systemd/writing-resolver-clients&lt;BR /&gt;Process: 688 ExecStart=/usr/lib/systemd/systemd-resolved (code=exited, status=203/EXEC)&lt;BR /&gt;Main PID: 688 (code=exited, status=203/EXEC)&lt;BR /&gt;CPU: 114ms&lt;BR /&gt;&lt;BR /&gt;Feb 27 17:26:09 imx8mp-lpddr4-evk systemd[1]: systemd-resolved.service: Scheduled restart job, restart counter is at 5.&lt;BR /&gt;Feb 27 17:26:09 imx8mp-lpddr4-evk systemd[1]: systemd-resolved.service: Start request repeated too quickly.&lt;BR /&gt;Feb 27 17:26:09 imx8mp-lpddr4-evk systemd[1]: systemd-resolved.service: Failed with result 'exit-code'.&lt;BR /&gt;Feb 27 17:26:09 imx8mp-lpddr4-evk systemd[1]: Failed to start Network Name Resolution.&lt;/PRE&gt;&lt;P&gt;&lt;STRONG&gt;systemd-timesyncd&lt;/STRONG&gt;&lt;/P&gt;&lt;PRE&gt;root@imx8mp-lpddr4-evk:~# systemctl status systemd-timesyncd.service&lt;BR /&gt;x systemd-timesyncd.service - Network Time Synchronization&lt;BR /&gt;Loaded: loaded (/usr/lib/systemd/system/systemd-timesyncd.service; enabled; preset: enabled)&lt;BR /&gt;Active: failed (Result: exit-code) since Tue 2024-02-27 17:26:08 UTC; 20min ago&lt;BR /&gt;Docs: man:systemd-timesyncd.service(8)&lt;BR /&gt;Process: 484 ExecStart=/usr/lib/systemd/systemd-timesyncd (code=exited, status=203/EXEC)&lt;BR /&gt;Main PID: 484 (code=exited, status=203/EXEC)&lt;BR /&gt;CPU: 117ms&lt;BR /&gt;&lt;BR /&gt;Feb 27 17:26:08 imx8mp-lpddr4-evk systemd[1]: systemd-timesyncd.service: Scheduled restart job, restart counter is at 5.&lt;BR /&gt;Feb 27 17:26:08 imx8mp-lpddr4-evk systemd[1]: systemd-timesyncd.service: Start request repeated too quickly.&lt;BR /&gt;Feb 27 17:26:08 imx8mp-lpddr4-evk systemd[1]: systemd-timesyncd.service: Failed with result 'exit-code'.&lt;BR /&gt;Feb 27 17:26:08 imx8mp-lpddr4-evk systemd[1]: Failed to start Network Time Synchronization.&lt;BR /&gt;Feb 27 17:26:08 imx8mp-lpddr4-evk systemd[1]: systemd-timesyncd.service: Start request repeated too quickly.&lt;BR /&gt;Feb 27 17:26:08 imx8mp-lpddr4-evk systemd[1]: systemd-timesyncd.service: Failed with result 'exit-code'.&lt;BR /&gt;Feb 27 17:26:08 imx8mp-lpddr4-evk systemd[1]: Failed to start Network Time Synchronization.&lt;BR /&gt;Feb 27 17:26:09 imx8mp-lpddr4-evk systemd[1]: systemd-timesyncd.service: Start request repeated too quickly.&lt;BR /&gt;Feb 27 17:26:09 imx8mp-lpddr4-evk systemd[1]: systemd-timesyncd.service: Failed with result 'exit-code'.&lt;BR /&gt;Feb 27 17:26:09 imx8mp-lpddr4-evk systemd[1]: Failed to start Network Time Synchronization.&lt;/PRE&gt;&lt;P&gt;Finally, if I check the logs for networkd:&lt;/P&gt;&lt;PRE&gt;root@imx8mp-lpddr4-evk:~# journalctl -u systemd-networkd&lt;BR /&gt;Feb 27 17:26:10 imx8mp-lpddr4-evk systemd[1]: Starting Network Configuration...&lt;BR /&gt;Feb 27 17:26:10 imx8mp-lpddr4-evk (networkd)[737]: systemd-networkd.service: Failed to execute /usr/lib/systemd/systemd-networkd: Permission denied&lt;BR /&gt;Feb 27 17:26:10 imx8mp-lpddr4-evk systemd[1]: systemd-networkd.service: Main process exited, code=exited, status=203/EXEC&lt;BR /&gt;Feb 27 17:26:10 imx8mp-lpddr4-evk systemd[1]: systemd-networkd.service: Failed with result 'exit-code'.&lt;BR /&gt;Feb 27 17:26:10 imx8mp-lpddr4-evk systemd[1]: Failed to start Network Configuration.&lt;BR /&gt;Feb 27 17:26:10 imx8mp-lpddr4-evk systemd[1]: systemd-networkd.service: Scheduled restart job, restart counter is at 1.&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;Any idea why this might happen? I have followed the instructions from the imx-manifest repo (&lt;A href="https://github.com/nxp-imx/imx-manifest/tree/imx-linux-scarthgap" target="_blank" rel="noopener"&gt;nxp-imx/imx-manifest: i.MX Release Manifest (github.com)&lt;/A&gt;) (with MACHINE=imx8mp-lpddr4-evk).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help would be greatly appreciated, many thanks!&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;</description>
      <pubDate>Mon, 30 Sep 2024 15:49:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-Start-Network-Configuration-on-iMX8MP/m-p/1964586#M229133</guid>
      <dc:creator>amosercq</dc:creator>
      <dc:date>2024-09-30T15:49:01Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to Start Network Configuration on iMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-Start-Network-Configuration-on-iMX8MP/m-p/1964753#M229146</link>
      <description>&lt;P&gt;Hi Alex,&lt;/P&gt;
&lt;P&gt;I'll try to reproduce this behavior and get back to you.&lt;/P&gt;
&lt;P&gt;In the mean time I have a few questions:&lt;/P&gt;
&lt;P&gt;Did you make any edits to your Yocto build?&lt;/P&gt;
&lt;P&gt;Do any of the network interfaces show up?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Clay&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Sep 2024 20:41:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-Start-Network-Configuration-on-iMX8MP/m-p/1964753#M229146</guid>
      <dc:creator>clay_miller</dc:creator>
      <dc:date>2024-09-30T20:41:14Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to Start Network Configuration on iMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-Start-Network-Configuration-on-iMX8MP/m-p/1965002#M229162</link>
      <description>&lt;P&gt;Hi Clay,&lt;/P&gt;&lt;P&gt;thanks for the quick reply.&lt;/P&gt;&lt;P&gt;I didn't modify the build, the only edit I made is adding the following to local.conf:&lt;/P&gt;&lt;PRE&gt;PARALLEL_MAKE = "-j 2"&lt;BR /&gt;BB_NUMBER_THREADS = "2"&lt;/PRE&gt;&lt;P&gt;Interestingly, none of the network interfaces seem to be showing up when running ifconfig (other than the loopback).&lt;/P&gt;</description>
      <pubDate>Tue, 01 Oct 2024 07:22:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-Start-Network-Configuration-on-iMX8MP/m-p/1965002#M229162</guid>
      <dc:creator>amosercq</dc:creator>
      <dc:date>2024-10-01T07:22:45Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to Start Network Configuration on iMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-Start-Network-Configuration-on-iMX8MP/m-p/1970028#M229453</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/176732"&gt;@clay_miller&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;have you had a chance to replicate this?&lt;/P&gt;</description>
      <pubDate>Wed, 09 Oct 2024 14:08:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-Start-Network-Configuration-on-iMX8MP/m-p/1970028#M229453</guid>
      <dc:creator>amosercq</dc:creator>
      <dc:date>2024-10-09T14:08:21Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to Start Network Configuration on iMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-Start-Network-Configuration-on-iMX8MP/m-p/1974586#M229721</link>
      <description>Hi Alex,&lt;BR /&gt;I ran into several build issues when using the machine target imx8mp-lpddr4-evk. I'm thinking this target may not have gotten all then package updates yet for the newer releases, and might not be pointing to the relevant dts files to configure the Ethernet interfaces.&lt;BR /&gt;Try building for the machine target "imx8mpevk" to see if your Ethernet interfaces and phy setup correctly. You can build for core-image-minimal to quickly test the interfaces, but I don't think it comes with a presetup network service.&lt;BR /&gt;Regards,&lt;BR /&gt;Clay</description>
      <pubDate>Tue, 15 Oct 2024 20:08:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-Start-Network-Configuration-on-iMX8MP/m-p/1974586#M229721</guid>
      <dc:creator>clay_miller</dc:creator>
      <dc:date>2024-10-15T20:08:26Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to Start Network Configuration on iMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-Start-Network-Configuration-on-iMX8MP/m-p/1980261#M230053</link>
      <description>Hi Alex,&lt;BR /&gt;Just following up in case that alternate/generic target didn't work. After resolving my own build issues, the target machine imx8mp-lpddr4-evk with the core-image-minimal recipe can successfully start up a network service  with both eth0 and eth1 links up. I suggest performing a clean build to trigger Yocto to rebuild all packages.&lt;BR /&gt;&lt;BR /&gt;I didn't get a chance to confirm with the imx-image-multimedia and imx-image-full recipes as those take much longer to build. Let me know if the issue persists.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Clay</description>
      <pubDate>Wed, 23 Oct 2024 14:09:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-Start-Network-Configuration-on-iMX8MP/m-p/1980261#M230053</guid>
      <dc:creator>clay_miller</dc:creator>
      <dc:date>2024-10-23T14:09:05Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to Start Network Configuration on iMX8MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-Start-Network-Configuration-on-iMX8MP/m-p/1980384#M230056</link>
      <description>&lt;P&gt;Hi Clay,&lt;/P&gt;&lt;P&gt;Thanks for the follow up. Unfortunately neither using the generic target nor setting up a clean environment worked. Could I be missing something in the process? Or perhaps there is something wrong with the board I have?&lt;/P&gt;&lt;P&gt;I now completely deleted the directory with my Yocto environment and set a fresh one up, using the latest scarthgap manifest (repo init -u &lt;A href="https://github.com/nxp-imx/imx-manifest" target="_blank"&gt;https://github.com/nxp-imx/imx-manifest&lt;/A&gt; -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml) and target&amp;nbsp;imx8mp-lpddr4-evk (MACHINE=imx8mp-lpddr4-evk DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh -b bld-xwayland).&lt;/P&gt;&lt;P&gt;The build succeeds (bitbake imx-image-core), but when I run the device it once again doesn't show any network interface.&lt;/P&gt;&lt;PRE&gt;root@imx8mp-lpddr4-evk:~# ifconfig&lt;BR /&gt;lo Link encap:Local Loopback&lt;BR /&gt;inet addr:127.0.0.1 Mask:255.0.0.0&lt;BR /&gt;inet6 addr: ::1/128 Scope:Host&lt;BR /&gt;UP LOOPBACK RUNNING MTU:65536 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;I attached a log file with all the boot messages, in case that can be helpful.&lt;/P&gt;&lt;P&gt;Thank you for the support,&lt;BR /&gt;Alex&lt;/P&gt;</description>
      <pubDate>Wed, 23 Oct 2024 17:13:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-Start-Network-Configuration-on-iMX8MP/m-p/1980384#M230056</guid>
      <dc:creator>amosercq</dc:creator>
      <dc:date>2024-10-23T17:13:25Z</dc:date>
    </item>
  </channel>
</rss>