<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: eNET pins gets no voltage in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/eNET-pins-gets-no-voltage/m-p/1979290#M229984</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You better try the 6.6.36 BSP since the enet in this version change is better to have the latest one.&lt;/P&gt;
&lt;P&gt;Regards&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 22 Oct 2024 13:57:22 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-10-22T13:57:22Z</dc:date>
    <item>
      <title>eNET pins gets no voltage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eNET-pins-gets-no-voltage/m-p/1978224#M229916</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am using IMX8MM with 5.4.70 kernel version. I am trying to toggle ENET_TD2, ENET_RD2, ENET_RD3 as general gpios. I have configured them as&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;    pinctrl_temp: temp2 {
        fsl,pins = &amp;lt;
            MX8MM_IOMUXC_ENET_RD2_GPIO1_IO28      0x00000140 
            MX8MM_IOMUXC_ENET_RD3_GPIO1_IO29      0x00000160
            MX8MM_IOMUXC_ENET_TD2_GPIO1_IO19      0x00000160 
        &amp;gt;;
    }; &lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;below. When I try to toggle them through "/sys/class/gpio" but no voltage variation on pins. While I configure to use NAND_CE0_B as follow&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;    pinctrl_gpio_led1: gpioledgrp1 {
        fsl,pins = &amp;lt;
            MX8MM_IOMUXC_NAND_CE0_B_GPIO3_IO1   0x140
        &amp;gt;;
    };&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I able to see toggle voltages on oscilloscope. My toggle script is as follow:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;#!/bin/bash

echo "Performing GPIO PIN configuration"
cd /sys/class/gpio

# Set gpios
echo 28 &amp;gt; export
echo 19 &amp;gt; export
echo 29 &amp;gt; export
echo 65 &amp;gt; export
echo out &amp;gt; gpio28/direction
echo out &amp;gt; gpio19/direction
echo out &amp;gt; gpio65/direction
echo out &amp;gt; gpio29/direction
while true;
do
    echo "Enabling Reset low"

    echo 0 &amp;gt; gpio28/value
    echo 0 &amp;gt; gpio19/value
    echo 0 &amp;gt; gpio29/value
    echo 0 &amp;gt; gpio65/value
    sleep 1
    echo "Enabling Reset high"
    echo 1 &amp;gt; gpio28/value
    echo 1 &amp;gt; gpio19/value
    echo 1 &amp;gt; gpio29/value
    echo 1 &amp;gt; gpio65/value
    sleep 1
done&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone help me with this?&lt;/P&gt;&lt;P&gt;#IMX8MM&amp;nbsp; #GPIO&amp;nbsp; #IMX8&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ajita&lt;/P&gt;</description>
      <pubDate>Mon, 21 Oct 2024 11:57:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eNET-pins-gets-no-voltage/m-p/1978224#M229916</guid>
      <dc:creator>ajita02</dc:creator>
      <dc:date>2024-10-21T11:57:44Z</dc:date>
    </item>
    <item>
      <title>Re: eNET pins gets no voltage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eNET-pins-gets-no-voltage/m-p/1979290#M229984</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You better try the 6.6.36 BSP since the enet in this version change is better to have the latest one.&lt;/P&gt;
&lt;P&gt;Regards&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Oct 2024 13:57:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eNET-pins-gets-no-voltage/m-p/1979290#M229984</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-10-22T13:57:22Z</dc:date>
    </item>
  </channel>
</rss>