<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX7D HAB required for OPTEE? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-HAB-required-for-OPTEE/m-p/1979033#M229977</link>
    <description>Adding examples was not the question. I asked if I need to enable High assurance boot on nxp processors to use the OPTEE Feature.</description>
    <pubDate>Tue, 22 Oct 2024 08:50:57 GMT</pubDate>
    <dc:creator>marcer1</dc:creator>
    <dc:date>2024-10-22T08:50:57Z</dc:date>
    <item>
      <title>IMX7D HAB required for OPTEE?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-HAB-required-for-OPTEE/m-p/1973340#M229639</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I would like to install OPTEE on an IMX7D or an IMX8X. Do I really have to enable HAB to use OPTEE? My Project is student preliminary work, so it would be okay if the system is not completly secure, as long as i document it.&lt;BR /&gt;But I don't know if it's a prerequisite of optee to have HAB and SecureBoot running to use it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you so much,&lt;/P&gt;&lt;P&gt;marcer1&lt;/P&gt;</description>
      <pubDate>Mon, 14 Oct 2024 12:22:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-HAB-required-for-OPTEE/m-p/1973340#M229639</guid>
      <dc:creator>marcer1</dc:creator>
      <dc:date>2024-10-14T12:22:04Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D HAB required for OPTEE?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-HAB-required-for-OPTEE/m-p/1974357#M229710</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;With yocto&lt;/P&gt;
&lt;P&gt;Add to your &lt;CODE&gt;local.conf&lt;/CODE&gt;:&lt;/P&gt;
&lt;PRE&gt;&lt;CODE&gt;IMAGE_INSTALL_append = " optee-examples"
&lt;/CODE&gt;&lt;/PRE&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;In future how to add my own trusted applications to Yocto.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Create a recipe based on &lt;CODE&gt;recipes-security/optee/optee-examples.bb&lt;/CODE&gt; and add it to the image as stated above.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 15 Oct 2024 14:11:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-HAB-required-for-OPTEE/m-p/1974357#M229710</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-10-15T14:11:13Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D HAB required for OPTEE?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-HAB-required-for-OPTEE/m-p/1979033#M229977</link>
      <description>Adding examples was not the question. I asked if I need to enable High assurance boot on nxp processors to use the OPTEE Feature.</description>
      <pubDate>Tue, 22 Oct 2024 08:50:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-HAB-required-for-OPTEE/m-p/1979033#M229977</guid>
      <dc:creator>marcer1</dc:creator>
      <dc:date>2024-10-22T08:50:57Z</dc:date>
    </item>
  </channel>
</rss>