<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX8QM HARDWARE H264 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1978230#M229917</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In the "i.MX 8 GStreamer User Guide" PDF, it is stated that the hardware H.264 capabilities vpuenc_h264 and vpudec can be implemented. However, these features are not present in the GStreamer library. How should I configure the Yocto project to enable these hardware features? Currently, we are using the v4l2h265dec and v4l2h265enc codecs, but we are experiencing issues with high-resolution video using these plugins. How can I add the vpuenc_h264 and vpudec GStreamer plugins to the Yocto project for the i.MX 8QM?&lt;/P&gt;</description>
    <pubDate>Mon, 21 Oct 2024 12:01:41 GMT</pubDate>
    <dc:creator>HAKANAYDN</dc:creator>
    <dc:date>2024-10-21T12:01:41Z</dc:date>
    <item>
      <title>IMX8QM HARDWARE H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1978230#M229917</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In the "i.MX 8 GStreamer User Guide" PDF, it is stated that the hardware H.264 capabilities vpuenc_h264 and vpudec can be implemented. However, these features are not present in the GStreamer library. How should I configure the Yocto project to enable these hardware features? Currently, we are using the v4l2h265dec and v4l2h265enc codecs, but we are experiencing issues with high-resolution video using these plugins. How can I add the vpuenc_h264 and vpudec GStreamer plugins to the Yocto project for the i.MX 8QM?&lt;/P&gt;</description>
      <pubDate>Mon, 21 Oct 2024 12:01:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1978230#M229917</guid>
      <dc:creator>HAKANAYDN</dc:creator>
      <dc:date>2024-10-21T12:01:41Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM HARDWARE H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1979310#M229990</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Which resolution do you want to decode? since Mx8QM support 4K @30 fps and videos work well in this resolution with gstreamer.&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Tue, 22 Oct 2024 14:10:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1979310#M229990</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-10-22T14:10:46Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM HARDWARE H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1979312#M229991</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Which resolution do you want to decode? since Mx8QM support 4K @30 fps and videos work well in this resolution with gstreamer.&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Tue, 22 Oct 2024 14:13:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1979312#M229991</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-10-22T14:13:55Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM HARDWARE H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1984100#M230262</link>
      <description>Hi.&lt;BR /&gt;Firstly, thank you alot. I want to design a voip phone. We need to encode and decode h264 feature using gstreamer. Please could you share gstream command how can I decode and encode a video captured from camera high resolution ? What do I need to configure Linux kernel, dts and imx GST plugins?</description>
      <pubDate>Tue, 29 Oct 2024 18:58:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1984100#M230262</guid>
      <dc:creator>HAKANAYDN</dc:creator>
      <dc:date>2024-10-29T18:58:09Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM HARDWARE H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1986276#M230377</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Download the latest BSP from nxp page, it includes all the features you want:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Nov 2024 12:40:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1986276#M230377</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-11-01T12:40:17Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM HARDWARE H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1991853#M230716</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Are vpudec and vpuenc_h264 plugin for gstreamer available in imx8qm SOC ? We are not seeing the vpudec and&amp;nbsp;vpuenc_h264 listed using gst-inspect. But we see&amp;nbsp;v4l2h264dec, v4l2h264enc. Which ones do I use for h264 encoding and decoding ? Which one is supported by hardware ?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Nov 2024 09:08:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1991853#M230716</guid>
      <dc:creator>HAKANAYDN</dc:creator>
      <dc:date>2024-11-11T09:08:56Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM HARDWARE H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1992871#M230762</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Please check:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Video-Encoding-capabilities-of-iMX8M/td-p/1335057" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Video-Encoding-capabilities-of-iMX8M/td-p/1335057&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Tue, 12 Nov 2024 13:47:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1992871#M230762</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-11-12T13:47:49Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QM HARDWARE H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1993348#M230794</link>
      <description>Hi&lt;BR /&gt;Thanks for replying. But I didnt see my solution that I ask.&lt;BR /&gt;&lt;BR /&gt;1) Are vpudec and vpuenc_h264 plugin for gstreamer available in imx8qm SOC ?&lt;BR /&gt;&lt;BR /&gt;We are not seeing the vpudec and vpuenc_h264 listed using gst-inspect. But we see v4l2h264dec, v4l2h264enc. Which ones do I use for h264 encoding and decoding ? Which one is supported by hardware ?</description>
      <pubDate>Wed, 13 Nov 2024 05:09:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QM-HARDWARE-H264/m-p/1993348#M230794</guid>
      <dc:creator>HAKANAYDN</dc:creator>
      <dc:date>2024-11-13T05:09:45Z</dc:date>
    </item>
  </channel>
</rss>