<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB BULK TRANSFER PROBLEM in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-BULK-TRANSFER-PROBLEM/m-p/1977583#M229889</link>
    <description>&lt;P&gt;HI every one&lt;BR /&gt;i have customized board based on i.mx6 dual lite&lt;BR /&gt;i am developing a bare metal USB ,ass storage protocol&lt;BR /&gt;Enumeration done successfully for my pen drive&lt;BR /&gt;base of Enumeration code taken from SDK and modified for MSD&lt;BR /&gt;SCSI protocol related code taken from u-boot&lt;BR /&gt;it has COMMAND PHASE, DATA PHASE and STATUS PHASE&lt;BR /&gt;i am not controlling port power through GPIO, instead connected directly to POWER&lt;BR /&gt;COMMAND PAHSE transaction processed successfully&lt;BR /&gt;DATA PHASE, i am getting token=0x01F38D08&lt;BR /&gt;when i refer reference manual, it is transaction error&lt;BR /&gt;what could be the issue&lt;BR /&gt;can any one help in this regard&lt;BR /&gt;i am struggling lot&lt;BR /&gt;if required i shared the code&lt;BR /&gt;thanks and regards&lt;/P&gt;&lt;P&gt;Saida&lt;/P&gt;</description>
    <pubDate>Sun, 20 Oct 2024 18:29:08 GMT</pubDate>
    <dc:creator>saida</dc:creator>
    <dc:date>2024-10-20T18:29:08Z</dc:date>
    <item>
      <title>USB BULK TRANSFER PROBLEM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-BULK-TRANSFER-PROBLEM/m-p/1977583#M229889</link>
      <description>&lt;P&gt;HI every one&lt;BR /&gt;i have customized board based on i.mx6 dual lite&lt;BR /&gt;i am developing a bare metal USB ,ass storage protocol&lt;BR /&gt;Enumeration done successfully for my pen drive&lt;BR /&gt;base of Enumeration code taken from SDK and modified for MSD&lt;BR /&gt;SCSI protocol related code taken from u-boot&lt;BR /&gt;it has COMMAND PHASE, DATA PHASE and STATUS PHASE&lt;BR /&gt;i am not controlling port power through GPIO, instead connected directly to POWER&lt;BR /&gt;COMMAND PAHSE transaction processed successfully&lt;BR /&gt;DATA PHASE, i am getting token=0x01F38D08&lt;BR /&gt;when i refer reference manual, it is transaction error&lt;BR /&gt;what could be the issue&lt;BR /&gt;can any one help in this regard&lt;BR /&gt;i am struggling lot&lt;BR /&gt;if required i shared the code&lt;BR /&gt;thanks and regards&lt;/P&gt;&lt;P&gt;Saida&lt;/P&gt;</description>
      <pubDate>Sun, 20 Oct 2024 18:29:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-BULK-TRANSFER-PROBLEM/m-p/1977583#M229889</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2024-10-20T18:29:08Z</dc:date>
    </item>
    <item>
      <title>Re: USB BULK TRANSFER PROBLEM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-BULK-TRANSFER-PROBLEM/m-p/1978300#M229927</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The token=0x01F38D08 occurs when adding or removing another USB device or when the USB device has been used for an extended period of time. The error may occur within 30 minutes or after multiple days of usage before the device stops communicating. Resetting the device or restarting the task results in the same error.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;To solve the error, you can try the following tests:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;​Disconnect the USB cable, then reconnect it&lt;/LI&gt;
&lt;LI&gt;Remove power from the USB device, then reconnect it&lt;/LI&gt;
&lt;LI&gt;Try replacing or using another USB cable&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Is not error by software.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&lt;LI-WRAPPER&gt;&lt;/LI-WRAPPER&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Oct 2024 14:00:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-BULK-TRANSFER-PROBLEM/m-p/1978300#M229927</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-10-21T14:00:26Z</dc:date>
    </item>
  </channel>
</rss>