<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX8MQ gets too hot.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-gets-too-hot/m-p/1974429#M229716</link>
    <description>&lt;P&gt;It turned out to be that different power supplies resulted in wildly different temperatures.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 15 Oct 2024 15:58:40 GMT</pubDate>
    <dc:creator>synaption</dc:creator>
    <dc:date>2024-10-15T15:58:40Z</dc:date>
    <item>
      <title>IMX8MQ gets too hot.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-gets-too-hot/m-p/1686909#M209169</link>
      <description>&lt;DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;H1&gt;&lt;STRONG&gt;&lt;FONT size="2"&gt;My IMX8MQ based modules are running a bit hotter than I would like. They have a passive heat sink, but they are outside in a weatherproof enclosure. On the hottest days, some do get past the 95C thermal tipping point. I have lowered my cpu frequency to 1GHz (that helped a lot) and I have turned off two cores (that did not help much). I am constantly using two cores at ~60% load. Still, the modules runs about 20C hotter than a raspberry pi CM4 running similar code which I feel is a pretty comparable processor in terms of process node (28nm) and horespower (quad core, 1.5Ghz). What else can I do to get my temps down? I heard the latest IMX8 silicon revisions are supposed to run a lot cooler. Is that anybody elses experience? Mine are about a year old and are silicon revision B0. I'm running imx linux kernel version 5-15-lf if that matters.&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/H1&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 12 Jul 2023 22:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-gets-too-hot/m-p/1686909#M209169</guid>
      <dc:creator>synaption</dc:creator>
      <dc:date>2023-07-12T22:37:07Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MQ gets too hot.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-gets-too-hot/m-p/1687893#M209256</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;You can refer yourself to Reducing &lt;A href="https://www.nxp.com/docs/en/nxp/application-notes/AN12118.pdf" target="_self"&gt;Power Consumption&lt;/A&gt; and Chapter 6 Thermal Considerations from &lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX8MMHDG" target="_self"&gt;8M Mini Hardware Developers Guide&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jul 2023 20:46:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-gets-too-hot/m-p/1687893#M209256</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2023-07-13T20:46:11Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MQ gets too hot.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-gets-too-hot/m-p/1974429#M229716</link>
      <description>&lt;P&gt;It turned out to be that different power supplies resulted in wildly different temperatures.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Oct 2024 15:58:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-gets-too-hot/m-p/1974429#M229716</guid>
      <dc:creator>synaption</dc:creator>
      <dc:date>2024-10-15T15:58:40Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MQ gets too hot.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-gets-too-hot/m-p/2117751#M238303</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;May I know more about your possible solution?&lt;/P&gt;&lt;P&gt;I have an imx8m+ running hot as well and would like to know different considerations of decreasing the heat generated.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jun 2025 12:20:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-gets-too-hot/m-p/2117751#M238303</guid>
      <dc:creator>AL_186</dc:creator>
      <dc:date>2025-06-17T12:20:29Z</dc:date>
    </item>
  </channel>
</rss>