<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic xen in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/xen/m-p/1974384#M229714</link>
    <description>&lt;P&gt;By using UUU tool images are successfully flashed onto imx8qxp board and rebooted the board, the auto-boot is interrupted by pressing key and given &lt;STRONG&gt;$ run xenmmcboot &lt;/STRONG&gt;command in the boot environment. It accepted command loaded images but it bricked at starting kernel log are given below:&lt;/P&gt;&lt;P&gt;***************************************************************************************&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;U-Boot SPL 2020.04-5.4.24-2.1.0+g4979a99482f (Jun 24 2024 - 05:54:23 +0000)&lt;BR /&gt;Normal Boot&lt;BR /&gt;WDT: Not found!&lt;BR /&gt;Trying to boot from MMC2_2&lt;BR /&gt;Load image from MMC/SD 0x63c00&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2020.04-5.4.24-2.1.0+g4979a99482f (Jun 24 2024 - 05:54:23 +0000)&lt;/P&gt;&lt;P&gt;CPU: NXP i.MX8QXP RevC A35 at 1200 MHz at 27C&lt;/P&gt;&lt;P&gt;Model: NXP i.MX8QXP MEK&lt;BR /&gt;Board: iMX8QXP MEK&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- SCFW 4a1654e0, SECO-FW 376e3c15, IMX-MKIMAGE 6745ccdc, ATF b0a00f2&lt;BR /&gt;- U-Boot 2020.04-5.4.24-2.1.0+g4979a99482f&lt;/P&gt;&lt;P&gt;Boot: SD1&lt;BR /&gt;DRAM: 3 GiB&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Loading Environment from MMC... Run CMD11 1.8V switch&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0 (1280 x 720)&lt;BR /&gt;[0] dpu@56180000, video&lt;BR /&gt;[1] lvds-channel@0, display&lt;BR /&gt;[2] lvds-to-hdmi-bridge@4c, video_bridge&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;Net:&lt;BR /&gt;Warning: ethernet@5b040000 using MAC address from ROM&lt;BR /&gt;eth0: ethernet@5b040000 [PRIME]&lt;BR /&gt;Warning: ethernet@5b050000 (eth1) using random MAC address - 22:51:60:0f:43:75&lt;BR /&gt;, eth1: ethernet@5b050000&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;23163392 bytes read in 263 ms (84 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;WARN: Cannot load the DT&lt;BR /&gt;=&amp;gt; run xenmmcboot&lt;BR /&gt;83664 bytes read in 17 ms (4.7 MiB/s)&lt;BR /&gt;23163392 bytes read in 263 ms (84 MiB/s)&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt;Booting using the fdt blob at 0x83000000&lt;BR /&gt;Using Device Tree in place at 0000000083000000, end 0000000083017fff&lt;BR /&gt;Disable gpt0@5d140000, resource id 207 not owned&lt;BR /&gt;Disable jr3@40000, resource id 502 not owned&lt;BR /&gt;/dma-controller@591F0000, 62224&lt;BR /&gt;/dma-controller@599F0000, 63112&lt;BR /&gt;/dma-controller@5a1f0000, 61348&lt;BR /&gt;/dma-controller@5a1f0000, 61348&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;**********************************************************************************************&lt;/P&gt;&lt;P&gt;Also it showing&lt;STRONG&gt; "WARN: Cannot load the DT" &lt;/STRONG&gt;during general Linux booting what could be the reason for this?&lt;/P&gt;</description>
    <pubDate>Tue, 15 Oct 2024 14:51:48 GMT</pubDate>
    <dc:creator>yeswanth</dc:creator>
    <dc:date>2024-10-15T14:51:48Z</dc:date>
    <item>
      <title>xen</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/xen/m-p/1974384#M229714</link>
      <description>&lt;P&gt;By using UUU tool images are successfully flashed onto imx8qxp board and rebooted the board, the auto-boot is interrupted by pressing key and given &lt;STRONG&gt;$ run xenmmcboot &lt;/STRONG&gt;command in the boot environment. It accepted command loaded images but it bricked at starting kernel log are given below:&lt;/P&gt;&lt;P&gt;***************************************************************************************&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;U-Boot SPL 2020.04-5.4.24-2.1.0+g4979a99482f (Jun 24 2024 - 05:54:23 +0000)&lt;BR /&gt;Normal Boot&lt;BR /&gt;WDT: Not found!&lt;BR /&gt;Trying to boot from MMC2_2&lt;BR /&gt;Load image from MMC/SD 0x63c00&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2020.04-5.4.24-2.1.0+g4979a99482f (Jun 24 2024 - 05:54:23 +0000)&lt;/P&gt;&lt;P&gt;CPU: NXP i.MX8QXP RevC A35 at 1200 MHz at 27C&lt;/P&gt;&lt;P&gt;Model: NXP i.MX8QXP MEK&lt;BR /&gt;Board: iMX8QXP MEK&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- SCFW 4a1654e0, SECO-FW 376e3c15, IMX-MKIMAGE 6745ccdc, ATF b0a00f2&lt;BR /&gt;- U-Boot 2020.04-5.4.24-2.1.0+g4979a99482f&lt;/P&gt;&lt;P&gt;Boot: SD1&lt;BR /&gt;DRAM: 3 GiB&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Loading Environment from MMC... Run CMD11 1.8V switch&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0 (1280 x 720)&lt;BR /&gt;[0] dpu@56180000, video&lt;BR /&gt;[1] lvds-channel@0, display&lt;BR /&gt;[2] lvds-to-hdmi-bridge@4c, video_bridge&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;Net:&lt;BR /&gt;Warning: ethernet@5b040000 using MAC address from ROM&lt;BR /&gt;eth0: ethernet@5b040000 [PRIME]&lt;BR /&gt;Warning: ethernet@5b050000 (eth1) using random MAC address - 22:51:60:0f:43:75&lt;BR /&gt;, eth1: ethernet@5b050000&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;23163392 bytes read in 263 ms (84 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;WARN: Cannot load the DT&lt;BR /&gt;=&amp;gt; run xenmmcboot&lt;BR /&gt;83664 bytes read in 17 ms (4.7 MiB/s)&lt;BR /&gt;23163392 bytes read in 263 ms (84 MiB/s)&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt;Booting using the fdt blob at 0x83000000&lt;BR /&gt;Using Device Tree in place at 0000000083000000, end 0000000083017fff&lt;BR /&gt;Disable gpt0@5d140000, resource id 207 not owned&lt;BR /&gt;Disable jr3@40000, resource id 502 not owned&lt;BR /&gt;/dma-controller@591F0000, 62224&lt;BR /&gt;/dma-controller@599F0000, 63112&lt;BR /&gt;/dma-controller@5a1f0000, 61348&lt;BR /&gt;/dma-controller@5a1f0000, 61348&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;**********************************************************************************************&lt;/P&gt;&lt;P&gt;Also it showing&lt;STRONG&gt; "WARN: Cannot load the DT" &lt;/STRONG&gt;during general Linux booting what could be the reason for this?&lt;/P&gt;</description>
      <pubDate>Tue, 15 Oct 2024 14:51:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/xen/m-p/1974384#M229714</guid>
      <dc:creator>yeswanth</dc:creator>
      <dc:date>2024-10-15T14:51:48Z</dc:date>
    </item>
  </channel>
</rss>