<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB Mass Storage drivers in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-Mass-Storage-drivers/m-p/1973073#M229610</link>
    <description>&lt;P&gt;HI every one&lt;BR /&gt;i have customized board based on i.mx6 dual lite&lt;BR /&gt;i am developing a bare metal USB ,ass storage protocol&lt;BR /&gt;Enumeration done successfully for my pen drive&lt;BR /&gt;base of Enumeration code taken from SDK and modified for MSD&lt;BR /&gt;SCSI protocol related code taken from u-boot&lt;BR /&gt;it has COMMAND PHASE, DATA PHASE and STATUS PHASE&lt;BR /&gt;i am not controlling port power through GPIO, instead connected directly to POWER&lt;BR /&gt;COMMAND PAHSE transaction processed successfully&lt;BR /&gt;DATA PHASE, i am getting token=0x01F38D08&lt;BR /&gt;when i refer reference manual, it is transaction error&lt;BR /&gt;what could be the issue&lt;BR /&gt;can any one help in this regard&lt;BR /&gt;i am struggling lot&lt;BR /&gt;if required i shared the code&lt;BR /&gt;thanks and regards&lt;/P&gt;&lt;P&gt;Saida&lt;/P&gt;</description>
    <pubDate>Mon, 14 Oct 2024 07:22:58 GMT</pubDate>
    <dc:creator>saida</dc:creator>
    <dc:date>2024-10-14T07:22:58Z</dc:date>
    <item>
      <title>USB Mass Storage drivers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Mass-Storage-drivers/m-p/1545131#M196941</link>
      <description>&lt;P&gt;Hi&lt;BR /&gt;Can any one have USB mass storage drivers for i.mx6 board (baremetal)&lt;/P&gt;&lt;P&gt;please help me in this regard&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Oct 2022 15:34:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Mass-Storage-drivers/m-p/1545131#M196941</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2022-10-27T15:34:59Z</dc:date>
    </item>
    <item>
      <title>Re: USB Mass Storage drivers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Mass-Storage-drivers/m-p/1548218#M197156</link>
      <description>&lt;P&gt;It can support USB mass storage, what problem have you met, it maybe cause by the hardware problem.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Nov 2022 09:58:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Mass-Storage-drivers/m-p/1548218#M197156</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2022-11-03T09:58:56Z</dc:date>
    </item>
    <item>
      <title>IRe: USB Mass Storage drivers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Mass-Storage-drivers/m-p/1549237#M197234</link>
      <description>&lt;P&gt;I want source code for USB Mass storage device&lt;/P&gt;&lt;P&gt;SDK do not have example for mass storage, it has only key board and mouse examples&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Saida&lt;/P&gt;</description>
      <pubDate>Sun, 06 Nov 2022 14:46:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Mass-Storage-drivers/m-p/1549237#M197234</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2022-11-06T14:46:38Z</dc:date>
    </item>
    <item>
      <title>Re: USB Mass Storage drivers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Mass-Storage-drivers/m-p/1973073#M229610</link>
      <description>&lt;P&gt;HI every one&lt;BR /&gt;i have customized board based on i.mx6 dual lite&lt;BR /&gt;i am developing a bare metal USB ,ass storage protocol&lt;BR /&gt;Enumeration done successfully for my pen drive&lt;BR /&gt;base of Enumeration code taken from SDK and modified for MSD&lt;BR /&gt;SCSI protocol related code taken from u-boot&lt;BR /&gt;it has COMMAND PHASE, DATA PHASE and STATUS PHASE&lt;BR /&gt;i am not controlling port power through GPIO, instead connected directly to POWER&lt;BR /&gt;COMMAND PAHSE transaction processed successfully&lt;BR /&gt;DATA PHASE, i am getting token=0x01F38D08&lt;BR /&gt;when i refer reference manual, it is transaction error&lt;BR /&gt;what could be the issue&lt;BR /&gt;can any one help in this regard&lt;BR /&gt;i am struggling lot&lt;BR /&gt;if required i shared the code&lt;BR /&gt;thanks and regards&lt;/P&gt;&lt;P&gt;Saida&lt;/P&gt;</description>
      <pubDate>Mon, 14 Oct 2024 07:22:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Mass-Storage-drivers/m-p/1973073#M229610</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2024-10-14T07:22:58Z</dc:date>
    </item>
    <item>
      <title>Re: USB Mass Storage drivers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Mass-Storage-drivers/m-p/1977582#M229888</link>
      <description>hi&lt;BR /&gt;can you check my post regarding usb Bulk transfer</description>
      <pubDate>Sun, 20 Oct 2024 18:25:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Mass-Storage-drivers/m-p/1977582#M229888</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2024-10-20T18:25:03Z</dc:date>
    </item>
  </channel>
</rss>