<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: weston in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/weston/m-p/1971427#M229515</link>
    <description>Hi,&lt;BR /&gt;LVGL GUI configured at the position but we need to run 2nd application top of GUI LVGL application. 2nd app streaming the video by gstemer. but every new start it position change. we required to freeze the position of streaming on top of running LVGL Application.</description>
    <pubDate>Thu, 10 Oct 2024 14:21:27 GMT</pubDate>
    <dc:creator>gopal_rhsharma</dc:creator>
    <dc:date>2024-10-10T14:21:27Z</dc:date>
    <item>
      <title>weston</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/weston/m-p/1971274#M229503</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We r using Gui-guider application and need to run separate DMS app with size 160x160. we need to fix DMS APP position on window and run always top of the Gui-guider running app how it possible please Suggest or help.&lt;/P&gt;&lt;P&gt;working setup is:-&lt;/P&gt;&lt;P&gt;imx93evk-11x11&lt;/P&gt;&lt;P&gt;DISTRO=fsl-imx-xwayland MACHINE=imx93evk source imx-setup-release.sh -b build-xwayland&lt;/P&gt;&lt;P&gt;BSP 6.6.3&lt;/P&gt;&lt;P&gt;weston 12.0.3&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 10:19:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/weston/m-p/1971274#M229503</guid>
      <dc:creator>gopal_rhsharma</dc:creator>
      <dc:date>2024-10-10T10:19:09Z</dc:date>
    </item>
    <item>
      <title>Re: weston</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/weston/m-p/1971419#M229513</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;If you are working with LVGL you can configure the GUI at the position you want. please open the source code of the GUI.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 13:53:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/weston/m-p/1971419#M229513</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-10-10T13:53:48Z</dc:date>
    </item>
    <item>
      <title>Re: weston</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/weston/m-p/1971427#M229515</link>
      <description>Hi,&lt;BR /&gt;LVGL GUI configured at the position but we need to run 2nd application top of GUI LVGL application. 2nd app streaming the video by gstemer. but every new start it position change. we required to freeze the position of streaming on top of running LVGL Application.</description>
      <pubDate>Thu, 10 Oct 2024 14:21:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/weston/m-p/1971427#M229515</guid>
      <dc:creator>gopal_rhsharma</dc:creator>
      <dc:date>2024-10-10T14:21:27Z</dc:date>
    </item>
  </channel>
</rss>