<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flashing eMMC on iMX93 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/1968550#M229384</link>
    <description>Hi ! Thanks for your reply.&lt;BR /&gt;&lt;BR /&gt;Yes I boot with the SD card, then I just run a command like :&lt;BR /&gt;dd if=/mount/MyWicFile.wic of=/dev/mmcblk0&lt;BR /&gt;&lt;BR /&gt;When I make a binary dump to verify mmcblk0 it seems to be the same structure as the SD card, SPL starts at 0x8000 and FAT partition at 0x800000</description>
    <pubDate>Tue, 08 Oct 2024 06:29:28 GMT</pubDate>
    <dc:creator>vbal</dc:creator>
    <dc:date>2024-10-08T06:29:28Z</dc:date>
    <item>
      <title>Flashing eMMC on iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/1967411#M229310</link>
      <description>&lt;P&gt;&lt;BR /&gt;Hello !&lt;/P&gt;&lt;P&gt;I am currently working on a system that would be based on the i.MX93, I work with the&amp;nbsp;i.MX 93 Evaluation Kit for now, and I have two questions :&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&amp;nbsp;I can build the uboot bootloader and the .wic image with Yocto, flashing the wic on an SD card will work just fine, but if I flash the eMMC with dd , I will get several errors on dmesg, and the error&amp;nbsp;&lt;STRONG&gt;fsl-se-fw se-fw2: Command Id[205], Response Failure = 0x29&amp;nbsp;&lt;/STRONG&gt;continuously.&lt;BR /&gt;With UUU I don't get those issues, but my board will not have USB and only SD card for updates/maintenance. Is there a way to flash through SD card easily ?&lt;/LI&gt;&lt;LI&gt;On the Yocto side, I could build an image with only the Open Embedded meta, and meta-freescale.&lt;BR /&gt;Is meta-imx needed ?&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Thanks a lot !&lt;/P&gt;</description>
      <pubDate>Sun, 06 Oct 2024 03:54:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/1967411#M229310</guid>
      <dc:creator>vbal</dc:creator>
      <dc:date>2024-10-06T03:54:53Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing eMMC on iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/1968282#M229371</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241541"&gt;@vbal&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;How do you flash emmc with dd? boot into rootfs with SD card?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Oct 2024 01:44:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/1968282#M229371</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-10-08T01:44:26Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing eMMC on iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/1968550#M229384</link>
      <description>Hi ! Thanks for your reply.&lt;BR /&gt;&lt;BR /&gt;Yes I boot with the SD card, then I just run a command like :&lt;BR /&gt;dd if=/mount/MyWicFile.wic of=/dev/mmcblk0&lt;BR /&gt;&lt;BR /&gt;When I make a binary dump to verify mmcblk0 it seems to be the same structure as the SD card, SPL starts at 0x8000 and FAT partition at 0x800000</description>
      <pubDate>Tue, 08 Oct 2024 06:29:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/1968550#M229384</guid>
      <dc:creator>vbal</dc:creator>
      <dc:date>2024-10-08T06:29:28Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing eMMC on iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/1971121#M229493</link>
      <description>&lt;P&gt;Hi &lt;/P&gt;
&lt;P&gt;meta-imx is need, you better use or modify based on yocto project NXP release.&lt;/P&gt;
&lt;P&gt;I don't see same log when i use dd to flash mmc.&lt;BR /&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 07:41:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/1971121#M229493</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-10-10T07:41:08Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing eMMC on iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/1977483#M229879</link>
      <description>Thanks for your help !&lt;BR /&gt;&lt;BR /&gt;I followed the procedure in the Linux guide, but the image was too big and I wanted to start from scratch with only linux-fscl.&lt;BR /&gt;I will give a try with meta-imx so, did you use the guide procedure and then dd the .wic into the eMMC ?&lt;BR /&gt;&lt;BR /&gt;Interestingly, I tried buildroot and the kernel 6.6 creates the same issues with linux-imx as source, while 6.1 does not.&lt;BR /&gt;&lt;BR /&gt;Thanks a lot again</description>
      <pubDate>Sat, 19 Oct 2024 03:19:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/1977483#M229879</guid>
      <dc:creator>vbal</dc:creator>
      <dc:date>2024-10-19T03:19:31Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing eMMC on iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/1978875#M229965</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241541"&gt;@vbal&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;did you use the guide procedure and then dd the .wic into the eMMC ?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;--&amp;gt;Yes, dd the imx-image-core-xxx.wic file from SD card.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Tue, 22 Oct 2024 06:54:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/1978875#M229965</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-10-22T06:54:22Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing eMMC on iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/1980748#M230079</link>
      <description>I tested with the IMX_YOCTO_PROJECT_USERS_GUIDE procedure, and indeed it seems to work all fine.&lt;BR /&gt;&lt;BR /&gt;With only the meta-freescale layer, I used Poky as a distro, while I used fsl-imx-wayland here. Probably something is needed in the distro that I did not have before.&lt;BR /&gt;&lt;BR /&gt;I will start from there so, thanks a lot !</description>
      <pubDate>Thu, 24 Oct 2024 04:06:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/1980748#M230079</guid>
      <dc:creator>vbal</dc:creator>
      <dc:date>2024-10-24T04:06:55Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing eMMC on iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/2008243#M231606</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My answer arrives late but I just had the same error messages.&lt;/P&gt;&lt;P&gt;I solved it by unmounting mmcblk0 and 1 before using dd&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Dec 2024 13:44:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flashing-eMMC-on-iMX93/m-p/2008243#M231606</guid>
      <dc:creator>Frederic_Thierry_Adlink</dc:creator>
      <dc:date>2024-12-05T13:44:34Z</dc:date>
    </item>
  </channel>
</rss>