<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic question regarding npu profiling tools in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/question-regarding-npu-profiling-tools/m-p/1965483#M229195</link>
    <description>&lt;P&gt;Hello&lt;BR /&gt;&lt;BR /&gt;Right now I am curious on how the NPU profiling tools works. Is it possible to profile 2 or more models at the same time when we run a code where we use 2 or more models? if it is possible, what will the log looks like?&lt;BR /&gt;&lt;BR /&gt;also is it only limited to libvx_delegate.so only? or can we get the same profiler result if we run a code where it run using opencv cv::dnn::DNN_BACKEND_TIMVX?&lt;BR /&gt;&lt;BR /&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Wed, 02 Oct 2024 06:27:45 GMT</pubDate>
    <dc:creator>astel_</dc:creator>
    <dc:date>2024-10-02T06:27:45Z</dc:date>
    <item>
      <title>question regarding npu profiling tools</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/question-regarding-npu-profiling-tools/m-p/1965483#M229195</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;&lt;BR /&gt;Right now I am curious on how the NPU profiling tools works. Is it possible to profile 2 or more models at the same time when we run a code where we use 2 or more models? if it is possible, what will the log looks like?&lt;BR /&gt;&lt;BR /&gt;also is it only limited to libvx_delegate.so only? or can we get the same profiler result if we run a code where it run using opencv cv::dnn::DNN_BACKEND_TIMVX?&lt;BR /&gt;&lt;BR /&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Wed, 02 Oct 2024 06:27:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/question-regarding-npu-profiling-tools/m-p/1965483#M229195</guid>
      <dc:creator>astel_</dc:creator>
      <dc:date>2024-10-02T06:27:45Z</dc:date>
    </item>
    <item>
      <title>Re: question regarding npu profiling tools</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/question-regarding-npu-profiling-tools/m-p/1965710#M229213</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;No is not possible to profile two or more models in NPU and only is limited to libvx_delegate.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 02 Oct 2024 14:34:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/question-regarding-npu-profiling-tools/m-p/1965710#M229213</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-10-02T14:34:13Z</dc:date>
    </item>
    <item>
      <title>Re: question regarding npu profiling tools</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/question-regarding-npu-profiling-tools/m-p/1966043#M229228</link>
      <description>&lt;P&gt;thank you for your reply&lt;BR /&gt;&lt;BR /&gt;also can i ask, if imx support the&amp;nbsp;cv::dnn::DNN_BACKEND_TIMVX and&amp;nbsp;cv::dnn::DNN_TARGET_NPU to run inference in npu?&lt;BR /&gt;&lt;BR /&gt;bc i just read that opencv zoo model have this integration (&lt;A href="https://github.com/opencv/opencv/wiki/TIM-VX-Backend-For-Running-OpenCV-On-NPU" target="_self"&gt;link&lt;/A&gt;)&lt;/P&gt;</description>
      <pubDate>Thu, 03 Oct 2024 02:47:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/question-regarding-npu-profiling-tools/m-p/1966043#M229228</guid>
      <dc:creator>astel_</dc:creator>
      <dc:date>2024-10-03T02:47:12Z</dc:date>
    </item>
  </channel>
</rss>