<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic [IMX8ULPEVK] Decreasing Yocto Linux boot time in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8ULPEVK-Decreasing-Yocto-Linux-boot-time/m-p/1965378#M229187</link>
    <description>&lt;P&gt;Hello all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the IMX8ULP-EVK board for an embedded solution, where I need the boot time for linux to be very low (shooting for ~2 seconds), my application will involve booting the machine, doing meaningful work, and then turning off in a periodic cycle to decrease power consumption.&lt;/P&gt;&lt;P&gt;I am using Yocto Linux 6.6.23_2.0.0, and with the `core-image-minimal-dev` image, I am being taken to user login after about 12 seconds. Are there any guides I can follow to decrease the boot time? Are there any better images I can use that are more suitable for my application?&lt;BR /&gt;&lt;BR /&gt;I am currently working on removing features from the image, as well as cutting down the kernel features, however I fear this will not be enough (current 2 second kernel boot time and ~12 second systemd boot time). Any guidance would be much appreciated.&lt;/P&gt;</description>
    <pubDate>Tue, 01 Oct 2024 20:03:14 GMT</pubDate>
    <dc:creator>ksingh</dc:creator>
    <dc:date>2024-10-01T20:03:14Z</dc:date>
    <item>
      <title>[IMX8ULPEVK] Decreasing Yocto Linux boot time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8ULPEVK-Decreasing-Yocto-Linux-boot-time/m-p/1965378#M229187</link>
      <description>&lt;P&gt;Hello all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the IMX8ULP-EVK board for an embedded solution, where I need the boot time for linux to be very low (shooting for ~2 seconds), my application will involve booting the machine, doing meaningful work, and then turning off in a periodic cycle to decrease power consumption.&lt;/P&gt;&lt;P&gt;I am using Yocto Linux 6.6.23_2.0.0, and with the `core-image-minimal-dev` image, I am being taken to user login after about 12 seconds. Are there any guides I can follow to decrease the boot time? Are there any better images I can use that are more suitable for my application?&lt;BR /&gt;&lt;BR /&gt;I am currently working on removing features from the image, as well as cutting down the kernel features, however I fear this will not be enough (current 2 second kernel boot time and ~12 second systemd boot time). Any guidance would be much appreciated.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Oct 2024 20:03:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8ULPEVK-Decreasing-Yocto-Linux-boot-time/m-p/1965378#M229187</guid>
      <dc:creator>ksingh</dc:creator>
      <dc:date>2024-10-01T20:03:14Z</dc:date>
    </item>
    <item>
      <title>Re: [IMX8ULPEVK] Decreasing Yocto Linux boot time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8ULPEVK-Decreasing-Yocto-Linux-boot-time/m-p/1965731#M229217</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241345"&gt;@ksingh&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;At the moment we don´t have examples using the iMX8ULP EVK but you can refer to the&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN14093.pdf" target="_self"&gt;AN14093&lt;/A&gt;&amp;nbsp; in that Application note we explain how to reduce the boot time in iMX8M.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Wed, 02 Oct 2024 15:13:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8ULPEVK-Decreasing-Yocto-Linux-boot-time/m-p/1965731#M229217</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2024-10-02T15:13:57Z</dc:date>
    </item>
  </channel>
</rss>