<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックQuestions about uuu</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Questions-about-uuu/m-p/1962819#M228968</link>
    <description>&lt;P&gt;I'm working on both i.MX 8mm evk and I.MX 8mm custom board. After I produce the .wic from the yocto, I can easily flash it to the emmc by this:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;sudo uuu -b emmc_all imx-boot-imx8mm-lpddr4-evk-sd.bin-flash_evk core-image-minimal-imx8mm-lpddr4-evk.rootfs-20240925213534.wic&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However, if I would like to flash the &lt;STRONG&gt;bootloader, .dtb, kernel image and root file system seperately&lt;/STRONG&gt;, can I still use the uuu?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I also saw an example involved with the&amp;nbsp;&lt;STRONG&gt;_initramfs.cpio.gz.uboot&lt;/STRONG&gt;, it use uuu scripts flash them sperately, but right now &lt;STRONG&gt;I don't have the&amp;nbsp;_initramfs.cpio.gz.uboot&lt;/STRONG&gt;, how can I use the uuu to flash the &lt;STRONG&gt;emmc&lt;/STRONG&gt;?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 26 Sep 2024 16:05:46 GMT</pubDate>
    <dc:creator>Blake001</dc:creator>
    <dc:date>2024-09-26T16:05:46Z</dc:date>
    <item>
      <title>Questions about uuu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Questions-about-uuu/m-p/1962819#M228968</link>
      <description>&lt;P&gt;I'm working on both i.MX 8mm evk and I.MX 8mm custom board. After I produce the .wic from the yocto, I can easily flash it to the emmc by this:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;sudo uuu -b emmc_all imx-boot-imx8mm-lpddr4-evk-sd.bin-flash_evk core-image-minimal-imx8mm-lpddr4-evk.rootfs-20240925213534.wic&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However, if I would like to flash the &lt;STRONG&gt;bootloader, .dtb, kernel image and root file system seperately&lt;/STRONG&gt;, can I still use the uuu?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I also saw an example involved with the&amp;nbsp;&lt;STRONG&gt;_initramfs.cpio.gz.uboot&lt;/STRONG&gt;, it use uuu scripts flash them sperately, but right now &lt;STRONG&gt;I don't have the&amp;nbsp;_initramfs.cpio.gz.uboot&lt;/STRONG&gt;, how can I use the uuu to flash the &lt;STRONG&gt;emmc&lt;/STRONG&gt;?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Sep 2024 16:05:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Questions-about-uuu/m-p/1962819#M228968</guid>
      <dc:creator>Blake001</dc:creator>
      <dc:date>2024-09-26T16:05:46Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about uuu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Questions-about-uuu/m-p/1962891#M228979</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;You could use &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-upgrade-Linux-Kernel-and-dtb-on-eMMC-without-UUU/ta-p/1116428?attachment-id=60213" target="_self"&gt;this propose&lt;/A&gt; for debugging your changes.&lt;/P&gt;
&lt;P&gt;The script using UUU would be to write to the partition the additional .dtb and replace the kernel image. This is an example of adding a .dtb to the partition.&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;uuu -v -b fat_write .\&amp;lt;built-on-pc&amp;gt;.dtb mmc &amp;lt;usdhc interface&amp;gt;:1 &amp;lt;flashed-on-target&amp;gt;.dtb&lt;/LI-CODE&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 26 Sep 2024 18:44:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Questions-about-uuu/m-p/1962891#M228979</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-09-26T18:44:03Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about uuu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Questions-about-uuu/m-p/1965428#M229191</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you so much for the instrucitons. It is really helpful to use the emmc as sdcard and change the dtb or image instantly.&lt;/P&gt;&lt;P&gt;I'm trying to use the &lt;STRONG&gt;ums&lt;/STRONG&gt; command but it shows the error like below, it is a imx8mm custom board, how can I resovle it? If you have any suggestion, please let me know.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Blake001_0-1727825042184.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/302288i2475676B19D9CB81/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Blake001_0-1727825042184.png" alt="Blake001_0-1727825042184.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Blake001_0-1727825042184.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Blake&lt;/P&gt;</description>
      <pubDate>Tue, 01 Oct 2024 23:26:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Questions-about-uuu/m-p/1965428#M229191</guid>
      <dc:creator>Blake001</dc:creator>
      <dc:date>2024-10-01T23:26:53Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about uuu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Questions-about-uuu/m-p/1968277#M229370</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Is the board getting detected when running the command?&lt;/P&gt;
&lt;P&gt;You could try with fastboot command or booting in serial download mode.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Tue, 08 Oct 2024 01:39:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Questions-about-uuu/m-p/1968277#M229370</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-10-08T01:39:36Z</dc:date>
    </item>
  </channel>
</rss>