<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Android OS for IMX93 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-OS-for-IMX93/m-p/1961305#M228878</link>
    <description>&lt;P&gt;Hi all,&lt;BR /&gt;&lt;BR /&gt;I am starting to work with the IMX93 Evaluation Kit and we were wondering wherever or not it can work with Android OS, I do see that Android is offered for i.MX8 line of processors - but there is no mention of i.MX9 in documentations or forum (as far as I can tell).&lt;/P&gt;&lt;P&gt;Is Android OS BSP for i.MX93 in the works or are there no plans to have Android running on i.MX9?&lt;BR /&gt;&lt;BR /&gt;Thanks in advance,&lt;BR /&gt;Ivan&lt;/P&gt;</description>
    <pubDate>Wed, 25 Sep 2024 04:45:36 GMT</pubDate>
    <dc:creator>Ivan_tch</dc:creator>
    <dc:date>2024-09-25T04:45:36Z</dc:date>
    <item>
      <title>Android OS for IMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-OS-for-IMX93/m-p/1961305#M228878</link>
      <description>&lt;P&gt;Hi all,&lt;BR /&gt;&lt;BR /&gt;I am starting to work with the IMX93 Evaluation Kit and we were wondering wherever or not it can work with Android OS, I do see that Android is offered for i.MX8 line of processors - but there is no mention of i.MX9 in documentations or forum (as far as I can tell).&lt;/P&gt;&lt;P&gt;Is Android OS BSP for i.MX93 in the works or are there no plans to have Android running on i.MX9?&lt;BR /&gt;&lt;BR /&gt;Thanks in advance,&lt;BR /&gt;Ivan&lt;/P&gt;</description>
      <pubDate>Wed, 25 Sep 2024 04:45:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-OS-for-IMX93/m-p/1961305#M228878</guid>
      <dc:creator>Ivan_tch</dc:creator>
      <dc:date>2024-09-25T04:45:36Z</dc:date>
    </item>
    <item>
      <title>Re: Android OS for IMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-OS-for-IMX93/m-p/1962158#M228930</link>
      <description>&lt;P&gt;Hi &lt;/P&gt;
&lt;P&gt;Official release will not support i.MX93, no such plan.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Thu, 26 Sep 2024 02:03:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-OS-for-IMX93/m-p/1962158#M228930</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-09-26T02:03:29Z</dc:date>
    </item>
    <item>
      <title>Re: Android OS for IMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-OS-for-IMX93/m-p/1962677#M228958</link>
      <description>&lt;P&gt;Starting with Android 10 we had to exclude the i.MX devices which do not have a 3D GPU. Even if the CPU power of an i.MX 93 would be ok for a smaller Android based product, there are some Android requirements which are not met, especially the GPU + Extensions.&lt;/P&gt;
&lt;P&gt;In the end it would be technically possible to implement it, but from the marketing point of view it doesn't make any sense to create an NXP proprietary Android version.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Bernhard.&lt;/P&gt;</description>
      <pubDate>Thu, 26 Sep 2024 12:28:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-OS-for-IMX93/m-p/1962677#M228958</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2024-09-26T12:28:52Z</dc:date>
    </item>
    <item>
      <title>Re: Android OS for IMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-OS-for-IMX93/m-p/1963331#M229004</link>
      <description>&lt;P&gt;Thank you for the clarification Bernhard - makes more sense now&lt;/P&gt;</description>
      <pubDate>Fri, 27 Sep 2024 07:23:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-OS-for-IMX93/m-p/1963331#M229004</guid>
      <dc:creator>Ivan_tch</dc:creator>
      <dc:date>2024-09-27T07:23:31Z</dc:date>
    </item>
  </channel>
</rss>