<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMx28 Linux - Atheros WiFi</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMx28-Linux-Atheros-WiFi/m-p/250972#M22880</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Matt,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are aware of ath6kl driver, which is part of compat-wireless pacakge, for Atheros AR6000 series chipsets. My question was specific for the support of ath6kl in iMx28-Linux BSP release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Whether the iMx28-Linux BSP release has compat-wireless package (specifically ath6kl driver) ported to iMx28 or not? We don't see&amp;nbsp; compat-wireless package in iMx28-Linux BSP release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Or Do we need to take compat-wireless pacakge and port to iMx-Linux BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Apr 2013 17:30:42 GMT</pubDate>
    <dc:creator>pradeep2802</dc:creator>
    <dc:date>2013-04-04T17:30:42Z</dc:date>
    <item>
      <title>iMx28 Linux - Atheros WiFi</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMx28-Linux-Atheros-WiFi/m-p/250970#M22878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have downloaded iMx28 Linux source package (L2.6.35_1.1.0_130130_source.tar.gz) , which is updated in Feb,2013. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have following questions:&lt;/P&gt;&lt;P&gt;1. We found pkgs/atheros-wifi-2.6.35.3-1.1.0.tar.gz. This seems AR6002 driver, but not sure whether it is Linux-driver or Android-driver. Is it Linux or android driver? Does it support AR6003 also?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Do we have compat-wireless package support in this i.Mx28 Linux release ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2013 10:13:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMx28-Linux-Atheros-WiFi/m-p/250970#M22878</guid>
      <dc:creator>pradeep2802</dc:creator>
      <dc:date>2013-04-04T10:13:40Z</dc:date>
    </item>
    <item>
      <title>Re: iMx28 Linux - Atheros WiFi</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMx28-Linux-Atheros-WiFi/m-p/250971#M22879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;on newer Kernel releases the driver is included! Normaly it should be not a big deal to use the wireless driver !&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://git.kernel.org/cgit/linux/kernel/git/stable/linux-stable.git/tree/drivers/net/wireless/ath/ath6kl/Kconfig?id=refs/tags/v3.8.5" title="https://git.kernel.org/cgit/linux/kernel/git/stable/linux-stable.git/tree/drivers/net/wireless/ath/ath6kl/Kconfig?id=refs/tags/v3.8.5"&gt;kernel.org.&lt;/A&gt;&lt;A href="https://git.kernel.org/cgit/linux/kernel/git/stable/linux-stable.git/tree/drivers/net/wireless/ath/ath6kl/Kconfig?id=refs/tags/v3.8.5" title="https://git.kernel.org/cgit/linux/kernel/git/stable/linux-stable.git/tree/drivers/net/wireless/ath/ath6kl/Kconfig?id=refs/tags/v3.8.5"&gt;https://git.kernel.org/cgit/linux/kernel/git/stable/linux-stable.git/tree/drivers/net/wireless/ath/ath6kl/Kconfig?id=refs/tags/v3.8.5&lt;/A&gt;&lt;/P&gt;&lt;P&gt;drivers/net/wireless/ath/ath6kl&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Furthermore I found a note in Kconfig. Because of that hint i think the driver for AR6002 is incompatible to AR6003.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;This module adds support for wireless adapters based on&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Atheros AR6003 and AR6004 chipsets running over SDIO. If you&lt;/P&gt;
&lt;P&gt;&amp;nbsp; choose to build it as a module, it will be called ath6kl_sdio.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Please note that AR6002 and AR6001 are not supported by this&lt;/P&gt;
&lt;P&gt;&amp;nbsp; driver.&lt;/P&gt;
&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;
&lt;P&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;without engagement!!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MaTT&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/englisch-deutsch/without engagement.html" title="frequency: 0"&gt;&lt;/A&gt;&lt;A href="https://community.freescale.com/englisch-deutsch/without" target="test_blank"&gt;https://community.freescale.com/englisch-deutsch/without&lt;/A&gt; engagement.html &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2013 14:16:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMx28-Linux-Atheros-WiFi/m-p/250971#M22879</guid>
      <dc:creator>matthiasniederm</dc:creator>
      <dc:date>2013-04-04T14:16:33Z</dc:date>
    </item>
    <item>
      <title>Re: iMx28 Linux - Atheros WiFi</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMx28-Linux-Atheros-WiFi/m-p/250972#M22880</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Matt,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are aware of ath6kl driver, which is part of compat-wireless pacakge, for Atheros AR6000 series chipsets. My question was specific for the support of ath6kl in iMx28-Linux BSP release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Whether the iMx28-Linux BSP release has compat-wireless package (specifically ath6kl driver) ported to iMx28 or not? We don't see&amp;nbsp; compat-wireless package in iMx28-Linux BSP release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Or Do we need to take compat-wireless pacakge and port to iMx-Linux BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2013 17:30:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMx28-Linux-Atheros-WiFi/m-p/250972#M22880</guid>
      <dc:creator>pradeep2802</dc:creator>
      <dc:date>2013-04-04T17:30:42Z</dc:date>
    </item>
    <item>
      <title>Re: iMx28 Linux - Atheros WiFi</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMx28-Linux-Atheros-WiFi/m-p/250973#M22881</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello pradeep&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you get the information needed? Iam also looking for the same information. Can anyone please reply?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2013 15:40:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMx28-Linux-Atheros-WiFi/m-p/250973#M22881</guid>
      <dc:creator>vikranthreddy</dc:creator>
      <dc:date>2013-04-09T15:40:32Z</dc:date>
    </item>
  </channel>
</rss>