<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Two different camera on MIPI-CSI using mux</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Two-different-camera-on-MIPI-CSI-using-mux/m-p/1959954#M228776</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Even you connect convert board, but imx8mm doesn't have virtual channel to handle this, if you need dual camera, maybe you can use MIPI CSI+ usb camera&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Mon, 23 Sep 2024 14:12:02 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-09-23T14:12:02Z</dc:date>
    <item>
      <title>Two different camera on MIPI-CSI using mux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Two-different-camera-on-MIPI-CSI-using-mux/m-p/1959867#M228768</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;We want to use two different cameras on single MIPI-CSI port using MUX with IMX8MM linux. At a time only one camera module will be active in runtime. How to make dts entries for this? Can someone guide us achieve this objective?&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Ajita&lt;/P&gt;&lt;P&gt;#imx8mm #linux&lt;/P&gt;</description>
      <pubDate>Mon, 23 Sep 2024 11:30:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Two-different-camera-on-MIPI-CSI-using-mux/m-p/1959867#M228768</guid>
      <dc:creator>ajita02</dc:creator>
      <dc:date>2024-09-23T11:30:50Z</dc:date>
    </item>
    <item>
      <title>Re: Two different camera on MIPI-CSI using mux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Two-different-camera-on-MIPI-CSI-using-mux/m-p/1959954#M228776</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Even you connect convert board, but imx8mm doesn't have virtual channel to handle this, if you need dual camera, maybe you can use MIPI CSI+ usb camera&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 23 Sep 2024 14:12:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Two-different-camera-on-MIPI-CSI-using-mux/m-p/1959954#M228776</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-09-23T14:12:02Z</dc:date>
    </item>
    <item>
      <title>Re: Two different camera on MIPI-CSI using mux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Two-different-camera-on-MIPI-CSI-using-mux/m-p/1960429#M228812</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/34846"&gt;@Bio_TICFSL&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Can we use single channel used by mux as at a time single camera will be in use? Mux select line will be handle by GPIO.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Ajita&lt;/P&gt;</description>
      <pubDate>Tue, 24 Sep 2024 06:00:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Two-different-camera-on-MIPI-CSI-using-mux/m-p/1960429#M228812</guid>
      <dc:creator>ajita02</dc:creator>
      <dc:date>2024-09-24T06:00:29Z</dc:date>
    </item>
    <item>
      <title>Re: Two different camera on MIPI-CSI using mux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Two-different-camera-on-MIPI-CSI-using-mux/m-p/1960689#M228820</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/30870"&gt;@jack_mao&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt; Please help&lt;/P&gt;</description>
      <pubDate>Tue, 24 Sep 2024 09:54:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Two-different-camera-on-MIPI-CSI-using-mux/m-p/1960689#M228820</guid>
      <dc:creator>ajita02</dc:creator>
      <dc:date>2024-09-24T09:54:25Z</dc:date>
    </item>
    <item>
      <title>Re: Two different camera on MIPI-CSI using mux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Two-different-camera-on-MIPI-CSI-using-mux/m-p/1961145#M228867</link>
      <description>&lt;P&gt;maybe you can refer to this topic, with switch&amp;nbsp;&lt;SPAN&gt;NX3DV642&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/bring-up-dual-Camera-under-single-mipi-csi/ta-p/1728321" target="_blank"&gt;bring up dual Camera under single mipi csi - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Sep 2024 00:14:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Two-different-camera-on-MIPI-CSI-using-mux/m-p/1961145#M228867</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2024-09-25T00:14:31Z</dc:date>
    </item>
    <item>
      <title>Re: Two different camera on MIPI-CSI using mux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Two-different-camera-on-MIPI-CSI-using-mux/m-p/1986781#M230417</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/34846"&gt;@Bio_TICFSL&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;We have tried to implement the patch shared by &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt;. We made changes in these files "&lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/staging/media/imx/imx8-mipi-csi2-sam.c&amp;quot;" target="_blank"&gt;https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/staging/media/imx/imx8-mipi-csi2-sam.c"&lt;/A&gt; and "“&lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/staging/media/imx/imx8-media-dev.c”" target="_blank"&gt;https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/staging/media/imx/imx8-media-dev.c”&lt;/A&gt; . But IMX8MM is not using any of these files. So as a result its only probing first endpoint mentioned in dts and ignoring second endpoint of camera.&lt;/P&gt;&lt;P&gt;Can you provide us a lead?&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Ajita&lt;/P&gt;</description>
      <pubDate>Mon, 04 Nov 2024 06:57:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Two-different-camera-on-MIPI-CSI-using-mux/m-p/1986781#M230417</guid>
      <dc:creator>ajita02</dc:creator>
      <dc:date>2024-11-04T06:57:50Z</dc:date>
    </item>
  </channel>
</rss>