<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MIMX8ML8CVNKZAB Thermal Management</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIMX8ML8CVNKZAB-Thermal-Management/m-p/1959835#M228767</link>
    <description>&lt;P&gt;Hi Joanxie,&lt;/P&gt;&lt;P&gt;Thanks for the reply&lt;/P&gt;</description>
    <pubDate>Mon, 23 Sep 2024 10:46:59 GMT</pubDate>
    <dc:creator>Pavanecon</dc:creator>
    <dc:date>2024-09-23T10:46:59Z</dc:date>
    <item>
      <title>MIMX8ML8CVNKZAB Thermal Management</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMX8ML8CVNKZAB-Thermal-Management/m-p/1956244#M228536</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;We developed a customized board for our application with MIMX8ML8CVNKZAB SOC. During our thermal test, we observed that at 55 °C, our board is getting shutdown. This is due to the default thermal shutdown at 95 °C junction temperature.&lt;/P&gt;&lt;P&gt;As per the reference manual, the SOC Thermal Shutdown temperature can be configured up to 105C.&lt;/P&gt;&lt;P&gt;Now we are planning to configure the thermal shutdown temperature to 100 °C.&lt;/P&gt;&lt;P&gt;So, is it worth changing the thermal shutdown temperature to 100 °C? or do we have any risk of doing this?&lt;/P&gt;&lt;P&gt;Can NXP provide any views or comments on this?&lt;/P&gt;</description>
      <pubDate>Wed, 18 Sep 2024 05:44:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMX8ML8CVNKZAB-Thermal-Management/m-p/1956244#M228536</guid>
      <dc:creator>Pavanecon</dc:creator>
      <dc:date>2024-09-18T05:44:14Z</dc:date>
    </item>
    <item>
      <title>Re: MIMX8ML8CVNKZAB Thermal Management</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMX8ML8CVNKZAB-Thermal-Management/m-p/1956481#M228560</link>
      <description>Is it safe to change the thermal shutdown temperature to 100 C? Can anyone reply on this</description>
      <pubDate>Wed, 18 Sep 2024 09:03:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMX8ML8CVNKZAB-Thermal-Management/m-p/1956481#M228560</guid>
      <dc:creator>Pavanecon</dc:creator>
      <dc:date>2024-09-18T09:03:33Z</dc:date>
    </item>
    <item>
      <title>Re: MIMX8ML8CVNKZAB Thermal Management</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMX8ML8CVNKZAB-Thermal-Management/m-p/1957028#M228605</link>
      <description>&lt;P&gt;&lt;SPAN class="uiOutputText"&gt;refer to the data sheet, industrial can support up to the 105&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="joanxie_0-1726708185871.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/299816i05851E22F87869DF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="joanxie_0-1726708185871.png" alt="joanxie_0-1726708185871.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="uiOutputText"&gt;but consider the margin 10°C to the max temperature, we suggest customer set 95°C as critical temperature, which not mean the 100 is not allowed, just consider the sensor accuracy&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Sep 2024 01:10:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMX8ML8CVNKZAB-Thermal-Management/m-p/1957028#M228605</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2024-09-19T01:10:34Z</dc:date>
    </item>
    <item>
      <title>Re: MIMX8ML8CVNKZAB Thermal Management</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMX8ML8CVNKZAB-Thermal-Management/m-p/1959835#M228767</link>
      <description>&lt;P&gt;Hi Joanxie,&lt;/P&gt;&lt;P&gt;Thanks for the reply&lt;/P&gt;</description>
      <pubDate>Mon, 23 Sep 2024 10:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMX8ML8CVNKZAB-Thermal-Management/m-p/1959835#M228767</guid>
      <dc:creator>Pavanecon</dc:creator>
      <dc:date>2024-09-23T10:46:59Z</dc:date>
    </item>
  </channel>
</rss>