<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックabout the camera interface for ov8820</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/about-the-camera-interface-for-ov8820/m-p/250952#M22876</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on the camera interface of ov8820 for sabresd board. i suppose these are out of box function modules. But it after put u10 on and short SH501. it still gives a i2c write error. ( After double check the pins, looks like the pwdn pin is not set correctly, so i modified the board-mx6q_sabresd.c to force the pwdn pin to be 1. After that i2c function correct.&amp;nbsp; But still can not capture image. i did modprobe ov8820_camera_mipi &amp;amp; modprobe mxc_v4l2_capture. then &lt;STRONG style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #000000; background-color: #ffffff;"&gt;gst-launch v4l2src num-buffers=1 ! jpegenc ! filesink location=sample.jpeg ( the camera is hooked up with /dev/video0) it shows error message &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Out of memory: Kill process 6725 (gst-launch-0.10) score 577 or sacrifice child&lt;/P&gt;&lt;P&gt;Killed process 6725 (gst-launch-0.10) total-vm:552648kB, anon-rss:542996kB, file-rss:0kB&lt;/P&gt;&lt;P&gt;Killed (my system is linux kernel 3.0.35 with ltib &amp;amp; rootfs is ubuntu 11.10)&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Jul 2013 18:09:29 GMT</pubDate>
    <dc:creator>erichu</dc:creator>
    <dc:date>2013-07-02T18:09:29Z</dc:date>
    <item>
      <title>about the camera interface for ov8820</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-the-camera-interface-for-ov8820/m-p/250952#M22876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on the camera interface of ov8820 for sabresd board. i suppose these are out of box function modules. But it after put u10 on and short SH501. it still gives a i2c write error. ( After double check the pins, looks like the pwdn pin is not set correctly, so i modified the board-mx6q_sabresd.c to force the pwdn pin to be 1. After that i2c function correct.&amp;nbsp; But still can not capture image. i did modprobe ov8820_camera_mipi &amp;amp; modprobe mxc_v4l2_capture. then &lt;STRONG style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #000000; background-color: #ffffff;"&gt;gst-launch v4l2src num-buffers=1 ! jpegenc ! filesink location=sample.jpeg ( the camera is hooked up with /dev/video0) it shows error message &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Out of memory: Kill process 6725 (gst-launch-0.10) score 577 or sacrifice child&lt;/P&gt;&lt;P&gt;Killed process 6725 (gst-launch-0.10) total-vm:552648kB, anon-rss:542996kB, file-rss:0kB&lt;/P&gt;&lt;P&gt;Killed (my system is linux kernel 3.0.35 with ltib &amp;amp; rootfs is ubuntu 11.10)&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2013 18:09:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-the-camera-interface-for-ov8820/m-p/250952#M22876</guid>
      <dc:creator>erichu</dc:creator>
      <dc:date>2013-07-02T18:09:29Z</dc:date>
    </item>
    <item>
      <title>Re: about the camera interface for ov8820</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-the-camera-interface-for-ov8820/m-p/250953#M22877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Suggest reading &lt;A href="https://community.nxp.com/message/328301"&gt;Some Experience When Enable MIPI Camera&lt;/A&gt; first.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2013 03:39:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-the-camera-interface-for-ov8820/m-p/250953#M22877</guid>
      <dc:creator>JayTu</dc:creator>
      <dc:date>2013-08-27T03:39:54Z</dc:date>
    </item>
  </channel>
</rss>