<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX8MP RAM ISSUE</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1957479#M228637</link>
    <description>Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/46293"&gt;@jakub&lt;/a&gt;,&lt;BR /&gt;I downloaded the files and tried following the Readme file included inside. But I am not able to Init.sh anywhere inside imx-yocto-bsp directory. I followed the Yocto USer's Guide to download and create the BSP.</description>
    <pubDate>Thu, 19 Sep 2024 08:51:01 GMT</pubDate>
    <dc:creator>bgaurav1718</dc:creator>
    <dc:date>2024-09-19T08:51:01Z</dc:date>
    <item>
      <title>IMX8MP RAM ISSUE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1666120#M207316</link>
      <description>&lt;P&gt;Hi we are facing a problem in our board which was developed based on the IMX8MP board. We are not able to boot the board with 2GB ram in Windows 10 IoT. What is the minimum ram requirement for windows 10 IoT with imx8mp ?&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jun 2023 10:55:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1666120#M207316</guid>
      <dc:creator>Athi</dc:creator>
      <dc:date>2023-06-08T10:55:14Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP RAM ISSUE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1668095#M207476</link>
      <description>Hi Athi,&lt;BR /&gt;You have to properly modify boot firmware, particularly UEFI for lesser RAM. The BSP runs on i.MX 8M Mini and Nano which feature just 2 GB RAM. However You should expect worse OS responsiveness with this configuration.</description>
      <pubDate>Tue, 13 Jun 2023 07:45:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1668095#M207476</guid>
      <dc:creator>Frantisek_Prochaska</dc:creator>
      <dc:date>2023-06-13T07:45:36Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP RAM ISSUE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1668133#M207480</link>
      <description>&lt;P&gt;Thanks&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/79780"&gt;@Frantisek_Prochaska&lt;/a&gt;&amp;nbsp;.&lt;/P&gt;&lt;P&gt;We have modified the base memory address in MX8M_PLUS_EVK.dsc file and successfully&amp;nbsp;&lt;SPAN&gt;flashed the Windows IoT image to eMMC. After that, we got a blue screen error while it automatically tried to restart the windows.&lt;/SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MicrosoftTeams-image (30).png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/227347iF7D8655D3213C31C/image-size/large?v=v2&amp;amp;px=999" role="button" title="MicrosoftTeams-image (30).png" alt="MicrosoftTeams-image (30).png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 08:12:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1668133#M207480</guid>
      <dc:creator>Athi</dc:creator>
      <dc:date>2023-06-13T08:12:07Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP RAM ISSUE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1668148#M207483</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218568"&gt;@Athi&lt;/a&gt;,&lt;BR /&gt;okay, that implies WinPe run without crashing. Is that correct?&lt;BR /&gt;&lt;BR /&gt;Edit: You can always try to hook up a debugger, create boot log, or look for a crash dump on eMMC.&lt;BR /&gt;Edit2:&amp;nbsp;BSOD at boot time could also be caused by RPMB. If this was the case WinPe will boot okay but installed Windows will boot only into safe mode or in test-signed mode with un-secured UEFI. I'm not completely sure abut that without searching community.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 09:57:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1668148#M207483</guid>
      <dc:creator>Frantisek_Prochaska</dc:creator>
      <dc:date>2023-06-13T09:57:00Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP RAM ISSUE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1669328#M207605</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/79780"&gt;@Frantisek_Prochaska&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Yes, WinPE is running without any crash. When we trying to restart the windows, it will go in to BSOD with "CLOCK WATCHDOG TIMEOUT". Also we have windbg error log.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jun 2023 12:55:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1669328#M207605</guid>
      <dc:creator>Athi</dc:creator>
      <dc:date>2023-06-14T12:55:17Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP RAM ISSUE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1670156#M207654</link>
      <description>Hi @Ahti,&lt;BR /&gt;good that WinPe boots. I will forward the problem to support team.&lt;BR /&gt;&lt;BR /&gt;Meanwhile, could you send us dump or at least mini dump?&lt;BR /&gt;&lt;A href="https://learn.microsoft.com/en-us/windows-hardware/drivers/debugger/-dump--create-dump-file-" target="_blank"&gt;https://learn.microsoft.com/en-us/windows-hardware/drivers/debugger/-dump--create-dump-file-&lt;/A&gt;</description>
      <pubDate>Thu, 15 Jun 2023 09:39:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1670156#M207654</guid>
      <dc:creator>Frantisek_Prochaska</dc:creator>
      <dc:date>2023-06-15T09:39:03Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP RAM ISSUE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1670247#M207662</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218568"&gt;@Athi&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;the 6GB to 2GB RAM reduction on the 8MP was also addressed by another customer, there is a zip with a patch for BSP firmware version 1.3.0 in this post &lt;A href="https://community.nxp.com/t5/i-MX-WIN10-IoT-Enterprise/Nexcom-Customize-i-MX8MP-DDR-size-from-6G-to-2G/m-p/1616550/highlight/true#M278" target="_self"&gt;https://community.nxp.com/t5/i-MX-WIN10-IoT-Enterprise/Nexcom-Customize-i-MX8MP-DDR-size-from-6G-to-2G/m-p/1616550/highlight/true#M278&lt;/A&gt; that worked for me on the EVK. Plus below is a patch for the ACPI table to show 2GB in the task manager as well.&lt;BR /&gt;Questions about Windows 10 IoT are better directed directly to this community &lt;A href="https://community.nxp.com/t5/i-MX-WIN10-IoT-Enterprise/gh-p/52533" target="_self"&gt;https://community.nxp.com/t5/i-MX-WIN10-IoT-Enterprise/gh-p/52533&lt;/A&gt;.&lt;BR /&gt;If you don't have access there, I'll try to arrange it.&lt;/P&gt;
&lt;P&gt;Best Regards, Jakub&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jun 2023 11:21:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1670247#M207662</guid>
      <dc:creator>jakub_zigacek</dc:creator>
      <dc:date>2023-06-15T11:21:12Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP RAM ISSUE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1670987#M207716</link>
      <description>&lt;P&gt;Thanks&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204770"&gt;@jakub_zigacek&lt;/a&gt;&amp;nbsp;, It's working fine.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jun 2023 09:01:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1670987#M207716</guid>
      <dc:creator>Athi</dc:creator>
      <dc:date>2023-06-16T09:01:59Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP RAM ISSUE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1671952#M207802</link>
      <description>&lt;P&gt;&lt;SPAN class="im"&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218568"&gt;@Athi&lt;/a&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;DIV&gt;I hope you are doing well.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;Glad to know that issue is resolved.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;can I mark this case as close?&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;Thanks &amp;amp; Regards,&lt;/DIV&gt;
&lt;DIV&gt;Sanket Parekh&lt;/DIV&gt;
&lt;P&gt;&lt;LI-WRAPPER&gt;&lt;/LI-WRAPPER&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jun 2023 11:34:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1671952#M207802</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-06-19T11:34:50Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP RAM ISSUE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1672482#M207845</link>
      <description>&lt;P&gt;yes&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202155"&gt;@Sanket_Parekh&lt;/a&gt;&amp;nbsp;,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jun 2023 07:41:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1672482#M207845</guid>
      <dc:creator>Athi</dc:creator>
      <dc:date>2023-06-20T07:41:28Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP RAM ISSUE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1957479#M228637</link>
      <description>Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/46293"&gt;@jakub&lt;/a&gt;,&lt;BR /&gt;I downloaded the files and tried following the Readme file included inside. But I am not able to Init.sh anywhere inside imx-yocto-bsp directory. I followed the Yocto USer's Guide to download and create the BSP.</description>
      <pubDate>Thu, 19 Sep 2024 08:51:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1957479#M228637</guid>
      <dc:creator>bgaurav1718</dc:creator>
      <dc:date>2024-09-19T08:51:01Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP RAM ISSUE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1961729#M228910</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218700"&gt;@bgaurav1718&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;sorry for the confusion, but the patch is only meant for Windows 10 IoT BSP&amp;nbsp; as can be found here: &lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/windows-10-11-iot-enterprise-for-i-mx-applications-processors:IMXWIN10IOT" target="_blank"&gt;https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/windows-10-11-iot-enterprise-for-i-mx-applications-processors:IMXWIN10IOT&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards, Jakub&lt;/P&gt;</description>
      <pubDate>Wed, 25 Sep 2024 11:39:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-RAM-ISSUE/m-p/1961729#M228910</guid>
      <dc:creator>jakub_zigacek</dc:creator>
      <dc:date>2024-09-25T11:39:58Z</dc:date>
    </item>
  </channel>
</rss>