<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Can Connectivity</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-Connectivity/m-p/1957175#M228610</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203368"&gt;@Manuel_Salas&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you cant provide me a Connector . Can you please let me know the use of each pin in the 8-pin port? like CAN0_H for which pin and CAN0_L for which pin etc.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Athul&lt;/P&gt;</description>
    <pubDate>Thu, 19 Sep 2024 04:42:43 GMT</pubDate>
    <dc:creator>athul_am</dc:creator>
    <dc:date>2024-09-19T04:42:43Z</dc:date>
    <item>
      <title>Can Connectivity</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-Connectivity/m-p/1951857#M228304</link>
      <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;I have a IMX6 ULL evk board with me . My understanding is that it has a CAN Capability.&lt;/P&gt;&lt;P&gt;Can someone let me know the connector to connect a DB-9 connector to the Board, also if the base image that comes with the box has CAN enabled if not how to enable it.&lt;BR /&gt;&lt;BR /&gt;Thanks in Advance,&lt;BR /&gt;Athul&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 08:04:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-Connectivity/m-p/1951857#M228304</guid>
      <dc:creator>athul_am</dc:creator>
      <dc:date>2024-09-11T08:04:40Z</dc:date>
    </item>
    <item>
      <title>Re: Can Connectivity</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-Connectivity/m-p/1952638#M228348</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226643"&gt;@athul_am&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;All i.MX 6 supports one CAN with the default device tree on i.MX 6SABRE-AI. Supports both CANs using the FlexCAN device tree but has a pin conflict with FEC. Supports with the default device tree on i.MX 6SoloX-SD, 7Dual SABRE-SD, 6Ultre Lite EVK, and 6ULL EVK. With the platform that supports the FlexCAN module, FlexCAN supports CANFD mode.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also you can take a look to the table&amp;nbsp;Table 42. FlexCAN Driver Files on &lt;A href="https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf" target="_self"&gt;IMX Reference Manual&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also, the i.MX6ULL provides a CAN access through the&amp;nbsp;J1201 port.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alejandro_Salas_0-1726090008241.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/298649i64980550D871A707/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alejandro_Salas_0-1726090008241.png" alt="Alejandro_Salas_0-1726090008241.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 21:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-Connectivity/m-p/1952638#M228348</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2024-09-11T21:27:03Z</dc:date>
    </item>
    <item>
      <title>Re: Can Connectivity</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-Connectivity/m-p/1952825#M228353</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203368"&gt;@Manuel_Salas&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for the reply . I would like the connector to be used to connect the imx6ull board can port to the DB-9 Connector as the package of the board did not come with one included.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Athul&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 01:40:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-Connectivity/m-p/1952825#M228353</guid>
      <dc:creator>athul_am</dc:creator>
      <dc:date>2024-09-12T01:40:14Z</dc:date>
    </item>
    <item>
      <title>Re: Can Connectivity</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-Connectivity/m-p/1957175#M228610</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203368"&gt;@Manuel_Salas&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you cant provide me a Connector . Can you please let me know the use of each pin in the 8-pin port? like CAN0_H for which pin and CAN0_L for which pin etc.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Athul&lt;/P&gt;</description>
      <pubDate>Thu, 19 Sep 2024 04:42:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-Connectivity/m-p/1957175#M228610</guid>
      <dc:creator>athul_am</dc:creator>
      <dc:date>2024-09-19T04:42:43Z</dc:date>
    </item>
    <item>
      <title>Re: Can Connectivity</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-Connectivity/m-p/1960006#M228780</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you are looking for the exact part number, is&amp;nbsp;WF1250801200, but it appears is not longer in production.&lt;/P&gt;
&lt;P&gt;You can refer to &lt;A href="https://cms-emu-slicetest.web.cern.ch/904/Documentation/Manuals/CAN%20Bus%20Interface.htm" target="_self"&gt;this link&lt;/A&gt; to see the pinout of the&amp;nbsp;&lt;SPAN&gt;9-pin D connector.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alejandro_Salas_0-1727104403705.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/300733i9C65CBB2CFB42874/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alejandro_Salas_0-1727104403705.png" alt="Alejandro_Salas_0-1727104403705.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Sep 2024 15:13:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-Connectivity/m-p/1960006#M228780</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2024-09-23T15:13:53Z</dc:date>
    </item>
  </channel>
</rss>