<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 IMX8MM mipi settings</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-mipi-settings/m-p/1955949#M228518</link>
    <description>&lt;P&gt;I used Yocto to build a 6.6.23 version wic image and flashed it to my imx8MM custom board. It booted successfully, and I can log in through Minicom, but the display is not working. I tried using other DTBs, such as &lt;STRONG&gt;imx8mm-ddr4-evk-rm67191.dtb&lt;/STRONG&gt;, but they didn't work. The display is connected directly through MIPI, not MIPI to HDMI. How can I turn on the display? Should I modify the DTS from the Yocto project or change the bootloader?&lt;/P&gt;</description>
    <pubDate>Tue, 17 Sep 2024 22:03:08 GMT</pubDate>
    <dc:creator>Blake001</dc:creator>
    <dc:date>2024-09-17T22:03:08Z</dc:date>
    <item>
      <title>IMX8MM mipi settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-mipi-settings/m-p/1955949#M228518</link>
      <description>&lt;P&gt;I used Yocto to build a 6.6.23 version wic image and flashed it to my imx8MM custom board. It booted successfully, and I can log in through Minicom, but the display is not working. I tried using other DTBs, such as &lt;STRONG&gt;imx8mm-ddr4-evk-rm67191.dtb&lt;/STRONG&gt;, but they didn't work. The display is connected directly through MIPI, not MIPI to HDMI. How can I turn on the display? Should I modify the DTS from the Yocto project or change the bootloader?&lt;/P&gt;</description>
      <pubDate>Tue, 17 Sep 2024 22:03:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-mipi-settings/m-p/1955949#M228518</guid>
      <dc:creator>Blake001</dc:creator>
      <dc:date>2024-09-17T22:03:08Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM mipi settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-mipi-settings/m-p/1956621#M228574</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239825"&gt;@Blake001&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Our precompiled images are only for our boards.&lt;/P&gt;
&lt;P&gt;To generate an image according to your custom hardware, you should port our BSP to your board, to do that you can follow our porting guide:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_PORTING_GUIDE.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX_PORTING_GUIDE.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Wed, 18 Sep 2024 11:46:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-mipi-settings/m-p/1956621#M228574</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2024-09-18T11:46:50Z</dc:date>
    </item>
  </channel>
</rss>