<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: UUU Log Help in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/UUU-Log-Help/m-p/1953691#M228391</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;It does tell you that it fails at that stage of the command, I would suggest to also check the UART logs as Uboot should output more meaningful information of what actually went wrong on this command.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Thu, 12 Sep 2024 20:02:24 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2024-09-12T20:02:24Z</dc:date>
    <item>
      <title>UUU Log Help</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UUU-Log-Help/m-p/1952545#M228342</link>
      <description>&lt;P&gt;I could use a hand deciphering an error using UUU. The error information output by UUU does not help me that much. I highlighted the error in red below. Anyone know if I can obtain more information out of UUU?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;programming/usb$ &lt;FONT color="#339966"&gt;sudo uuu -V uuu_projectX.auto&lt;/FONT&gt;&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.243-0-ged48c51&lt;/P&gt;&lt;P&gt;Build in config:&lt;BR /&gt;Pctl Chip Vid Pid BcdVersion&lt;BR /&gt;==================================================&lt;BR /&gt;SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]&lt;BR /&gt;SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]&lt;BR /&gt;SDPS: MX8DXL 0x1fc9 0x0147&lt;BR /&gt;SDPS: MX28 0x15a2 0x004f&lt;BR /&gt;SDPS: MX815 0x1fc9 0x013e&lt;BR /&gt;SDPS: MX865 0x1fc9 0x0146&lt;BR /&gt;SDPS: MX8ULP 0x1fc9 0x014a&lt;BR /&gt;SDPS: MX8ULP 0x1fc9 0x014b&lt;BR /&gt;SDPS: MX93 0x1fc9 0x014e&lt;BR /&gt;SDP: MX7D 0x15a2 0x0076&lt;BR /&gt;SDP: MX6Q 0x15a2 0x0054&lt;BR /&gt;SDP: MX6D 0x15a2 0x0061&lt;BR /&gt;SDP: MX6SL 0x15a2 0x0063&lt;BR /&gt;SDP: MX6SX 0x15a2 0x0071&lt;BR /&gt;SDP: MX6UL 0x15a2 0x007d&lt;BR /&gt;SDP: MX6ULL 0x15a2 0x0080&lt;BR /&gt;SDP: MX6SLL 0x1fc9 0x0128&lt;BR /&gt;SDP: MX7ULP 0x1fc9 0x0126&lt;BR /&gt;SDP: MXRT106X 0x1fc9 0x0135&lt;BR /&gt;SDP: MX8MM 0x1fc9 0x0134&lt;BR /&gt;SDP: MX8MQ 0x1fc9 0x012b&lt;BR /&gt;SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]&lt;BR /&gt;SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]&lt;BR /&gt;SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998]&lt;BR /&gt;SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]&lt;BR /&gt;SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]&lt;BR /&gt;SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]&lt;BR /&gt;FBK: 0x066f 0x9afe&lt;BR /&gt;FBK: 0x066f 0x9bff&lt;BR /&gt;FBK: 0x1fc9 0x0153&lt;BR /&gt;FB: 0x0525 0xa4a5&lt;BR /&gt;FB: 0x18d1 0x0d02&lt;BR /&gt;FB: 0x3016 0x0001&lt;BR /&gt;FB: 0x1fc9 0x0152&lt;BR /&gt;Wait for Known USB Device Appear...&lt;BR /&gt;New USB Device Attached at 1:101&lt;BR /&gt;1:101&amp;gt;Start Cmd:SDPS: boot -f imx-boot-projectX-sd.bin-flash&lt;BR /&gt;100%1:101&amp;gt;Okay (0.817s)&lt;BR /&gt;libusb: error [udev_hotplug_event] ignoring udev action bind&lt;BR /&gt;New USB Device Attached at 1:101&lt;BR /&gt;1:101&amp;gt;Start Cmd:FB: ucmd setenv fastboot_dev mmc&lt;BR /&gt;1:101&amp;gt;Okay (0.106s)&lt;BR /&gt;1:101&amp;gt;Start Cmd:FB: ucmd setenv mmcdev ${emmc_dev}&lt;BR /&gt;1:101&amp;gt;Okay (0.004s)&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;1:101&amp;gt;Start Cmd:FB: ucmd mmc dev ${emmc_dev}&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;1:101&amp;gt;Fail (0.048s)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;programming/usb$&lt;/P&gt;&lt;/BLOCKQUOTE&gt;</description>
      <pubDate>Wed, 11 Sep 2024 19:59:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UUU-Log-Help/m-p/1952545#M228342</guid>
      <dc:creator>TimNew</dc:creator>
      <dc:date>2024-09-11T19:59:36Z</dc:date>
    </item>
    <item>
      <title>Re: UUU Log Help</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UUU-Log-Help/m-p/1953691#M228391</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;It does tell you that it fails at that stage of the command, I would suggest to also check the UART logs as Uboot should output more meaningful information of what actually went wrong on this command.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 20:02:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UUU-Log-Help/m-p/1953691#M228391</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2024-09-12T20:02:24Z</dc:date>
    </item>
  </channel>
</rss>