<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Watchdog timer usage imx6ull</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Watchdog-timer-usage-imx6ull/m-p/1953538#M228382</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are planning to use the Watchdog timer for our existing system for any type of os failure or hardware failure,&lt;/P&gt;&lt;P&gt;and we are using the&lt;STRONG&gt; IMX6ULL&lt;/STRONG&gt; board so can you suggest which watchdog we can use for the best output and feasibility point of view?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 12 Sep 2024 14:08:30 GMT</pubDate>
    <dc:creator>amiraj_patel</dc:creator>
    <dc:date>2024-09-12T14:08:30Z</dc:date>
    <item>
      <title>Watchdog timer usage imx6ull</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Watchdog-timer-usage-imx6ull/m-p/1953538#M228382</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are planning to use the Watchdog timer for our existing system for any type of os failure or hardware failure,&lt;/P&gt;&lt;P&gt;and we are using the&lt;STRONG&gt; IMX6ULL&lt;/STRONG&gt; board so can you suggest which watchdog we can use for the best output and feasibility point of view?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 14:08:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Watchdog-timer-usage-imx6ull/m-p/1953538#M228382</guid>
      <dc:creator>amiraj_patel</dc:creator>
      <dc:date>2024-09-12T14:08:30Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog timer usage imx6ull</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Watchdog-timer-usage-imx6ull/m-p/1955870#M228507</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/240033"&gt;@amiraj_patel&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing very well.&lt;/P&gt;
&lt;P&gt;You can refer to the &lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/arch/arm/boot/dts/nxp/imx/imx6ul-14x14-evk.dtsi#L444" target="_self"&gt;imx6ul device tree&lt;/A&gt;, the only wdog used is the wdog1, you can use wdog2 and wdog3, just you must declare it on the device tree.&lt;/P&gt;
&lt;P&gt;I hope this can helps to you.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Sep 2024 19:44:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Watchdog-timer-usage-imx6ull/m-p/1955870#M228507</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2024-09-17T19:44:43Z</dc:date>
    </item>
  </channel>
</rss>