<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx8mplus boot flow</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mplus-boot-flow/m-p/1952417#M228338</link>
    <description>&lt;P&gt;I am using i.MX8M&amp;nbsp; Plus lpddr4 evk board and have built the "IMXLXYOCTOUG v.LF6.6.3_1.0.0" BSP using Yocto&lt;/P&gt;&lt;P&gt;I successfully flashed the image onto the SD card and tested it. But I want to know the boot flow of the image from the SD card. Is there any document available for boot flow? Please help me.&lt;/P&gt;&lt;P&gt;Thanks, Regards&lt;/P&gt;&lt;P&gt;Srinivas&lt;/P&gt;</description>
    <pubDate>Wed, 11 Sep 2024 18:18:57 GMT</pubDate>
    <dc:creator>srinivas_123</dc:creator>
    <dc:date>2024-09-11T18:18:57Z</dc:date>
    <item>
      <title>imx8mplus boot flow</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mplus-boot-flow/m-p/1952417#M228338</link>
      <description>&lt;P&gt;I am using i.MX8M&amp;nbsp; Plus lpddr4 evk board and have built the "IMXLXYOCTOUG v.LF6.6.3_1.0.0" BSP using Yocto&lt;/P&gt;&lt;P&gt;I successfully flashed the image onto the SD card and tested it. But I want to know the boot flow of the image from the SD card. Is there any document available for boot flow? Please help me.&lt;/P&gt;&lt;P&gt;Thanks, Regards&lt;/P&gt;&lt;P&gt;Srinivas&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 18:18:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mplus-boot-flow/m-p/1952417#M228338</guid>
      <dc:creator>srinivas_123</dc:creator>
      <dc:date>2024-09-11T18:18:57Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mplus boot flow</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mplus-boot-flow/m-p/1952588#M228344</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231093"&gt;@srinivas_123&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;After power on or reset, i.MX 8M executes the Boot ROM (the primary program loader), stored in its read-only memory (ROM).&lt;/P&gt;
&lt;P&gt;Boot ROM configures the system-on-chip (SoC) by performing basic peripheral initializations such as Phase Locked Loops (PLLs), clock configurations, memory initialization (SRAM). Then it finds a boot device from where it loads a bootloader image, which can include the following components: U-Boot SPL, ATF, U-Boot, and so on.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alejandro_Salas_0-1726088609062.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/298632iA663B949B2E8270D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alejandro_Salas_0-1726088609062.png" alt="Alejandro_Salas_0-1726088609062.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Alejandro_Salas_0-1726088609062.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Information from&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN14093.pdf" target="_self"&gt;AN14093&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 21:04:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mplus-boot-flow/m-p/1952588#M228344</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2024-09-11T21:04:24Z</dc:date>
    </item>
  </channel>
</rss>