<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックFirmware Upgrade Scheme using emmc in imx8mplus</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Firmware-Upgrade-Scheme-using-emmc-in-imx8mplus/m-p/1951943#M228310</link>
    <description>&lt;P&gt;Do you already have A/B partitioning firmware update scheme for emmc implemented for imx8mplus boards?&lt;/P&gt;&lt;P&gt;Requirement&lt;/P&gt;&lt;P&gt;A/B system updates use two sets of partitions referred to as slots (normally slot A and slot B). The system runs from the current slot while the partitions in the unused slot are not accessed by the running system during normal operation.&lt;SPAN&gt;This approach makes updates fault resistant by keeping the unused slot as a fallback: If an error occurs during or immediately after an update, the system can rollback to the old slot and continue to have a working system. To achieve this goal, no partition used by the current slot should be updated as part of the OTA update&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 11 Sep 2024 09:22:18 GMT</pubDate>
    <dc:creator>anjuv</dc:creator>
    <dc:date>2024-09-11T09:22:18Z</dc:date>
    <item>
      <title>Firmware Upgrade Scheme using emmc in imx8mplus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Firmware-Upgrade-Scheme-using-emmc-in-imx8mplus/m-p/1951943#M228310</link>
      <description>&lt;P&gt;Do you already have A/B partitioning firmware update scheme for emmc implemented for imx8mplus boards?&lt;/P&gt;&lt;P&gt;Requirement&lt;/P&gt;&lt;P&gt;A/B system updates use two sets of partitions referred to as slots (normally slot A and slot B). The system runs from the current slot while the partitions in the unused slot are not accessed by the running system during normal operation.&lt;SPAN&gt;This approach makes updates fault resistant by keeping the unused slot as a fallback: If an error occurs during or immediately after an update, the system can rollback to the old slot and continue to have a working system. To achieve this goal, no partition used by the current slot should be updated as part of the OTA update&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 09:22:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Firmware-Upgrade-Scheme-using-emmc-in-imx8mplus/m-p/1951943#M228310</guid>
      <dc:creator>anjuv</dc:creator>
      <dc:date>2024-09-11T09:22:18Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Upgrade Scheme using emmc in imx8mplus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Firmware-Upgrade-Scheme-using-emmc-in-imx8mplus/m-p/1952421#M228339</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I believe that you are refering to Android BSP, if so then yes we do support this, please do refer to the Android User's Guide chapter&amp;nbsp;7.2 Implementing OTA update &lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/ANDROID_USERS_GUIDE.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/ANDROID_USERS_GUIDE.pdf&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 18:22:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Firmware-Upgrade-Scheme-using-emmc-in-imx8mplus/m-p/1952421#M228339</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2024-09-11T18:22:25Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Upgrade Scheme using emmc in imx8mplus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Firmware-Upgrade-Scheme-using-emmc-in-imx8mplus/m-p/1953029#M228365</link>
      <description>&lt;P&gt;No, its linux OS.&lt;/P&gt;&lt;P&gt;Board -&amp;nbsp;imx8mplus.&lt;/P&gt;&lt;P&gt;SDK -&amp;nbsp;&amp;nbsp;6.1.36 Mickledore&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 05:22:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Firmware-Upgrade-Scheme-using-emmc-in-imx8mplus/m-p/1953029#M228365</guid>
      <dc:creator>anjuv</dc:creator>
      <dc:date>2024-09-12T05:22:08Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Upgrade Scheme using emmc in imx8mplus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Firmware-Upgrade-Scheme-using-emmc-in-imx8mplus/m-p/1953682#M228389</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Then maybe SWUpdate may be an option, please have a look here:&lt;BR /&gt;&lt;A href="https://docs.nxp.com/bundle/AN13872/page/topics/double_copy_with_fall-back.html" target="_blank"&gt;https://docs.nxp.com/bundle/AN13872/page/topics/double_copy_with_fall-back.html&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 19:24:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Firmware-Upgrade-Scheme-using-emmc-in-imx8mplus/m-p/1953682#M228389</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2024-09-12T19:24:33Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Upgrade Scheme using emmc in imx8mplus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Firmware-Upgrade-Scheme-using-emmc-in-imx8mplus/m-p/1959826#M228766</link>
      <description>&lt;P&gt;Thanks&amp;nbsp;&lt;SPAN&gt;Aldo.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there any code reference available?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Sep 2024 10:38:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Firmware-Upgrade-Scheme-using-emmc-in-imx8mplus/m-p/1959826#M228766</guid>
      <dc:creator>anjuv</dc:creator>
      <dc:date>2024-09-23T10:38:04Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Upgrade Scheme using emmc in imx8mplus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Firmware-Upgrade-Scheme-using-emmc-in-imx8mplus/m-p/1960170#M228789</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Please refer to the Building SWUpdate section of the document I have shared, ther you'll find the repositories.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Mon, 23 Sep 2024 23:19:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Firmware-Upgrade-Scheme-using-emmc-in-imx8mplus/m-p/1960170#M228789</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2024-09-23T23:19:10Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware Upgrade Scheme using emmc in imx8mplus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Firmware-Upgrade-Scheme-using-emmc-in-imx8mplus/m-p/1963828#M229054</link>
      <description>&lt;P&gt;Hi Aldo,&amp;nbsp;&lt;/P&gt;&lt;P&gt;The above documentation gives the setup for imx6ull, imx8mm &amp;amp; imx93.&lt;/P&gt;&lt;P&gt;I manually made some changes to build this for imx8mplus . But I'm facing errors while running it.&lt;/P&gt;&lt;P&gt;So do you have the correct working patch of these repository files especially (&lt;EM&gt;&lt;STRONG&gt;meta-swupdate-imx &amp;amp; swupdate-scripts&lt;/STRONG&gt;&lt;/EM&gt;) to enable this feature on&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;imx8mplus-evk.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 28 Sep 2024 07:44:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Firmware-Upgrade-Scheme-using-emmc-in-imx8mplus/m-p/1963828#M229054</guid>
      <dc:creator>sanum19</dc:creator>
      <dc:date>2024-09-28T07:44:25Z</dc:date>
    </item>
  </channel>
</rss>