<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Simultaneously use eth0 and eth1 imx8mp</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Simultaneously-use-eth0-and-eth1-imx8mp/m-p/1949694#M228173</link>
    <description>&lt;P&gt;Could you provide steps / command which should be implemented to configure bridge since im new to sdk .&lt;/P&gt;</description>
    <pubDate>Mon, 09 Sep 2024 05:08:06 GMT</pubDate>
    <dc:creator>A_M01</dc:creator>
    <dc:date>2024-09-09T05:08:06Z</dc:date>
    <item>
      <title>Simultaneously use eth0 and eth1 imx8mp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Simultaneously-use-eth0-and-eth1-imx8mp/m-p/1947173#M228027</link>
      <description>&lt;P&gt;we are building the image via Yocto in evk&lt;BR /&gt;When we try to ping after making the interface (eth0)up and eth1 (up)&lt;BR /&gt;Able to ping from eth0 to same domain and eth1 to its same domain&lt;BR /&gt;eth1 is connected to laptop and iam able to ping to laptop via shared network&lt;BR /&gt;&lt;BR /&gt;but if i try to ping to 8.8.8.8&lt;/P&gt;&lt;P&gt;root@imx8mp-lpddr4-evk:~#&lt;BR /&gt;root@imx8mp-lpddr4-evk:~#&lt;BR /&gt;root@imx8mp-lpddr4-evk:~# ping -I eth0 8.8.8.8&lt;BR /&gt;PING 8.8.8.8 (8.8.8.8) from 192.168.1.100 eth0: 56(84) bytes of data.&lt;BR /&gt;^C&lt;BR /&gt;--- 8.8.8.8 ping statistics ---&lt;BR /&gt;1 packets transmitted, 0 received, 100% packet loss, time 0ms&lt;/P&gt;&lt;P&gt;root@imx8mp-lpddr4-evk:~# ping -I eth1 8.8.8.8&lt;BR /&gt;PING 8.8.8.8 (8.8.8.8) from 10.42.0.47 eth1: 56(84) bytes of data.&lt;BR /&gt;64 bytes from 8.8.8.8: icmp_seq=1 ttl=113 time=45.2 ms&lt;BR /&gt;64 bytes from 8.8.8.8: icmp_seq=2 ttl=113 time=66.3 ms&lt;BR /&gt;64 bytes from 8.8.8.8: icmp_seq=3 ttl=113 time=31.3 ms&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;root@imx8mp-lpddr4-evk:~# ping 8.8.8.8&lt;BR /&gt;PING 8.8.8.8 (8.8.8.8) 56(84) bytes of data.&lt;BR /&gt;From 192.168.1.100 icmp_seq=1 Destination Host Unreachable&lt;BR /&gt;From 192.168.1.100 icmp_seq=2 Destination Host Unreachable&lt;BR /&gt;From 192.168.1.100 icmp_seq=3 Destination Host Unreachable&lt;BR /&gt;^C&lt;BR /&gt;&lt;BR /&gt;its pinging from eth0&lt;BR /&gt;seems a routing difference&lt;BR /&gt;&lt;BR /&gt;could you please share the patch for kernel version &lt;STRONG&gt;6.1.36+gce06d21637ef&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Sep 2024 10:43:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Simultaneously-use-eth0-and-eth1-imx8mp/m-p/1947173#M228027</guid>
      <dc:creator>A_M01</dc:creator>
      <dc:date>2024-09-04T10:43:16Z</dc:date>
    </item>
    <item>
      <title>Re: Simultaneously use eth0 and eth1 imx8mp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Simultaneously-use-eth0-and-eth1-imx8mp/m-p/1948505#M228113</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/238776"&gt;@A_M01&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;That is a normal behavior due to both networks are independent.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You should configure a bridge between the networks or something like that to interconnect via software becase in hardware are independent each one.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Thu, 05 Sep 2024 19:51:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Simultaneously-use-eth0-and-eth1-imx8mp/m-p/1948505#M228113</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2024-09-05T19:51:22Z</dc:date>
    </item>
    <item>
      <title>Re: Simultaneously use eth0 and eth1 imx8mp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Simultaneously-use-eth0-and-eth1-imx8mp/m-p/1949694#M228173</link>
      <description>&lt;P&gt;Could you provide steps / command which should be implemented to configure bridge since im new to sdk .&lt;/P&gt;</description>
      <pubDate>Mon, 09 Sep 2024 05:08:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Simultaneously-use-eth0-and-eth1-imx8mp/m-p/1949694#M228173</guid>
      <dc:creator>A_M01</dc:creator>
      <dc:date>2024-09-09T05:08:06Z</dc:date>
    </item>
    <item>
      <title>Re: Simultaneously use eth0 and eth1 imx8mp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Simultaneously-use-eth0-and-eth1-imx8mp/m-p/1950268#M228207</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/238776"&gt;@A_M01&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;For the moment we don´t have examples for that.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chvaira&lt;/P&gt;</description>
      <pubDate>Mon, 09 Sep 2024 18:20:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Simultaneously-use-eth0-and-eth1-imx8mp/m-p/1950268#M228207</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2024-09-09T18:20:30Z</dc:date>
    </item>
  </channel>
</rss>