<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: USG OTG1 using the i.mx8M Mini</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USG-OTG1-using-the-i-mx8M-Mini/m-p/1948603#M228121</link>
    <description>&lt;P&gt;here is the circuit diagram which I did not attached in my question.&lt;/P&gt;</description>
    <pubDate>Fri, 06 Sep 2024 01:25:31 GMT</pubDate>
    <dc:creator>cchengwa123</dc:creator>
    <dc:date>2024-09-06T01:25:31Z</dc:date>
    <item>
      <title>USG OTG1 using the i.mx8M Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USG-OTG1-using-the-i-mx8M-Mini/m-p/1947919#M228072</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I have build my own i.mx8m mini board and I intend to set the otgusb1 to peripheral mode.&lt;/P&gt;&lt;P&gt;Please take a look at the attached section of my circuit design on the USB section of the i.mx8m Mini and the USB Type C receptacle. With this design, may I know how to configure the Device Tree file for "usbotg1" for i.mx8m Mini?&lt;/P&gt;&lt;P&gt;In addition, I like to know if there it is necessary to have a USB PD TCPC PHY IC component (example, MPN: PTN5110NHQ) for the connection of the CC1 and CC2 signals?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Sep 2024 06:58:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USG-OTG1-using-the-i-mx8M-Mini/m-p/1947919#M228072</guid>
      <dc:creator>cchengwa123</dc:creator>
      <dc:date>2024-09-05T06:58:10Z</dc:date>
    </item>
    <item>
      <title>Re: USG OTG1 using the i.mx8M Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USG-OTG1-using-the-i-mx8M-Mini/m-p/1948603#M228121</link>
      <description>&lt;P&gt;here is the circuit diagram which I did not attached in my question.&lt;/P&gt;</description>
      <pubDate>Fri, 06 Sep 2024 01:25:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USG-OTG1-using-the-i-mx8M-Mini/m-p/1948603#M228121</guid>
      <dc:creator>cchengwa123</dc:creator>
      <dc:date>2024-09-06T01:25:31Z</dc:date>
    </item>
    <item>
      <title>Re: USG OTG1 using the i.mx8M Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USG-OTG1-using-the-i-mx8M-Mini/m-p/1953957#M228405</link>
      <description>&lt;P&gt;For the usb design you need to following these tips:&lt;/P&gt;
&lt;P&gt;USB TYPE-C +CC logic chip ==&amp;gt;dual role&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;USB2.0 / USB3.0 : USB TYPE-C +CC logic chip ==&amp;gt;dual role&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;USB2.0: MicroUSB connecor + without CC logic chip ====&amp;gt;dual role&lt;/P&gt;
&lt;P&gt;Here our default BSP support usb1 dual mode"&lt;STRONG&gt;dr_mode = "otg";&lt;/STRONG&gt;"&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/arch/arm64/boot/dts/freescale/imx8mm-evk.dtsi" target="_blank"&gt;https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/arch/arm64/boot/dts/freescale/imx8mm-evk.dtsi&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;LI-WRAPPER&gt;&lt;SPAN data-teams="true"&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI-WRAPPER&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Sep 2024 05:17:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USG-OTG1-using-the-i-mx8M-Mini/m-p/1953957#M228405</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2024-09-13T05:17:13Z</dc:date>
    </item>
  </channel>
</rss>