<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.mx8mp ENET RGMII 3.3V worked</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8mp-ENET-RGMII-3-3V-worked/m-p/1948168#M228089</link>
    <description>&lt;P&gt;Hi Weidong,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a custom board with the iMX8MP processor. This processor is connected via RGMII to the 88LX5153 (G.hn Digital Chip MxL), which can configure its controller as either MAC or PHY.&lt;/P&gt;&lt;P&gt;In this case, it's set up as PHY to connect it to the iMX8MP. However, its voltage for the RGMII is 2.5V. In the design, I connected the NVCC_SAI1_SAI5 pin to 2.5V. Is this correct? Can it function properly at this voltage without issues? Should I consider anything else? Perhaps in boot strapping or DTB configuration?&lt;/P&gt;&lt;P&gt;The design is based on the iMX8MP-EVK evaluation board. Right now, the eth0 interface isn't coming up. During boot, these messages appear:&lt;/P&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;SPAN class=""&gt;Net:&lt;/SPAN&gt; Could &lt;SPAN class=""&gt;not&lt;/SPAN&gt; &lt;SPAN class=""&gt;get&lt;/SPAN&gt; PHY &lt;SPAN class=""&gt;for&lt;/SPAN&gt; FEC0: addr &lt;SPAN class=""&gt;1&lt;/SPAN&gt; Could &lt;SPAN class=""&gt;not&lt;/SPAN&gt; &lt;SPAN class=""&gt;get&lt;/SPAN&gt; PHY &lt;SPAN class=""&gt;for&lt;/SPAN&gt; FEC0: addr &lt;SPAN class=""&gt;1&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;[ &lt;SPAN class=""&gt;2.966142&lt;/SPAN&gt;] mdio_bus &lt;SPAN class=""&gt;30&lt;/SPAN&gt;be0000.ethernet-&lt;SPAN class=""&gt;1&lt;/SPAN&gt;: MDIO device at address &lt;SPAN class=""&gt;1&lt;/SPAN&gt; &lt;SPAN class=""&gt;is&lt;/SPAN&gt; missing.&lt;/DIV&gt;&lt;DIV class=""&gt;[ &lt;SPAN class=""&gt;2.974045&lt;/SPAN&gt;] fec &lt;SPAN class=""&gt;30&lt;/SPAN&gt;be0000.ethernet eth0: registered PHC device &lt;SPAN class=""&gt;0&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;Can you help me try to solve this problem?&lt;BR /&gt;Thank you.&lt;/P&gt;&lt;P&gt;Toni.&lt;/P&gt;</description>
    <pubDate>Thu, 05 Sep 2024 10:27:56 GMT</pubDate>
    <dc:creator>anhira</dc:creator>
    <dc:date>2024-09-05T10:27:56Z</dc:date>
    <item>
      <title>i.mx8mp ENET RGMII 3.3V worked</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8mp-ENET-RGMII-3-3V-worked/m-p/1828300#M221262</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We want to use RGMII on i.mx8mp, but the ENET uses 3.3V. Could it work?&lt;/P&gt;&lt;P&gt;I tested 3.3V on ENET and found RGMII worked. However, in datasheet, RGMII requestes 1.8V only.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you give advice if it riskly, like stability?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR.&lt;/P&gt;&lt;P&gt;Hunt Yang&lt;/P&gt;</description>
      <pubDate>Thu, 14 Mar 2024 09:27:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx8mp-ENET-RGMII-3-3V-worked/m-p/1828300#M221262</guid>
      <dc:creator>WALNUTY</dc:creator>
      <dc:date>2024-03-14T09:27:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx8mp ENET RGMII 3.3V worked</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8mp-ENET-RGMII-3-3V-worked/m-p/1828912#M221295</link>
      <description>&lt;P&gt;Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219951"&gt;@WALNUTY&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;See the following screeshot, which is from i.MX8MP datasheet.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="weidong_sun_0-1710465096443.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/268546i4EED62FB6640DAED/image-size/medium?v=v2&amp;amp;px=400" role="button" title="weidong_sun_0-1710465096443.png" alt="weidong_sun_0-1710465096443.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;weidong_sun_0-1710465096443.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;NVCC_ENET &amp;amp; NVCC_SAI1_SAI5 can be suppied by 3.3V.&lt;/P&gt;
&lt;P&gt;So for Ethernet IO, 3.3V power is no problem.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;&amp;gt;&amp;gt;Could you give advice if it riskly, like stability?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Most of gigabit Phy products supports 1.8V / 2.5V IO, it is easy to buy from current market. Actually ethernet phy with 3.3V can also be got, but few kinds of the products. I have ever used KSZ9031, which supports 3.3V IO, you can check it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks!&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 01:19:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx8mp-ENET-RGMII-3-3V-worked/m-p/1828912#M221295</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2024-03-15T01:19:50Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx8mp ENET RGMII 3.3V worked</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8mp-ENET-RGMII-3-3V-worked/m-p/1948168#M228089</link>
      <description>&lt;P&gt;Hi Weidong,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a custom board with the iMX8MP processor. This processor is connected via RGMII to the 88LX5153 (G.hn Digital Chip MxL), which can configure its controller as either MAC or PHY.&lt;/P&gt;&lt;P&gt;In this case, it's set up as PHY to connect it to the iMX8MP. However, its voltage for the RGMII is 2.5V. In the design, I connected the NVCC_SAI1_SAI5 pin to 2.5V. Is this correct? Can it function properly at this voltage without issues? Should I consider anything else? Perhaps in boot strapping or DTB configuration?&lt;/P&gt;&lt;P&gt;The design is based on the iMX8MP-EVK evaluation board. Right now, the eth0 interface isn't coming up. During boot, these messages appear:&lt;/P&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;SPAN class=""&gt;Net:&lt;/SPAN&gt; Could &lt;SPAN class=""&gt;not&lt;/SPAN&gt; &lt;SPAN class=""&gt;get&lt;/SPAN&gt; PHY &lt;SPAN class=""&gt;for&lt;/SPAN&gt; FEC0: addr &lt;SPAN class=""&gt;1&lt;/SPAN&gt; Could &lt;SPAN class=""&gt;not&lt;/SPAN&gt; &lt;SPAN class=""&gt;get&lt;/SPAN&gt; PHY &lt;SPAN class=""&gt;for&lt;/SPAN&gt; FEC0: addr &lt;SPAN class=""&gt;1&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;[ &lt;SPAN class=""&gt;2.966142&lt;/SPAN&gt;] mdio_bus &lt;SPAN class=""&gt;30&lt;/SPAN&gt;be0000.ethernet-&lt;SPAN class=""&gt;1&lt;/SPAN&gt;: MDIO device at address &lt;SPAN class=""&gt;1&lt;/SPAN&gt; &lt;SPAN class=""&gt;is&lt;/SPAN&gt; missing.&lt;/DIV&gt;&lt;DIV class=""&gt;[ &lt;SPAN class=""&gt;2.974045&lt;/SPAN&gt;] fec &lt;SPAN class=""&gt;30&lt;/SPAN&gt;be0000.ethernet eth0: registered PHC device &lt;SPAN class=""&gt;0&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;Can you help me try to solve this problem?&lt;BR /&gt;Thank you.&lt;/P&gt;&lt;P&gt;Toni.&lt;/P&gt;</description>
      <pubDate>Thu, 05 Sep 2024 10:27:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx8mp-ENET-RGMII-3-3V-worked/m-p/1948168#M228089</guid>
      <dc:creator>anhira</dc:creator>
      <dc:date>2024-09-05T10:27:56Z</dc:date>
    </item>
  </channel>
</rss>