<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: imx93,rm67199 driver not work</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1947628#M228052</link>
    <description>&lt;P&gt;老哥，我也是自己添加了屏幕，跟你报一样的错，请问是最后是怎么解决的啊？&lt;/P&gt;</description>
    <pubDate>Thu, 05 Sep 2024 01:09:50 GMT</pubDate>
    <dc:creator>周蔷123</dc:creator>
    <dc:date>2024-09-05T01:09:50Z</dc:date>
    <item>
      <title>imx93,rm67199 driver not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1884144#M224722</link>
      <description>&lt;P&gt;Hello:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; I am debugging the rm67199 on IMX93.I have already downloaded the image such as:Image and&amp;nbsp;imx93-11x11-evk-rm67199.dtb.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;But the log reported error and the driver of rm67199 cann't work.The log is as follows&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Can you help me?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot SPL 2023.04-dirty (Jun 03 2024 - 21:53:22 -0700)&lt;BR /&gt;SOC: 0xa1009300&lt;BR /&gt;LC: 0x2040010&lt;BR /&gt;PMIC: PCA9451A&lt;BR /&gt;PMIC: Over Drive Voltage Mode&lt;BR /&gt;DDR: 1866MTS&lt;BR /&gt;M33 prepare ok&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from BOOTROM&lt;BR /&gt;Boot Stage: Primary boot&lt;BR /&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;BR /&gt;Load image from 0x52400 by ROM_API&lt;BR /&gt;NOTICE: BL31: v2.8(release):lf-6.1.55-2.2.0-0-g08e9d4eef&lt;BR /&gt;NOTICE: BL31: Built : 06:43:30, Nov 21 2023&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2023.04-dirty (Jun 03 2024 - 21:53:22 -0700)&lt;/P&gt;&lt;P&gt;CPU: i.MX93(52) rev1.1 1700 MHz (running at 1692 MHz)&lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 28C&lt;BR /&gt;Reset cause: POR (0x1)&lt;BR /&gt;Model: NXP i.MX93 11X11 EVK board&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;tcpc_init: Can't find device id=0x52&lt;BR /&gt;setup_typec: tcpc portpd init failed, err=-19&lt;BR /&gt;setup_pd_switch: Can't find device id=0x73&lt;BR /&gt;TCPC: Vendor ID [0x33ef], Product ID [0x190c], Addr [I2C2 0x51]&lt;BR /&gt;tcpc_clear_alert dm_i2c_write failed, err -110&lt;BR /&gt;setup_typec: tcpc port1 init failed, err=-5&lt;BR /&gt;pca953x gpio@22: Error reading output register&lt;BR /&gt;Core: 226 devices, 36 uclasses, devicetree: separate&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Loading Environment from MMC... OK&lt;BR /&gt;[*]-Video Link 0adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device hdmi@3d&lt;BR /&gt;fail to get display timings&lt;BR /&gt;probe video device failed, ret -19&lt;/P&gt;&lt;P&gt;[0] lcd-controller@4ae30000, video&lt;BR /&gt;[1] dsi@4ae10000, video_bridge&lt;BR /&gt;[2] hdmi@3d, panel&lt;BR /&gt;adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device hdmi@3d&lt;BR /&gt;fail to get display timings&lt;BR /&gt;probe video device failed, ret -19&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ELE firmware version 0.1.0-44880904&lt;/P&gt;&lt;P&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;Net: pca953x gpio@22: Error reading output register&lt;BR /&gt;pca953x gpio@22: Error reading output register&lt;BR /&gt;Could not get PHY for FEC0: addr 2&lt;BR /&gt;pca953x gpio@22: Error reading output register&lt;BR /&gt;pca953x gpio@22: Error reading output register&lt;BR /&gt;Could not get PHY for FEC0: addr 2&lt;BR /&gt;pca953x gpio@22: Error reading output register&lt;BR /&gt;pca953x gpio@22: Error reading output register&lt;BR /&gt;eth1: ethernet@428a0000 [PRIME]&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;Working FDT set to 83000000&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0(part 0) is current device&lt;BR /&gt;** No partition table - mmc 0 **&lt;BR /&gt;Couldn't find partition mmc 0:1&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Scanning mmc 1:1...&lt;BR /&gt;65579 bytes read in 5 ms (12.5 MiB/s)&lt;BR /&gt;Working FDT set to 83000000&lt;BR /&gt;Unable to open OP-TEE session (err=-5)&lt;BR /&gt;mm_communicate failed!&lt;BR /&gt;Error: Cannot initialize UEFI sub-system, r = 3&lt;BR /&gt;starting USB...&lt;BR /&gt;Bus usb@4c100000: tcpc_init: Polling TCPC POWER STATUS Initialization Status bit failed, ret = -5&lt;BR /&gt;tcpc_get_cc_status dm_i2c_read failed, err 3&lt;BR /&gt;tcpc_send_command dm_i2c_write failed, err -110&lt;BR /&gt;tcpc_send_command dm_i2c_write failed, err 3&lt;BR /&gt;tcpc_get_cc_status dm_i2c_read failed, err 3&lt;BR /&gt;Port not available.&lt;BR /&gt;Bus usb@4c200000: tcpc_setup_ufp_mode: Polling ALERT register, TCPC_ALERT_CC_STATUS bit failed, ret = -62&lt;BR /&gt;Port not available.&lt;BR /&gt;USB is stopped. Please issue 'usb start' first.&lt;BR /&gt;Running BSP bootcmd ...&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Failed to load 'boot.scr'&lt;BR /&gt;35009024 bytes read in 377 ms (88.6 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;65579 bytes read in 5 ms (12.5 MiB/s)&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt;Booting using the fdt blob at 0x83000000&lt;BR /&gt;Working FDT set to 83000000&lt;BR /&gt;Using Device Tree in place at 0000000083000000, end 000000008301302a&lt;BR /&gt;Working FDT set to 83000000&lt;BR /&gt;adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device hdmi@3d&lt;BR /&gt;fail to get display timings&lt;BR /&gt;probe video device failed, ret -19&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x412fd050]&lt;BR /&gt;[ 0.000000] Linux version 6.6.3-gccf0a99701a7-dirty (tangyuan@ubuntu) (aarch64-poky-linux-gcc (GCC) 12.3.0, GNU ld (GNU Binutils) 2.40.0.20230703) #2 SMP PREEMPT Mon Jun 10 00:01:36 PDT 2024&lt;BR /&gt;[ 0.000000] KASLR disabled due to lack of seed&lt;BR /&gt;[ 0.000000] Machine model: NXP i.MX93 11X11 EVK board&lt;BR /&gt;[ 0.000000] efi: UEFI not found.&lt;BR /&gt;[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000b0000000, size 256 MiB&lt;BR /&gt;[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x00000000b0000000..0x00000000bfffffff (262144 KiB) map reusable linux,cma&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x000000002021e000..0x000000002021efff (4 KiB) nomap non-reusable rsc-table@2021e000&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x0000000096000000..0x0000000097dfffff (30720 KiB) nomap non-reusable optee_core@96000000&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x0000000097e00000..0x0000000097ffffff (2048 KiB) nomap non-reusable optee_shm@97e00000&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x00000000a4000000..0x00000000a4007fff (32 KiB) nomap non-reusable vdev0vring0@a4000000&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x00000000a4008000..0x00000000a400ffff (32 KiB) nomap non-reusable vdev0vring1@a4008000&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x00000000a4010000..0x00000000a4017fff (32 KiB) nomap non-reusable vdev1vring0@a4010000&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x00000000a4018000..0x00000000a401ffff (32 KiB) nomap non-reusable vdev1vring1@a4018000&lt;BR /&gt;[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4020000, size 1 MiB&lt;BR /&gt;[ 0.000000] OF: reserved mem: initialized node vdevbuffer@a4020000, compatible id shared-dma-pool&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x00000000a4020000..0x00000000a411ffff (1024 KiB) nomap non-reusable vdevbuffer@a4020000&lt;BR /&gt;[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4120000, size 1 MiB&lt;BR /&gt;[ 0.000000] OF: reserved mem: initialized node ele-reserved@a4120000, compatible id shared-dma-pool&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x00000000a4120000..0x00000000a421ffff (1024 KiB) nomap non-reusable ele-reserved@a4120000&lt;BR /&gt;[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000c0000000, size 256 MiB&lt;BR /&gt;[ 0.000000] OF: reserved mem: initialized node ethosu_region@C0000000, compatible id shared-dma-pool&lt;BR /&gt;[ 0.000000] OF: reserved mem: 0x00000000c0000000..0x00000000cfffffff (262144 KiB) map reusable ethosu_region@C0000000&lt;BR /&gt;[ 0.000000] earlycon: lpuart32 at MMIO32 0x0000000044380000 (options '')&lt;BR /&gt;[ 0.000000] printk: bootconsole [lpuart32] enabled&lt;BR /&gt;[ 0.000000] NUMA: No NUMA configuration found&lt;BR /&gt;[ 0.000000] NUMA: Faking a node at [mem 0x0000000080000000-0x00000000ffffffff]&lt;BR /&gt;[ 0.000000] NUMA: NODE_DATA [mem 0xffbc76c0-0xffbc9fff]&lt;BR /&gt;[ 0.000000] Zone ranges:&lt;BR /&gt;[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]&lt;BR /&gt;[ 0.000000] DMA32 empty&lt;BR /&gt;[ 0.000000] Normal empty&lt;BR /&gt;[ 0.000000] Movable zone start for each node&lt;BR /&gt;[ 0.000000] Early memory node ranges&lt;BR /&gt;[ 0.000000] node 0: [mem 0x0000000080000000-0x0000000095ffffff]&lt;BR /&gt;[ 0.000000] node 0: [mem 0x0000000098000000-0x00000000a3ffffff]&lt;BR /&gt;[ 0.000000] node 0: [mem 0x00000000a4000000-0x00000000a421ffff]&lt;BR /&gt;[ 0.000000] node 0: [mem 0x00000000a4220000-0x00000000ffffffff]&lt;BR /&gt;[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]&lt;BR /&gt;[ 0.000000] On node 0, zone DMA: 8192 pages in unavailable ranges&lt;BR /&gt;[ 0.000000] psci: probing for conduit method from DT.&lt;BR /&gt;[ 0.000000] psci: PSCIv1.1 detected in firmware.&lt;BR /&gt;[ 0.000000] psci: Using standard PSCI v0.2 function IDs&lt;BR /&gt;[ 0.000000] psci: Trusted OS migration not required&lt;BR /&gt;[ 0.000000] psci: SMC Calling Convention v1.2&lt;BR /&gt;[ 0.000000] percpu: Embedded 22 pages/cpu s50536 r8192 d31384 u90112&lt;BR /&gt;[ 0.000000] Detected VIPT I-cache on CPU0&lt;BR /&gt;[ 0.000000] CPU features: detected: GIC system register CPU interface&lt;BR /&gt;[ 0.000000] CPU features: detected: Virtualization Host Extensions&lt;BR /&gt;[ 0.000000] CPU features: detected: Qualcomm erratum 1009, or ARM erratum 1286807, 2441009&lt;BR /&gt;[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923&lt;BR /&gt;[ 0.000000] alternatives: applying boot alternatives&lt;BR /&gt;[ 0.000000] Kernel command line: console=ttyLP0,115200 earlycon root=/dev/mmcblk1p2 rootwait rw&lt;BR /&gt;[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)&lt;BR /&gt;[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)&lt;BR /&gt;[ 0.000000] Fallback order for Node 0: 0&lt;BR /&gt;[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 507904&lt;BR /&gt;[ 0.000000] Policy zone: DMA&lt;BR /&gt;[ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off&lt;BR /&gt;[ 0.000000] software IO TLB: area num 2.&lt;BR /&gt;[ 0.000000] software IO TLB: mapped [mem 0x00000000f9800000-0x00000000fd800000] (64MB)&lt;BR /&gt;[ 0.000000] Memory: 1396328K/2064384K available (20864K kernel code, 1612K rwdata, 7628K rodata, 3904K init, 634K bss, 143768K reserved, 524288K cma-reserved)&lt;BR /&gt;[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1&lt;BR /&gt;[ 0.000000] rcu: Preemptible hierarchical RCU implementation.&lt;BR /&gt;[ 0.000000] rcu: RCU event tracing is enabled.&lt;BR /&gt;[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.&lt;BR /&gt;[ 0.000000] Trampoline variant of Tasks RCU enabled.&lt;BR /&gt;[ 0.000000] Tracing variant of Tasks RCU enabled.&lt;BR /&gt;[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.&lt;BR /&gt;[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2&lt;BR /&gt;[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0&lt;BR /&gt;[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode&lt;BR /&gt;[ 0.000000] GICv3: 960 SPIs implemented&lt;BR /&gt;[ 0.000000] GICv3: 0 Extended SPIs implemented&lt;BR /&gt;[ 0.000000] Root IRQ handler: gic_handle_irq&lt;BR /&gt;[ 0.000000] GICv3: GICv3 features: 16 PPIs&lt;BR /&gt;[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000048040000&lt;BR /&gt;[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.&lt;BR /&gt;[ 0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (phys).&lt;BR /&gt;[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns&lt;BR /&gt;[ 0.000000] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns&lt;BR /&gt;[ 0.008445] Console: colour dummy device 80x25&lt;BR /&gt;[ 0.012704] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=96000)&lt;BR /&gt;[ 0.022860] pid_max: default: 32768 minimum: 301&lt;BR /&gt;[ 0.027504] LSM: initializing lsm=capability,integrity&lt;BR /&gt;[ 0.032658] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.039935] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.048572] cacheinfo: Unable to detect cache hierarchy for CPU 0&lt;BR /&gt;[ 0.055045] RCU Tasks: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1.&lt;BR /&gt;[ 0.061915] RCU Tasks Trace: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1.&lt;BR /&gt;[ 0.069550] rcu: Hierarchical SRCU implementation.&lt;BR /&gt;[ 0.074144] rcu: Max phase no-delay instances is 1000.&lt;BR /&gt;[ 0.080421] EFI services will not be available.&lt;BR /&gt;[ 0.085003] smp: Bringing up secondary CPUs ...&lt;BR /&gt;[ 0.089748] Detected VIPT I-cache on CPU1&lt;BR /&gt;[ 0.089822] GICv3: CPU1: found redistributor 100 region 0:0x0000000048060000&lt;BR /&gt;[ 0.089871] CPU1: Booted secondary processor 0x0000000100 [0x412fd050]&lt;BR /&gt;[ 0.090005] smp: Brought up 1 node, 2 CPUs&lt;BR /&gt;[ 0.111366] SMP: Total of 2 processors activated.&lt;BR /&gt;[ 0.116035] CPU features: detected: 32-bit EL0 Support&lt;BR /&gt;[ 0.121160] CPU features: detected: 32-bit EL1 Support&lt;BR /&gt;[ 0.126264] CPU features: detected: Data cache clean to the PoU not required for I/D coherence&lt;BR /&gt;[ 0.134845] CPU features: detected: Common not Private translations&lt;BR /&gt;[ 0.141078] CPU features: detected: CRC32 instructions&lt;BR /&gt;[ 0.146203] CPU features: detected: RCpc load-acquire (LDAPR)&lt;BR /&gt;[ 0.151912] CPU features: detected: LSE atomic instructions&lt;BR /&gt;[ 0.157458] CPU features: detected: Privileged Access Never&lt;BR /&gt;[ 0.163003] CPU features: detected: RAS Extension Support&lt;BR /&gt;[ 0.168380] CPU features: detected: Speculative Store Bypassing Safe (SSBS)&lt;BR /&gt;[ 0.175372] CPU: All CPU(s) started at EL2&lt;BR /&gt;[ 0.179385] alternatives: applying system-wide alternatives&lt;BR /&gt;[ 0.190888] devtmpfs: initialized&lt;BR /&gt;[ 0.200175] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns&lt;BR /&gt;[ 0.209689] futex hash table entries: 512 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.225921] pinctrl core: initialized pinctrl subsystem&lt;BR /&gt;[ 0.232934] DMI not present or invalid.&lt;BR /&gt;[ 0.237066] NET: Registered PF_NETLINK/PF_ROUTE protocol family&lt;BR /&gt;[ 0.243540] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations&lt;BR /&gt;[ 0.250485] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations&lt;BR /&gt;[ 0.258150] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations&lt;BR /&gt;[ 0.266013] audit: initializing netlink subsys (disabled)&lt;BR /&gt;[ 0.271527] audit: type=2000 audit(0.180:1): state=initialized audit_enabled=0 res=1&lt;BR /&gt;[ 0.271977] thermal_sys: Registered thermal governor 'step_wise'&lt;BR /&gt;[ 0.279036] thermal_sys: Registered thermal governor 'power_allocator'&lt;BR /&gt;[ 0.285047] cpuidle: using governor menu&lt;BR /&gt;[ 0.295637] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.&lt;BR /&gt;[ 0.302219] ASID allocator initialised with 65536 entries&lt;BR /&gt;[ 0.308413] Serial: AMBA PL011 UART driver&lt;BR /&gt;[ 0.312317] imx mu driver is registered.&lt;BR /&gt;[ 0.316151] imx rpmsg driver is registered.&lt;BR /&gt;[ 0.327094] imx93-pinctrl 443c0000.pinctrl: initialized IMX pinctrl driver&lt;BR /&gt;[ 0.340851] platform 4ae10000.dsi: Fixed dependency cycle(s) with /soc@0/dsi@4ae10000/panel@0/port/endpoint&lt;BR /&gt;[ 0.350608] platform 4ae30000.lcd-controller: Fixed dependency cycle(s) with /soc@0/dsi@4ae10000/ports/port@0/endpoint&lt;BR /&gt;[ 0.364221] Modules: 24048 pages in range for non-PLT usage&lt;BR /&gt;[ 0.364235] Modules: 515568 pages in range for PLT usage&lt;BR /&gt;[ 0.370532] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.382351] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page&lt;BR /&gt;[ 0.388589] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.395348] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page&lt;BR /&gt;[ 0.401588] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.408347] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page&lt;BR /&gt;[ 0.414588] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.421347] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page&lt;BR /&gt;[ 0.429622] ACPI: Interpreter disabled.&lt;BR /&gt;[ 0.434188] iommu: Default domain type: Translated&lt;BR /&gt;[ 0.438746] iommu: DMA domain TLB invalidation policy: strict mode&lt;BR /&gt;[ 0.445203] SCSI subsystem initialized&lt;BR /&gt;[ 0.449064] usbcore: registered new interface driver usbfs&lt;BR /&gt;[ 0.454309] usbcore: registered new interface driver hub&lt;BR /&gt;[ 0.459601] usbcore: registered new device driver usb&lt;BR /&gt;[ 0.465642] mc: Linux media interface: v0.10&lt;BR /&gt;[ 0.469700] videodev: Linux video capture interface: v2.00&lt;BR /&gt;[ 0.475165] pps_core: LinuxPPS API ver. 1 registered&lt;BR /&gt;[ 0.480049] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;giometti@linux.it&amp;gt;&lt;BR /&gt;[ 0.489155] PTP clock support registered&lt;BR /&gt;[ 0.493212] EDAC MC: Ver: 3.0.0&lt;BR /&gt;[ 0.496790] scmi_core: SCMI protocol bus registered&lt;BR /&gt;[ 0.502063] FPGA manager framework&lt;BR /&gt;[ 0.505272] Advanced Linux Sound Architecture Driver Initialized.&lt;BR /&gt;[ 0.511921] Bluetooth: Core ver 2.22&lt;BR /&gt;[ 0.515261] NET: Registered PF_BLUETOOTH protocol family&lt;BR /&gt;[ 0.520532] Bluetooth: HCI device and connection manager initialized&lt;BR /&gt;[ 0.526856] Bluetooth: HCI socket layer initialized&lt;BR /&gt;[ 0.531704] Bluetooth: L2CAP socket layer initialized&lt;BR /&gt;[ 0.536740] Bluetooth: SCO socket layer initialized&lt;BR /&gt;[ 0.542014] vgaarb: loaded&lt;BR /&gt;[ 0.545299] clocksource: Switched to clocksource arch_sys_counter&lt;BR /&gt;[ 0.551443] VFS: Disk quotas dquot_6.6.0&lt;BR /&gt;[ 0.555137] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)&lt;BR /&gt;[ 0.562117] pnp: PnP ACPI: disabled&lt;BR /&gt;[ 0.570786] NET: Registered PF_INET protocol family&lt;BR /&gt;[ 0.575626] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)&lt;BR /&gt;[ 0.583994] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)&lt;BR /&gt;[ 0.592344] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)&lt;BR /&gt;[ 0.599989] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)&lt;BR /&gt;[ 0.607930] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)&lt;BR /&gt;[ 0.615766] TCP: Hash tables configured (established 16384 bind 16384)&lt;BR /&gt;[ 0.622179] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.628740] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.635955] NET: Registered PF_UNIX/PF_LOCAL protocol family&lt;BR /&gt;[ 0.641876] RPC: Registered named UNIX socket transport module.&lt;BR /&gt;[ 0.647546] RPC: Registered udp transport module.&lt;BR /&gt;[ 0.652213] RPC: Registered tcp transport module.&lt;BR /&gt;[ 0.656891] RPC: Registered tcp-with-tls transport module.&lt;BR /&gt;[ 0.662353] RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;[ 0.669622] PCI: CLS 0 bytes, default 64&lt;BR /&gt;[ 0.673599] kvm [1]: IPA Size Limit: 40 bits&lt;BR /&gt;[ 0.677632] kvm [1]: GICv3: no GICV resource entry&lt;BR /&gt;[ 0.682375] kvm [1]: disabling GICv2 emulation&lt;BR /&gt;[ 0.686811] kvm [1]: GIC system register CPU interface enabled&lt;BR /&gt;[ 0.692630] kvm [1]: vgic interrupt IRQ9&lt;BR /&gt;[ 0.696526] kvm [1]: VHE mode initialized successfully&lt;BR /&gt;[ 0.702784] Initialise system trusted keyrings&lt;BR /&gt;[ 0.707212] workingset: timestamp_bits=42 max_order=19 bucket_order=0&lt;BR /&gt;[ 0.713722] squashfs: version 4.0 (2009/01/31) Phillip Lougher&lt;BR /&gt;[ 0.719617] NFS: Registering the id_resolver key type&lt;BR /&gt;[ 0.724459] Key type id_resolver registered&lt;BR /&gt;[ 0.728567] Key type id_legacy registered&lt;BR /&gt;[ 0.732573] nfs4filelayout_init: NFSv4 File Layout Driver Registering...&lt;BR /&gt;[ 0.739236] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...&lt;BR /&gt;[ 0.746612] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;BR /&gt;[ 0.752901] 9p: Installing v9fs 9p2000 file system support&lt;BR /&gt;[ 0.780607] Key type asymmetric registered&lt;BR /&gt;[ 0.784442] Asymmetric key parser 'x509' registered&lt;BR /&gt;[ 0.789349] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)&lt;BR /&gt;[ 0.796663] io scheduler mq-deadline registered&lt;BR /&gt;[ 0.801178] io scheduler kyber registered&lt;BR /&gt;[ 0.805190] io scheduler bfq registered&lt;BR /&gt;[ 0.814277] EINJ: ACPI disabled.&lt;BR /&gt;[ 0.822442] Bus freq driver module loaded&lt;BR /&gt;[ 0.832571] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled&lt;BR /&gt;[ 0.850821] printk: console [ttyLP0] enabled0x44380010 (irq = 17, base_baud = 1500000) is a FSL_LPUART&lt;BR /&gt;[ 0.850821] printk: console [ttyLP0] enabled&lt;BR /&gt;[ 0.859244] printk: bootconsole [lpuart32] disabled&lt;BR /&gt;[ 0.859244] printk: bootconsole [lpuart32] disabled&lt;BR /&gt;[ 0.884765] loop: module loaded&lt;BR /&gt;[ 0.889395] megasas: 07.725.01.00-rc1&lt;BR /&gt;[ 0.898961] tun: Universal TUN/TAP device driver, 1.6&lt;BR /&gt;[ 0.904892] thunder_xcv, ver 1.0&lt;BR /&gt;[ 0.908185] thunder_bgx, ver 1.0&lt;BR /&gt;[ 0.911430] nicpf, ver 1.0&lt;BR /&gt;[ 0.915254] pps pps0: new PPS source ptp0&lt;BR /&gt;[ 0.920267] fec 42890000.ethernet: Invalid MAC address: 00:00:00:00:00:00&lt;BR /&gt;[ 0.927108] fec 42890000.ethernet: Using random MAC address: de:86:74:8b:ea:31&lt;BR /&gt;[ 0.935737] mdio_bus 42890000.ethernet-1: MDIO device at address 2 is missing.&lt;BR /&gt;[ 0.943546] fec 42890000.ethernet eth0: registered PHC device 0&lt;BR /&gt;[ 0.951233] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version&lt;BR /&gt;[ 0.958488] hns3: Copyright (c) 2017 Huawei Corporation.&lt;BR /&gt;[ 0.963849] hclge is initializing&lt;BR /&gt;[ 0.967211] e1000: Intel(R) PRO/1000 Network Driver&lt;BR /&gt;[ 0.972084] e1000: Copyright (c) 1999-2006 Intel Corporation.&lt;BR /&gt;[ 0.977845] e1000e: Intel(R) PRO/1000 Network Driver&lt;BR /&gt;[ 0.982804] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.&lt;BR /&gt;[ 0.988731] igb: Intel(R) Gigabit Ethernet Network Driver&lt;BR /&gt;[ 0.994124] igb: Copyright (c) 2007-2014 Intel Corporation.&lt;BR /&gt;[ 0.999704] igbvf: Intel(R) Gigabit Virtual Function Network Driver&lt;BR /&gt;[ 1.005983] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.&lt;BR /&gt;[ 1.012126] sky2: driver version 1.30&lt;BR /&gt;[ 1.016318] usbcore: registered new device driver r8152-cfgselector&lt;BR /&gt;[ 1.022619] usbcore: registered new interface driver r8152&lt;BR /&gt;[ 1.028693] VFIO - User Level meta-driver version: 0.3&lt;BR /&gt;[ 1.036180] usbcore: registered new interface driver uas&lt;BR /&gt;[ 1.041545] usbcore: registered new interface driver usb-storage&lt;BR /&gt;[ 1.047610] usbcore: registered new interface driver usbserial_generic&lt;BR /&gt;[ 1.054152] usbserial: USB Serial support registered for generic&lt;BR /&gt;[ 1.060159] usbcore: registered new interface driver ftdi_sio&lt;BR /&gt;[ 1.065903] usbserial: USB Serial support registered for FTDI USB Serial Device&lt;BR /&gt;[ 1.073213] usbcore: registered new interface driver usb_serial_simple&lt;BR /&gt;[ 1.079792] usbserial: USB Serial support registered for carelink&lt;BR /&gt;[ 1.085895] usbserial: USB Serial support registered for flashloader&lt;BR /&gt;[ 1.092250] usbserial: USB Serial support registered for funsoft&lt;BR /&gt;[ 1.098255] usbserial: USB Serial support registered for google&lt;BR /&gt;[ 1.104180] usbserial: USB Serial support registered for hp4x&lt;BR /&gt;[ 1.109929] usbserial: USB Serial support registered for kaufmann&lt;BR /&gt;[ 1.116023] usbserial: USB Serial support registered for libtransistor&lt;BR /&gt;[ 1.122548] usbserial: USB Serial support registered for moto_modem&lt;BR /&gt;[ 1.128813] usbserial: USB Serial support registered for motorola_tetra&lt;BR /&gt;[ 1.135426] usbserial: USB Serial support registered for nokia&lt;BR /&gt;[ 1.141265] usbserial: USB Serial support registered for novatel_gps&lt;BR /&gt;[ 1.147624] usbserial: USB Serial support registered for siemens_mpi&lt;BR /&gt;[ 1.153982] usbserial: USB Serial support registered for suunto&lt;BR /&gt;[ 1.159900] usbserial: USB Serial support registered for vivopay&lt;BR /&gt;[ 1.165906] usbserial: USB Serial support registered for zio&lt;BR /&gt;[ 1.171574] usbcore: registered new interface driver usb_ehset_test&lt;BR /&gt;[ 1.181396] input: 44440000.bbnsm:pwrkey as /devices/platform/soc@0/44000000.bus/44440000.bbnsm/44440000.bbnsm:pwrkey/input/input0&lt;BR /&gt;[ 1.196817] bbnsm_rtc 44440000.bbnsm:rtc: registered as rtc0&lt;BR /&gt;[ 1.203161] bbnsm_rtc 44440000.bbnsm:rtc: setting system clock to 1970-01-01T00:00:00 UTC (0)&lt;BR /&gt;[ 1.212590] i2c_dev: i2c /dev entries driver&lt;BR /&gt;[ 1.219178] qoriq_thermal 44482000.tmu: invalid range data.&lt;BR /&gt;[ 1.226297] imx7ulp-wdt 42490000.watchdog: imx93 wdt probe&lt;BR /&gt;[ 1.260685] Bluetooth: HCI UART driver ver 2.3&lt;BR /&gt;[ 1.265179] Bluetooth: HCI UART protocol H4 registered&lt;BR /&gt;[ 1.270313] Bluetooth: HCI UART protocol BCSP registered&lt;BR /&gt;[ 1.275638] Bluetooth: HCI UART protocol LL registered&lt;BR /&gt;[ 1.280764] Bluetooth: HCI UART protocol ATH3K registered&lt;BR /&gt;[ 1.286167] Bluetooth: HCI UART protocol Three-wire (H5) registered&lt;BR /&gt;[ 1.292603] Bluetooth: HCI UART protocol Broadcom registered&lt;BR /&gt;[ 1.298273] Bluetooth: HCI UART protocol QCA registered&lt;BR /&gt;[ 1.305001] sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;[ 1.311224] sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;[ 1.316108] Synopsys Designware Multimedia Card Interface Driver&lt;BR /&gt;[ 1.322592] sdhci-pltfm: SDHCI platform and OF driver helper&lt;BR /&gt;[ 1.329815] ledtrig-cpu: registered to indicate activity on CPUs&lt;BR /&gt;[ 1.337172] fsl-se-fw se-fw2: assigned reserved memory node ele-reserved@a4120000&lt;BR /&gt;[ 1.346704] fsl-se-fw se-fw2: Successfully registered ele-trng&lt;BR /&gt;[ 1.352666] random: crng init done&lt;BR /&gt;[ 1.352992] fsl-se-fw se-fw2: i.MX secure-enclave: mu2 interface to firmware, configured.&lt;BR /&gt;[ 1.364344] mmc0: SDHCI controller on 42850000.mmc [42850000.mmc] using ADMA&lt;BR /&gt;[ 1.364475] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....&lt;BR /&gt;[ 1.378221] usbcore: registered new interface driver usbhid&lt;BR /&gt;[ 1.383838] usbhid: USB HID core driver&lt;BR /&gt;[ 1.390054] mxc-isi_v1 4ae40000.isi: mxc_isi.0 registered successfully&lt;BR /&gt;[ 1.398936] ethosu ethosu: assigned reserved memory node ethosu_region@C0000000&lt;BR /&gt;[ 1.445842] hw perfevents: enabled with armv8_cortex_a55 PMU driver, 7 counters available&lt;BR /&gt;[ 1.456614] cs_system_cfg: CoreSight Configuration manager initialised&lt;BR /&gt;[ 1.464977] optee: probing for conduit method.&lt;BR /&gt;[ 1.469537] optee: revision 4.0 (a303fc80)&lt;BR /&gt;[ 1.470143] optee: dynamic shared memory is enabled&lt;BR /&gt;[ 1.479504] optee: initialized driver&lt;BR /&gt;[ 1.487779] NET: Registered PF_LLC protocol family&lt;BR /&gt;[ 1.492703] u32 classifier&lt;BR /&gt;[ 1.495424] input device check on&lt;BR /&gt;[ 1.499080] Actions configured&lt;BR /&gt;[ 1.499092] mmc0: new HS400 Enhanced strobe MMC card at address 0001&lt;BR /&gt;[ 1.502946] NET: Registered PF_INET6 protocol family&lt;BR /&gt;[ 1.509499] mmcblk0: mmc0:0001 DA6016 14.7 GiB&lt;BR /&gt;[ 1.514728] Segment Routing with IPv6&lt;BR /&gt;[ 1.522117] In-situ OAM (IOAM) with IPv6&lt;BR /&gt;[ 1.522486] mmcblk0boot0: mmc0:0001 DA6016 4.00 MiB&lt;BR /&gt;[ 1.526192] NET: Registered PF_PACKET protocol family&lt;BR /&gt;[ 1.532237] mmcblk0boot1: mmc0:0001 DA6016 4.00 MiB&lt;BR /&gt;[ 1.536078] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.&lt;BR /&gt;[ 1.542037] mmcblk0rpmb: mmc0:0001 DA6016 4.00 MiB, chardev (234:0)&lt;BR /&gt;[ 1.554070] Bluetooth: RFCOMM TTY layer initialized&lt;BR /&gt;[ 1.565036] Bluetooth: RFCOMM socket layer initialized&lt;BR /&gt;[ 1.570185] Bluetooth: RFCOMM ver 1.11&lt;BR /&gt;[ 1.573939] Bluetooth: BNEP (Ethernet Emulation) ver 1.3&lt;BR /&gt;[ 1.579243] Bluetooth: BNEP filters: protocol multicast&lt;BR /&gt;[ 1.584467] Bluetooth: BNEP socket layer initialized&lt;BR /&gt;[ 1.589427] Bluetooth: HIDP (Human Interface Emulation) ver 1.2&lt;BR /&gt;[ 1.595341] Bluetooth: HIDP socket layer initialized&lt;BR /&gt;[ 1.600647] 8021q: 802.1Q VLAN Support v1.8&lt;BR /&gt;[ 1.604876] lib80211: common routines for IEEE802.11 drivers&lt;BR /&gt;[ 1.610585] 9pnet: Installing 9P2000 support&lt;BR /&gt;[ 1.615001] Key type dns_resolver registered&lt;BR /&gt;[ 1.632494] registered taskstats version 1&lt;BR /&gt;[ 1.636947] Loading compiled-in X.509 certificates&lt;BR /&gt;[ 1.668910] usb_phy_generic usbphynop1: dummy supplies not allowed for exclusive requests&lt;BR /&gt;[ 1.677339] usb_phy_generic usbphynop2: dummy supplies not allowed for exclusive requests&lt;BR /&gt;[ 1.699727] imx9_init_soc 47510000.efuse:imx93-soc: error -EINVAL: failed to register SoC device&lt;BR /&gt;[ 1.708551] imx9_init_soc: probe of 47510000.efuse:imx93-soc failed with error -22&lt;BR /&gt;[ 1.717987] mipi-dsi 4ae10000.dsi.0: Fixed dependency cycle(s) with /soc@0/dsi@4ae10000/ports/port@1/endpoint&lt;BR /&gt;[ 1.728793] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)&lt;BR /&gt;[ 1.736832] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517&lt;BR /&gt;[ 1.746936] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517&lt;BR /&gt;[ 1.756855] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517&lt;BR /&gt;[ 1.769033] imx-dwmac 428a0000.ethernet: IRQ eth_lpi not found&lt;BR /&gt;[ 1.775979] imx-dwmac 428a0000.ethernet: User ID: 0x10, Synopsys ID: 0x52&lt;BR /&gt;[ 1.782802] imx-dwmac 428a0000.ethernet: DWMAC4/5&lt;BR /&gt;[ 1.787586] imx-dwmac 428a0000.ethernet: DMA HW capability register supported&lt;BR /&gt;[ 1.794706] imx-dwmac 428a0000.ethernet: RX Checksum Offload Engine supported&lt;BR /&gt;[ 1.801829] imx-dwmac 428a0000.ethernet: TX Checksum insertion supported&lt;BR /&gt;[ 1.808519] imx-dwmac 428a0000.ethernet: Wake-Up On Lan supported&lt;BR /&gt;[ 1.814672] imx-dwmac 428a0000.ethernet: Enable RX Mitigation via HW Watchdog Timer&lt;BR /&gt;[ 1.822327] imx-dwmac 428a0000.ethernet: device MAC address de:9d:60:72:47:bb&lt;BR /&gt;[ 1.829473] imx-dwmac 428a0000.ethernet: Enabled L3L4 Flow TC (entries=8)&lt;BR /&gt;[ 1.836255] imx-dwmac 428a0000.ethernet: Enabled RFS Flow TC (entries=10)&lt;BR /&gt;[ 1.843037] imx-dwmac 428a0000.ethernet: Enabling HW TC (entries=256, max_off=256)&lt;BR /&gt;[ 1.850599] imx-dwmac 428a0000.ethernet: Using 32/32 bits DMA host/device width&lt;BR /&gt;[ 1.868771] remoteproc remoteproc0: imx-rproc is available&lt;BR /&gt;[ 1.885706] st_lsm6dsx_i2c 0-006a: supply vdd not found, using dummy regulator&lt;BR /&gt;[ 1.893093] st_lsm6dsx_i2c 0-006a: supply vddio not found, using dummy regulator&lt;BR /&gt;[ 1.957428] st_lsm6dsx_i2c 0-006a: failed to read whoami register&lt;BR /&gt;[ 1.963743] st_lsm6dsx_i2c: probe of 0-006a failed with error -5&lt;BR /&gt;[ 1.970129] i2c i2c-0: LPI2C adapter registered&lt;BR /&gt;[ 1.976661] pca953x 1-0022: supply vcc not found, using dummy regulator&lt;BR /&gt;[ 1.983441] pca953x 1-0022: using AI&lt;BR /&gt;[ 1.987130] pca953x 1-0022: failed writing register&lt;BR /&gt;[ 1.992176] pca953x: probe of 1-0022 failed with error -5&lt;BR /&gt;[ 1.997940] adp5585 1-0034: Failed to read reg 0x00, ret is -5&lt;BR /&gt;[ 2.003776] adp5585: probe of 1-0034 failed with error -5&lt;BR /&gt;[ 2.009280] i2c i2c-1: LPI2C adapter registered&lt;BR /&gt;[ 2.015058] i2c 2-0050: Fixed dependency cycle(s) with /soc@0/usb@4c100000/port/endpoint&lt;BR /&gt;[ 2.023493] tcpci: probe of 2-0050 failed with error -5&lt;BR /&gt;[ 2.028898] i2c 2-0051: Fixed dependency cycle(s) with /soc@0/usb@4c200000/port/endpoint&lt;BR /&gt;[ 2.038005] adp5585 2-0034: Failed to read reg 0x00, ret is -5&lt;BR /&gt;[ 2.043868] adp5585: probe of 2-0034 failed with error -5&lt;BR /&gt;[ 2.049494] i2c 2-003c: Fixed dependency cycle(s) with /soc@0/bus@42800000/camera/csi@4ae00000/port/endpoint&lt;BR /&gt;[ 2.059587] i2c i2c-2: LPI2C adapter registered&lt;BR /&gt;[ 2.066492] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)&lt;BR /&gt;[ 2.074503] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517&lt;BR /&gt;[ 2.084604] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517&lt;BR /&gt;[ 2.094535] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517&lt;BR /&gt;[ 2.119149] dwc-mipi-csi2-host 4ae00000.csi: lanes: 2, name: mxc-mipi-csi2.0&lt;BR /&gt;[ 2.119405] sdhci-esdhc-imx 42860000.mmc: Got CD GPIO&lt;BR /&gt;[ 2.137766] OF: graph: no port node found in /soc@0/bus@42000000/i2c@42530000/tcpc@51/connector&lt;BR /&gt;[ 2.146518] OF: graph: no port node found in /soc@0/bus@42000000/i2c@42530000/tcpc@51/connector&lt;BR /&gt;[ 2.155227] OF: graph: no port node found in /soc@0/bus@42000000/i2c@42530000/tcpc@51/connector&lt;BR /&gt;[ 2.164407] mmc1: SDHCI controller on 42860000.mmc [42860000.mmc] using ADMA&lt;BR /&gt;[ 2.175564] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)&lt;BR /&gt;[ 2.183579] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517&lt;BR /&gt;[ 2.193686] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517&lt;BR /&gt;[ 2.203635] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517&lt;BR /&gt;[ 2.227268] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)&lt;BR /&gt;[ 2.235374] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517&lt;BR /&gt;[ 2.245481] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517&lt;BR /&gt;[ 2.252130] mmc1: host does not support reading read-only switch, assuming write-enable&lt;BR /&gt;[ 2.263396] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517&lt;BR /&gt;[ 2.286155] cfg80211: Loading compiled-in X.509 certificates for regulatory database&lt;BR /&gt;[ 2.290257] mmc1: new ultra high speed SDR104 SDHC card at address 0001&lt;BR /&gt;[ 2.295753] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'&lt;BR /&gt;[ 2.301144] mmcblk1: mmc1:0001 SD16G 14.8 GiB&lt;BR /&gt;[ 2.306374] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2&lt;BR /&gt;[ 2.311171] clk: Disabling unused clocks&lt;BR /&gt;[ 2.319328] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db&lt;BR /&gt;[ 2.324525] mmcblk1: p1 p2&lt;BR /&gt;[ 2.331180] ALSA device list:&lt;BR /&gt;[ 2.336738] No soundcards found.&lt;BR /&gt;[ 2.336794] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)&lt;BR /&gt;[ 2.348116] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517&lt;BR /&gt;[ 2.358229] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517&lt;BR /&gt;[ 2.368182] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517&lt;BR /&gt;[ 2.400406] EXT4-fs (mmcblk1p2): recovery complete&lt;BR /&gt;[ 2.406511] EXT4-fs (mmcblk1p2): mounted filesystem 0ff2bc0a-e3a2-498e-8b3f-84260506d66a r/w with ordered data mode. Quota mode: none.&lt;BR /&gt;[ 2.418709] VFS: Mounted root (ext4 filesystem) on device 179:98.&lt;BR /&gt;[ 2.430013] devtmpfs: mounted&lt;BR /&gt;[ 2.434944] Freeing unused kernel memory: 3904K&lt;BR /&gt;[ 2.439653] Run /sbin/init as init process&lt;BR /&gt;[ 2.982741] systemd[1]: System time before build time, advancing clock.&lt;BR /&gt;[ 3.051177] systemd[1]: systemd 245.4-4ubuntu3.22 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD +IDN2 -IDN +PCRE2 default-hierarchy=hybrid)&lt;BR /&gt;[ 3.074300] systemd[1]: Detected architecture arm64.&lt;/P&gt;&lt;P&gt;Welcome to Ubuntu 20.04.6 LTS!&lt;/P&gt;&lt;P&gt;[ 3.143473] systemd[1]: Set hostname to &amp;lt;localhost.localdomain&amp;gt;.&lt;BR /&gt;[ 3.184576] systemd[1]: memfd_create() called without MFD_EXEC or MFD_NOEXEC_SEAL set&lt;BR /&gt;[ 3.732941] systemd[1]: Created slice system-getty.slice.&lt;BR /&gt;[ OK ] Created slice system-getty.slice.&lt;BR /&gt;[ 3.754627] systemd[1]: Created slice system-modprobe.slice.&lt;BR /&gt;[ OK ] Created slice system-modprobe.slice.&lt;BR /&gt;[ 3.778653] systemd[1]: Created slice system-serial\x2dgetty.slice.&lt;BR /&gt;[ OK ] Created slice system-serial\x2dgetty.slice.&lt;BR /&gt;[ 3.802484] systemd[1]: Created slice User and Session Slice.&lt;BR /&gt;[ OK ] Created slice User and Session Slice.&lt;BR /&gt;[ 3.825808] systemd[1]: Started Forward Password Requests to Wall Directory Watch.&lt;BR /&gt;[ OK ] Started Forward Password R…uests to Wall Directory Watch.&lt;BR /&gt;[ 3.849625] systemd[1]: Condition check resulted in Arbitrary Executable File Formats File System Automount Point being skipped.&lt;BR /&gt;[ 3.861479] systemd[1]: Reached target User and Group Name Lookups.&lt;BR /&gt;[ OK ] Reached target User and Group Name Lookups.&lt;BR /&gt;[ 3.885489] systemd[1]: Reached target Remote File Systems.&lt;BR /&gt;[ OK ] Reached target Remote File Systems.&lt;BR /&gt;[ 3.905441] systemd[1]: Reached target Slices.&lt;BR /&gt;[ OK ] Reached target Slices.&lt;BR /&gt;[ 3.925467] systemd[1]: Reached target Mounting snaps.&lt;BR /&gt;[ OK ] Reached target Mounting snaps.&lt;BR /&gt;[ 3.945432] systemd[1]: Reached target Mounted snaps.&lt;BR /&gt;[ OK ] Reached target Mounted snaps.&lt;BR /&gt;[ 3.965470] systemd[1]: Reached target Swap.&lt;BR /&gt;[ OK ] Reached target Swap.&lt;BR /&gt;[ 3.985883] systemd[1]: Listening on initctl Compatibility Named Pipe.&lt;BR /&gt;[ OK ] Listening on initctl Compatibility Named Pipe.&lt;BR /&gt;[ 4.010357] systemd[1]: Listening on Journal Audit Socket.&lt;BR /&gt;[ OK ] Listening on Journal Audit Socket.&lt;BR /&gt;[ 4.034026] systemd[1]: Listening on Journal Socket (/dev/log).&lt;BR /&gt;[ OK ] Listening on Journal Socket (/dev/log).&lt;BR /&gt;[ 4.058120] systemd[1]: Listening on Journal Socket.&lt;BR /&gt;[ OK ] Listening on Journal Socket.&lt;BR /&gt;[ 4.078154] systemd[1]: Listening on udev Control Socket.&lt;BR /&gt;[ OK ] Listening on udev Control Socket.&lt;BR /&gt;[ 4.101947] systemd[1]: Listening on udev Kernel Socket.&lt;BR /&gt;[ OK ] Listening on udev Kernel Socket.&lt;BR /&gt;[ 4.137874] systemd[1]: Mounting Huge Pages File System...&lt;BR /&gt;Mounting Huge Pages File System...&lt;BR /&gt;[ 4.162448] systemd[1]: Mounting POSIX Message Queue File System...&lt;BR /&gt;Mounting POSIX Message Queue File System...&lt;BR /&gt;[ 4.191321] systemd[1]: Mounting Kernel Debug File System...&lt;BR /&gt;Mounting Kernel Debug File System...&lt;BR /&gt;[ 4.213912] systemd[1]: Condition check resulted in Kernel Trace File System being skipped.&lt;BR /&gt;[ 4.242134] systemd[1]: Starting Journal Service...&lt;BR /&gt;Starting Journal Service...&lt;BR /&gt;[ 4.262024] systemd[1]: Condition check resulted in Create list of static device nodes for the current kernel being skipped.&lt;BR /&gt;[ 4.279706] systemd[1]: Starting Load Kernel Module chromeos_pstore...&lt;BR /&gt;Starting Load Kernel Module chromeos_pstore...&lt;BR /&gt;[ 4.313778] systemd[1]: Condition check resulted in Load Kernel Module drm being skipped.&lt;BR /&gt;[ 4.322329] systemd[1]: Condition check resulted in Load Kernel Module efi_pstore being skipped.&lt;BR /&gt;[ 4.350253] systemd[1]: Starting Load Kernel Module pstore_blk...&lt;BR /&gt;Starting Load Kernel Module pstore_blk...&lt;BR /&gt;[ 4.398074] systemd[1]: Starting Load Kernel Module pstore_zone...&lt;BR /&gt;Starting Load Kernel Module pstore_zone...&lt;BR /&gt;[ 4.426080] systemd[1]: Starting Load Kernel Module ramoops...&lt;BR /&gt;Starting Load Kernel Module ramoops...&lt;BR /&gt;[ 4.451617] systemd[1]: Condition check resulted in Set Up Additional Binary Formats being skipped.&lt;BR /&gt;[ 4.482092] systemd[1]: Starting Load Kernel Modules...&lt;BR /&gt;Starting Load Kernel Modules...&lt;BR /&gt;[ 4.508433] systemd[1]: Starting Remount Root and Kernel File Systems...&lt;BR /&gt;Starting Remount Root and Kernel File Systems...&lt;BR /&gt;[ 4.550123] systemd[1]: Starting udev Coldplug all Devices...&lt;BR /&gt;Starting udev Coldplug all Devices...&lt;BR /&gt;[ 4.574546] systemd[1]: Started Journal Service.&lt;BR /&gt;[ OK ] Started Journal Service.&lt;BR /&gt;[ OK ] Mounted Huge Pages File System.&lt;BR /&gt;[ OK ] Mounted POSIX Message Queue File System.&lt;BR /&gt;[ OK ] Mounted Kernel Debug File System.&lt;BR /&gt;[ OK ] Finished Load Kernel Module chromeos_pstore.&lt;BR /&gt;[ OK ] Finished Load Kernel Module pstore_blk.&lt;BR /&gt;[ OK ] Finished Load Kernel Module pstore_zone.&lt;BR /&gt;[ OK ] Finished Load Kernel Module ramoops.&lt;BR /&gt;[FAILED] Failed to start Load Kernel Modules.&lt;BR /&gt;See 'systemctl status systemd-modules-load.service' for details.&lt;BR /&gt;[ OK ] Finished Remount Root and Kernel File Systems.&lt;BR /&gt;Mounting Kernel Configuration File System...&lt;BR /&gt;Starting Flush Journal to Persistent Storage...&lt;BR /&gt;Starting Load/Save Random Seed...&lt;BR /&gt;Starting Apply Kernel Variables...&lt;BR /&gt;[ 4.914648] systemd-journald[138]: Received client request to flush runtime journal.&lt;BR /&gt;Starting Create System Users...&lt;BR /&gt;[ OK ] Mounted Kernel Configuration File System.&lt;BR /&gt;[ 5.031203] systemd-journald[138]: File /var/log/journal/f5fb6edf91414bdcbd789249cb473871/system.journal corrupted or uncleanly shut down, renaming and replacing.&lt;BR /&gt;[ OK ] Finished udev Coldplug all Devices.&lt;BR /&gt;[ OK ] Finished Load/Save Random Seed.&lt;BR /&gt;[ OK ] Finished Apply Kernel Variables.&lt;BR /&gt;[ OK ] Finished Create System Users.&lt;BR /&gt;Starting Create Static Device Nodes in /dev...&lt;BR /&gt;[ OK ] Finished Create Static Device Nodes in /dev.&lt;BR /&gt;[ OK ] Reached target Local File Systems (Pre).&lt;BR /&gt;[ OK ] Reached target Local File Systems.&lt;BR /&gt;Starting Tell Plymouth To Write Out Runtime Data...&lt;BR /&gt;Starting udev Kernel Device Manager...&lt;BR /&gt;[ OK ] Finished Flush Journal to Persistent Storage.&lt;BR /&gt;[ OK ] Finished Tell Plymouth To Write Out Runtime Data.&lt;BR /&gt;Starting Create Volatile Files and Directories...&lt;BR /&gt;[ OK ] Finished Create Volatile Files and Directories.&lt;BR /&gt;Starting Network Name Resolution...&lt;BR /&gt;Starting Network Time Synchronization...&lt;BR /&gt;Starting Update UTMP about System Boot/Shutdown...&lt;BR /&gt;[ OK ] Started udev Kernel Device Manager.&lt;BR /&gt;[ OK ] Finished Update UTMP about System Boot/Shutdown.&lt;BR /&gt;[ OK ] Started Dispatch Password …ts to Console Directory Watch.&lt;BR /&gt;[ OK ] Reached target Local Encrypted Volumes.&lt;BR /&gt;[ OK ] Started Network Time Synchronization.&lt;BR /&gt;[ OK ] Reached target System Initialization.&lt;BR /&gt;[ OK ] Started CUPS Scheduler.&lt;BR /&gt;[ OK ] Started Daily Cleanup of Temporary Directories.&lt;BR /&gt;[ OK ] Reached target Paths.&lt;BR /&gt;[ OK ] Reached target System Time Set.&lt;BR /&gt;[ OK ] Reached target System Time Synchronized.&lt;BR /&gt;[ OK ] Started Trigger anacron every hour.&lt;BR /&gt;[ OK ] Started Daily apt download activities.&lt;BR /&gt;[ OK ] Started Daily apt upgrade and clean activities.&lt;BR /&gt;[ OK ] Started Periodic ext4 Onli…ata Check for All Filesystems.&lt;BR /&gt;[ OK ] Started Discard unused blocks once a week.&lt;BR /&gt;[ OK ] Started Refresh fwupd metadata regularly.&lt;BR /&gt;[ OK ] Started Daily man-db regeneration.&lt;BR /&gt;[ OK ] Started Message of the Day.&lt;BR /&gt;[ OK ] Reached target Timers.&lt;BR /&gt;[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.&lt;BR /&gt;[ OK ] Listening on CUPS Scheduler.&lt;BR /&gt;[ OK ] Listening on D-Bus System Message Bus Socket.&lt;BR /&gt;Starting Socket activation for snappy daemon.&lt;BR /&gt;[ OK ] Started Network Name Resolution.&lt;BR /&gt;[ OK ] Listening on Socket activation for snappy daemon.&lt;BR /&gt;[ OK ] Reached target Host and Network Name Lookups.&lt;BR /&gt;[ OK ] Reached target Sockets.&lt;BR /&gt;[ OK ] Reached target Basic System.&lt;BR /&gt;Starting Accounts Service...&lt;BR /&gt;[ OK ] Started Run anacron jobs.&lt;BR /&gt;Starting LSB: automatic crash report generation...&lt;BR /&gt;Starting Avahi mDNS/DNS-SD Stack...&lt;BR /&gt;Starting Bluetooth management mechanism...&lt;BR /&gt;[ OK ] Started Regular background program processing daemon.&lt;BR /&gt;[ OK ] Started CUPS Scheduler.&lt;BR /&gt;[ OK ] Started D-Bus System Message Bus.&lt;BR /&gt;Starting Network Manager...&lt;BR /&gt;Starting Remove Stale Onli…t4 Metadata Check Snapshots...&lt;BR /&gt;Starting Initialize hardware monitoring sensors...&lt;BR /&gt;Starting Dispatcher daemon for systemd-networkd...&lt;BR /&gt;[ OK ] Started Set the CPU Frequency Scaling governor.&lt;BR /&gt;Starting Authorization Manager...&lt;BR /&gt;Starting Restore /etc/reso… the ppp link was shut down...&lt;BR /&gt;[ OK ] Reached target Login Prompts (Pre).&lt;BR /&gt;Starting Snap Daemon...&lt;BR /&gt;Starting Switcheroo Control Proxy service...&lt;BR /&gt;Starting Login Service...&lt;BR /&gt;Starting WPA supplicant...&lt;BR /&gt;[ OK ] Finished Restore /etc/reso…re the ppp link was shut down.&lt;BR /&gt;[ OK ] Finished Initialize hardware monitoring sensors.&lt;BR /&gt;[ OK ] Started LSB: automatic crash report generation.&lt;BR /&gt;[ OK ] Started Login Service.&lt;BR /&gt;[ OK ] Started WPA supplicant.&lt;BR /&gt;[ OK ] Started Avahi mDNS/DNS-SD Stack.&lt;BR /&gt;[ OK ] Started Switcheroo Control Proxy service.&lt;BR /&gt;[ OK ] Started Make remote CUPS printers available locally.&lt;BR /&gt;[ OK ] Started Authorization Manager.&lt;BR /&gt;Starting Modem Manager...&lt;BR /&gt;[ OK ] Started Network Manager.&lt;BR /&gt;[ OK ] Reached target Network.&lt;BR /&gt;Starting Network Manager Wait Online...&lt;BR /&gt;Starting Permit User Sessions...&lt;BR /&gt;[ OK ] Started Unattended Upgrades Shutdown.&lt;BR /&gt;[ OK ] Finished Permit User Sessions.&lt;BR /&gt;[ OK ] Started Accounts Service.&lt;BR /&gt;Starting Light Display Manager...&lt;BR /&gt;Starting Hold until boot process finishes up...&lt;BR /&gt;Starting Hostname Service...&lt;BR /&gt;[ OK ] Finished Hold until boot process finishes up.&lt;BR /&gt;[ OK ] Started Getty on tty1.&lt;BR /&gt;[ OK ] Started Hostname Service.&lt;BR /&gt;[ OK ] Started Light Display Manager.&lt;BR /&gt;[ OK ] Started Modem Manager.&lt;BR /&gt;Starting Network Manager Script Dispatcher Service...&lt;BR /&gt;[ OK ] Finished Remove Stale Onli…ext4 Metadata Check Snapshots.&lt;BR /&gt;[ OK ] Started Network Manager Script Dispatcher Service.&lt;BR /&gt;[ OK ] Started Snap Daemon.&lt;BR /&gt;[ OK ] Started Dispatcher daemon for systemd-networkd.&lt;BR /&gt;Starting Wait until snapd is fully seeded...&lt;BR /&gt;Starting Time &amp;amp; Date Service...&lt;BR /&gt;[ OK ] Started Time &amp;amp; Date Service.&lt;BR /&gt;[ 12.440938] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517&lt;BR /&gt;[ OK ] Finished Wait until [ 12.470227] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517&lt;BR /&gt;snapd is fully seeded.&lt;BR /&gt;[ 12.504731] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517&lt;BR /&gt;[ OK ] Found device /dev/ttyLP0.&lt;BR /&gt;[ OK ] Started Serial Getty on ttyLP0.&lt;BR /&gt;[ OK ] Reached target Login Prompts.&lt;/P&gt;&lt;P&gt;Ubuntu 20.04.6 LTS localhost.localdomain ttyLP0&lt;/P&gt;&lt;P&gt;localhost login:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The critical error is as follows:&lt;/P&gt;&lt;P&gt;[ 2.336794] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)&lt;BR /&gt;[ 2.348116] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517&lt;BR /&gt;[ 2.358229] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517&lt;BR /&gt;[ 2.368182] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jun 2024 09:13:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1884144#M224722</guid>
      <dc:creator>5454ty</dc:creator>
      <dc:date>2024-06-10T09:13:04Z</dc:date>
    </item>
    <item>
      <title>Re: imx93,rm67199 driver not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1885847#M224857</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191789"&gt;@5454ty&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please share all of your test step? Also our i.mx93 do not support ubuntu OS.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 08:37:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1885847#M224857</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2024-06-12T08:37:00Z</dc:date>
    </item>
    <item>
      <title>Re: imx93,rm67199 driver not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1887684#M224981</link>
      <description>&lt;P&gt;您好，&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; 张工，我可以用中文嘛&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;我是用TF卡来烧写的，&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;其实我暂时没有接我自己的新屏，我是这么想的，我首先在软件层次把RM67199跑起来，至少保证流程没错把，可是我加载了后，发现没有RM67191或者是RM67199的信息，PROBE函数加了打印也没有打&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;这个是我TF卡的内容&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="5454ty_0-1718351750181.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/284179i49D1ED7B77DBD0C0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="5454ty_0-1718351750181.png" alt="5454ty_0-1718351750181.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;我TF卡里面有Image和imx93-11x11-evk-rm67199.dtb，&lt;/P&gt;&lt;P&gt;其他另外个分区是文件系统&lt;/P&gt;&lt;P&gt;我的UBOOT信息如下：&lt;/P&gt;&lt;P&gt;u-boot=&amp;gt;&lt;BR /&gt;u-boot=&amp;gt; print&lt;BR /&gt;arch=arm&lt;BR /&gt;auth_os=auth_cntr ${cntr_addr}&lt;BR /&gt;baudrate=115200&lt;BR /&gt;board=imx93_evk&lt;BR /&gt;board_name=11X11_EVK&lt;BR /&gt;board_rev=iMX93&lt;BR /&gt;boot_a_script=load ${devtype} ${devnum}:${distro_bootpart} ${scriptaddr} ${prefix}${script}; source ${scriptaddr}&lt;BR /&gt;boot_efi_binary=load ${devtype} ${devnum}:${distro_bootpart} ${kernel_addr_r} efi/boot/bootaa64.efi; if fdt addr -q ${fdt_addr_r}; then bootefi ${kernel_addr_r} ${fdt_addr_r};else bootefi ${kernel_addr_r} ${fdtcontroladdr};fi&lt;BR /&gt;boot_efi_bootmgr=if fdt addr -q ${fdt_addr_r}; then bootefi bootmgr ${fdt_addr_r};else bootefi bootmgr;fi&lt;BR /&gt;boot_extlinux=sysboot ${devtype} ${devnum}:${distro_bootpart} any ${scriptaddr} ${prefix}${boot_syslinux_conf}&lt;BR /&gt;boot_fit=no&lt;BR /&gt;boot_net_usb_start=usb start&lt;BR /&gt;boot_os=booti ${loadaddr} - ${fdt_addr_r};&lt;BR /&gt;boot_prefixes=/ /boot/&lt;BR /&gt;boot_script_dhcp=boot.scr.uimg&lt;BR /&gt;boot_scripts=boot.scr.uimg boot.scr&lt;BR /&gt;boot_syslinux_conf=extlinux/extlinux.conf&lt;BR /&gt;boot_targets=mmc0 mmc1 usb0&lt;BR /&gt;bootargs=console=ttyLP0,115200 earlycon root=/dev/mmcblk1p2 rootwait rw&lt;BR /&gt;bootcmd=run sr_ir_v2_cmd;run distro_bootcmd;run bsp_bootcmd&lt;BR /&gt;bootcmd_mfg=run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot auto; fi;&lt;BR /&gt;bootcmd_mmc0=devnum=0; run mmc_boot&lt;BR /&gt;bootcmd_mmc1=devnum=1; run mmc_boot&lt;BR /&gt;bootcmd_usb0=devnum=0; run usb_boot&lt;BR /&gt;bootdelay=2&lt;BR /&gt;bootfstype=fat&lt;BR /&gt;bootm_size=0x10000000&lt;BR /&gt;bootscript=echo Running bootscript from mmc ...; source&lt;BR /&gt;bsp_bootcmd=echo Running BSP bootcmd ...; mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if test ${sec_boot} = yes; then if run loadcntr; then run mmcboot; else run netboot; fi; else if run loadimage; then run mmcboot; else run netboot; fi; fi; fi; fi;&lt;BR /&gt;cntr_addr=0x98000000&lt;BR /&gt;cntr_file=os_cntr_signed.bin&lt;BR /&gt;console=ttyLP0,115200 earlycon&lt;BR /&gt;cpu=armv8&lt;BR /&gt;distro_bootcmd=for target in ${boot_targets}; do run bootcmd_${target}; done&lt;BR /&gt;distro_bootpart_uuid=076c4a2a-01&lt;BR /&gt;efi_dtb_prefixes=/ /dtb/ /dtb/current/&lt;BR /&gt;emmc_dev=0&lt;BR /&gt;eth1addr=16:5c:70:e4:6d:96&lt;BR /&gt;ethact=ethernet@428a0000&lt;BR /&gt;ethprime=eth1&lt;BR /&gt;fastboot_dev=mmc1&lt;BR /&gt;fdt_addr=0x83000000&lt;BR /&gt;fdt_addr_r=0x83000000&lt;BR /&gt;fdt_file=imx93-11x11-evk-rm67199.dtb&lt;BR /&gt;fdt_high=0xffffffffffffffff&lt;BR /&gt;fdtaddr=83000000&lt;BR /&gt;fdtcontroladdr=fced2890&lt;BR /&gt;fdtfile=imx93-11x11-evk-rm67199.dtb&lt;BR /&gt;fileaddr=80400000&lt;BR /&gt;filesize=2163200&lt;BR /&gt;ftdfile=imx93-11x11-evk-rm67199.dtb&lt;BR /&gt;image=Image&lt;BR /&gt;initrd_addr=0x83800000&lt;BR /&gt;initrd_high=0xffffffffffffffff&lt;BR /&gt;jh_mmcboot=setenv fdtfile ${jh_root_dtb}; setenv jh_clk clk_ignore_unused mem=1248MB kvm-arm.mode=nvhe; if run loadimage; then run mmcboot;else run jh_netboot; fi;&lt;BR /&gt;jh_netboot=setenv fdtfile ${jh_root_dtb}; setenv jh_clk clk_ignore_unused mem=1248MB kvm-arm.mode=nvhe; run netboot;&lt;BR /&gt;jh_root_dtb=imx93-11x11-evk-root.dtb&lt;BR /&gt;kboot=booti&lt;BR /&gt;kernel_addr_r=0x80400000&lt;BR /&gt;load_efi_dtb=load ${devtype} ${devnum}:${distro_bootpart} ${fdt_addr_r} ${prefix}${efi_fdtfile}&lt;BR /&gt;loadaddr=0x80400000&lt;BR /&gt;loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};&lt;BR /&gt;loadcntr=fatload mmc ${mmcdev}:${mmcpart} ${cntr_addr} ${cntr_file}&lt;BR /&gt;loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr_r} ${fdtfile}&lt;BR /&gt;loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}&lt;BR /&gt;mfgtool_args=setenv bootargs console=${console},${baudrate} rdinit=/linuxrc clk_ignore_unused&lt;BR /&gt;mmc_boot=if mmc dev ${devnum}; then devtype=mmc; run scan_dev_for_boot_part; fi&lt;BR /&gt;mmcargs=setenv bootargs ${jh_clk} ${mcore_clk} console=${console} root=${mmcroot}&lt;BR /&gt;mmcautodetect=yes&lt;BR /&gt;mmcboot=echo Booting from mmc ...; run mmcargs; if test ${sec_boot} = yes; then if run auth_os; then run boot_os; else echo ERR: failed to authenticate; fi; else if test ${boot_fit} = yes || test ${boot_fit} = try; then bootm ${loadaddr}; else if run loadfdt; then run boot_os; else echo WARN: Cannot load the DT; fi; fi;fi;&lt;BR /&gt;mmcdev=1&lt;BR /&gt;mmcpart=1&lt;BR /&gt;mmcroot=/dev/mmcblk1p2 rootwait rw&lt;BR /&gt;netargs=setenv bootargs ${jh_clk} ${mcore_clk} console=${console} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp&lt;BR /&gt;netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if test ${sec_boot} = yes; then ${get_cmd} ${cntr_addr} ${cntr_file}; if run auth_os; then run boot_os; else echo ERR: failed to authenticate; fi; else ${get_cmd} ${loadaddr} ${image}; if test ${boot_fit} = yes || test ${boot_fit} = try; then bootm ${loadaddr}; else if ${get_cmd} ${fdt_addr_r} ${fdtfile}; then run boot_os; else echo WARN: Cannot load the DT; fi; fi;fi;&lt;BR /&gt;nodes=/usbg1 /usbg2 /wdt-reboot /rm67199_panel /dsi-host /display-subsystem /soc@0/bus@44000000/dma-controller@44000000 /soc@0/bus@44000000/sai@443b0000 /soc@0/bus@44000000/mqs1 /soc@0/bus@44000000/bbnsm@44440000 /soc@0/bus@44000000/system-controller@44460000 /soc@0/bus@44000000/tmu@44482000 /soc@0/bus@44000000/micfil@44520000 /soc@0/bus@42000000/dma-controller@42000000 /soc@0/bus@44000000/i3c-master@44330000 /soc@0/bus@42000000/i3c-master@42520000 /soc@0/bus@42000000/sai@42650000 /soc@0/bus@42000000/sai@42660000 /soc@0/bus@42000000/mqs2 /soc@0/bus@42000000/xcvr@42680000 /soc@0/bus@42000000/flexio@425c0000 /soc@0/bus@42800000/epxp@4ae20000 /soc@0/bus@42800000/camera /soc@0/efuse@47510000 /soc@0/system-controller@4ac10000 /soc@0/ldb@4ac10020 /soc@0/phy@4ac10024 /soc@0/ele-mu /soc@0/dsi@4ae10000 /soc@0/lcd-controller@4ae30000 /soc@0/blk-ctrl@4e010000 /soc@0/memory-controller@4e300000 /soc@0/bus@44000000/i2c@44350000/pmic@25 /imx93-lpm&lt;BR /&gt;prepare_mcore=setenv mcore_clk clk-imx93.mcore_booted;&lt;BR /&gt;scan_dev_for_boot=echo Scanning ${devtype} ${devnum}:${distro_bootpart}...; for prefix in ${boot_prefixes}; do run scan_dev_for_extlinux; run scan_dev_for_scripts; done;run scan_dev_for_efi;&lt;BR /&gt;scan_dev_for_boot_part=part list ${devtype} ${devnum} -bootable devplist; env exists devplist || setenv devplist 1; for distro_bootpart in ${devplist}; do if fstype ${devtype} ${devnum}:${distro_bootpart} bootfstype; then part uuid ${devtype} ${devnum}:${distro_bootpart} distro_bootpart_uuid ; run scan_dev_for_boot; fi; done; setenv devplist&lt;BR /&gt;scan_dev_for_efi=setenv efi_fdtfile ${fdtfile}; for prefix in ${efi_dtb_prefixes}; do if test -e ${devtype} ${devnum}:${distro_bootpart} ${prefix}${efi_fdtfile}; then run load_efi_dtb; fi;done;run boot_efi_bootmgr;if test -e ${devtype} ${devnum}:${distro_bootpart} efi/boot/bootaa64.efi; then echo Found EFI removable media binary efi/boot/bootaa64.efi; run boot_efi_binary; echo EFI LOAD FAILED: continuing...; fi; setenv efi_fdtfile&lt;BR /&gt;scan_dev_for_extlinux=if test -e ${devtype} ${devnum}:${distro_bootpart} ${prefix}${boot_syslinux_conf}; then echo Found ${prefix}${boot_syslinux_conf}; run boot_extlinux; echo EXTLINUX FAILED: continuing...; fi&lt;BR /&gt;scan_dev_for_scripts=for script in ${boot_scripts}; do if test -e ${devtype} ${devnum}:${distro_bootpart} ${prefix}${script}; then echo Found U-Boot script ${prefix}${script}; run boot_a_script; echo SCRIPT FAILED: continuing...; fi; done&lt;BR /&gt;scriptaddr=0x83500000&lt;BR /&gt;sd_dev=1&lt;BR /&gt;sec_boot=no&lt;BR /&gt;serial#=2134e7f964370db9&lt;BR /&gt;soc=imx9&lt;BR /&gt;soc_type=imx93&lt;BR /&gt;splashimage=0x90000000&lt;BR /&gt;sr_ir_v2_cmd=cp.b ${fdtcontroladdr} ${fdt_addr_r} 0x10000;fdt addr ${fdt_addr_r};fdt resize 0x400;fdt set /soc@0/bus@44000000/i2c@44350000/gpio@34 compatible adi,adp5585;for i in ${nodes}; do fdt rm ${i}; done&lt;BR /&gt;usb_boot=usb start; if usb dev ${devnum}; then devtype=usb; run scan_dev_for_boot_part; fi&lt;BR /&gt;vendor=freescale&lt;BR /&gt;video_link=2&lt;/P&gt;&lt;P&gt;Environment size: 7341/16380 bytes&lt;BR /&gt;u-boot=&amp;gt;&lt;/P&gt;&lt;P&gt;然后我也尝试过setenv&amp;nbsp;fdtfile imx93-11x11-evk-rm67199.dtb&lt;/P&gt;&lt;P&gt;&amp;nbsp;然后saveenv&lt;/P&gt;&lt;P&gt;仍然是不行，张工，能否看看，&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jun 2024 08:00:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1887684#M224981</guid>
      <dc:creator>5454ty</dc:creator>
      <dc:date>2024-06-14T08:00:26Z</dc:date>
    </item>
    <item>
      <title>Re: imx93,rm67199 driver not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1889076#M225096</link>
      <description>&lt;P&gt;HI,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191789"&gt;@5454ty&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;What is your BSP version？&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jun 2024 03:13:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1889076#M225096</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2024-06-18T03:13:39Z</dc:date>
    </item>
    <item>
      <title>Re: imx93,rm67199 driver not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1889128#M225104</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="5454ty_0-1718685751538.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/284564i0C596A2D26378050/image-size/medium?v=v2&amp;amp;px=400" role="button" title="5454ty_0-1718685751538.png" alt="5454ty_0-1718685751538.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;git clone &lt;A href="https://github.com/nxp-imx/linux-imx" target="_blank" rel="noopener"&gt;https://github.com/nxp-imx/linux-imx&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;我运行这个命令下载的内核&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jun 2024 04:43:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1889128#M225104</guid>
      <dc:creator>5454ty</dc:creator>
      <dc:date>2024-06-18T04:43:40Z</dc:date>
    </item>
    <item>
      <title>Re: imx93,rm67199 driver not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1889316#M225125</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191789"&gt;@5454ty&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;I have tested your issue on my site, and also add the log on the probe function, when the board boot, i can see the log output.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="pengyong_zhang_0-1718700126505.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/284616i0BB7568608DC595D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="pengyong_zhang_0-1718700126505.png" alt="pengyong_zhang_0-1718700126505.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I think you can use the latest BSP code for test, and the driver file is&amp;nbsp; "linux-imx/drivers/gpu/drm/panel/panel-raydium-rm67191.c"&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jun 2024 08:42:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1889316#M225125</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2024-06-18T08:42:48Z</dc:date>
    </item>
    <item>
      <title>Re: imx93,rm67199 driver not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1947628#M228052</link>
      <description>&lt;P&gt;老哥，我也是自己添加了屏幕，跟你报一样的错，请问是最后是怎么解决的啊？&lt;/P&gt;</description>
      <pubDate>Thu, 05 Sep 2024 01:09:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1947628#M228052</guid>
      <dc:creator>周蔷123</dc:creator>
      <dc:date>2024-09-05T01:09:50Z</dc:date>
    </item>
    <item>
      <title>Re: imx93,rm67199 driver not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1947631#M228053</link>
      <description>&lt;P&gt;发你的DTS来看看&lt;/P&gt;</description>
      <pubDate>Thu, 05 Sep 2024 01:19:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1947631#M228053</guid>
      <dc:creator>5454ty</dc:creator>
      <dc:date>2024-09-05T01:19:29Z</dc:date>
    </item>
    <item>
      <title>Re: imx93,rm67199 driver not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1947632#M228054</link>
      <description>&lt;P&gt;日志也发看看呗&lt;/P&gt;</description>
      <pubDate>Thu, 05 Sep 2024 01:19:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-rm67199-driver-not-work/m-p/1947632#M228054</guid>
      <dc:creator>5454ty</dc:creator>
      <dc:date>2024-09-05T01:19:58Z</dc:date>
    </item>
  </channel>
</rss>