<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Accessing RPMB key in Android 9 and Android 12 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-RPMB-key-in-Android-9-and-Android-12/m-p/1947156#M228026</link>
    <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;Based on the information I have, Widevine DRM is based on different TEEs depending on the Android version in NXP i.MX8MQ solution: Android 9 uses OPTEE, while Android 12 uses Trusty.&lt;/P&gt;&lt;P&gt;In our tests, we found that an RPMB key written under the "Android 9 + OPTEE" architecture fails verification when used under the "Android 12 + Trusty" architecture. After tracing the relevant code, it appears that OPTEE and Trusty use different algorithms to generate the RPMB key.&lt;/P&gt;&lt;P&gt;We would like to know whether Widevine DRM feature can work well while upgrading from "Android 9 + OPTEE" to "Android 12 + Trusty"?&lt;BR /&gt;If the differences between OPTEE and Trusty are causing Widevine DRM to malfunction after the upgrade to Android 12, is there a patch from NXP that supports Android 12 with OPTEE?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Wed, 04 Sep 2024 10:25:32 GMT</pubDate>
    <dc:creator>herman_lin</dc:creator>
    <dc:date>2024-09-04T10:25:32Z</dc:date>
    <item>
      <title>Accessing RPMB key in Android 9 and Android 12</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-RPMB-key-in-Android-9-and-Android-12/m-p/1947156#M228026</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;Based on the information I have, Widevine DRM is based on different TEEs depending on the Android version in NXP i.MX8MQ solution: Android 9 uses OPTEE, while Android 12 uses Trusty.&lt;/P&gt;&lt;P&gt;In our tests, we found that an RPMB key written under the "Android 9 + OPTEE" architecture fails verification when used under the "Android 12 + Trusty" architecture. After tracing the relevant code, it appears that OPTEE and Trusty use different algorithms to generate the RPMB key.&lt;/P&gt;&lt;P&gt;We would like to know whether Widevine DRM feature can work well while upgrading from "Android 9 + OPTEE" to "Android 12 + Trusty"?&lt;BR /&gt;If the differences between OPTEE and Trusty are causing Widevine DRM to malfunction after the upgrade to Android 12, is there a patch from NXP that supports Android 12 with OPTEE?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 04 Sep 2024 10:25:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Accessing-RPMB-key-in-Android-9-and-Android-12/m-p/1947156#M228026</guid>
      <dc:creator>herman_lin</dc:creator>
      <dc:date>2024-09-04T10:25:32Z</dc:date>
    </item>
    <item>
      <title>Re: Accessing RPMB key in Android 9 and Android 12</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-RPMB-key-in-Android-9-and-Android-12/m-p/1951213#M228268</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You have to change all "&lt;SPAN data-teams="true"&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;setUserAuthenticationRequired(true)" by "setUserAuthenticationRequired(false)"&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;Regards&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Sep 2024 15:24:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Accessing-RPMB-key-in-Android-9-and-Android-12/m-p/1951213#M228268</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-09-10T15:24:31Z</dc:date>
    </item>
    <item>
      <title>Re: Accessing RPMB key in Android 9 and Android 12</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-RPMB-key-in-Android-9-and-Android-12/m-p/1951869#M228305</link>
      <description>&lt;P&gt;Hi BIO,&lt;/P&gt;&lt;P&gt;Let's first clarify one thing: Is it possible to use Widevine DRM with an Android 12 + Trusty environment, even if the RPMB key was originally written in an Android 9 + OP-TEE environment?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 08:19:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Accessing-RPMB-key-in-Android-9-and-Android-12/m-p/1951869#M228305</guid>
      <dc:creator>herman_lin</dc:creator>
      <dc:date>2024-09-11T08:19:03Z</dc:date>
    </item>
  </channel>
</rss>