<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Help Needed: Running Custom TensorFlow Lite Model using efficientnet_lite on NPU</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Help-Needed-Running-Custom-TensorFlow-Lite-Model-using/m-p/1946350#M227981</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;It looks like the model is not compatible with Tensor flow lite that came in the eIQ of MX8Mplus, you need to create a model with the tensor flow lite 2.1v&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Tue, 03 Sep 2024 14:22:06 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-09-03T14:22:06Z</dc:date>
    <item>
      <title>Help Needed: Running Custom TensorFlow Lite Model using efficientnet_lite on NPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Help-Needed-Running-Custom-TensorFlow-Lite-Model-using/m-p/1945531#M227927</link>
      <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I’m working on deploying a custom TensorFlow Lite model on the i.MX8M Plus following the guidelines provided in the TensorFlow Lite &lt;A href="https://www.tensorflow.org/lite/models/modify/model_maker/object_detection" target="_self"&gt;Model Maker documentation&lt;/A&gt;. While the model works fine on the CPU, it fails to run on the NPU despite enabling libvx_delegate.so.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Request:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Model Compatibility&lt;/STRONG&gt;: How can I ensure my .tflite model is compatible with the i.MX8M Plus NPU?&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Configuration&lt;/STRONG&gt;: Are there specific settings needed for NPU execution?&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Troubleshooting&lt;/STRONG&gt;: What are common steps for resolving issues where a model runs on CPU but not on NPU?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I’ve attached the .tflite model and detection code for reference.&lt;/P&gt;&lt;P&gt;Thank you for your help!&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Adarsh K V&lt;/P&gt;</description>
      <pubDate>Mon, 02 Sep 2024 14:06:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Help-Needed-Running-Custom-TensorFlow-Lite-Model-using/m-p/1945531#M227927</guid>
      <dc:creator>adarshkv</dc:creator>
      <dc:date>2024-09-02T14:06:10Z</dc:date>
    </item>
    <item>
      <title>Re: Help Needed: Running Custom TensorFlow Lite Model using efficientnet_lite on NPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Help-Needed-Running-Custom-TensorFlow-Lite-Model-using/m-p/1946350#M227981</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;It looks like the model is not compatible with Tensor flow lite that came in the eIQ of MX8Mplus, you need to create a model with the tensor flow lite 2.1v&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 03 Sep 2024 14:22:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Help-Needed-Running-Custom-TensorFlow-Lite-Model-using/m-p/1946350#M227981</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-09-03T14:22:06Z</dc:date>
    </item>
  </channel>
</rss>