<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: qtpdf throws continously compile time errors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/qtpdf-throws-continously-compile-time-errors/m-p/1945276#M227901</link>
    <description>&lt;P&gt;Try to&lt;SPAN&gt;&amp;nbsp;comment out the meta-chromium layer in the bblayers.conf&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
    <pubDate>Mon, 02 Sep 2024 07:59:08 GMT</pubDate>
    <dc:creator>Harvey021</dc:creator>
    <dc:date>2024-09-02T07:59:08Z</dc:date>
    <item>
      <title>qtpdf throws continously compile time errors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/qtpdf-throws-continously-compile-time-errors/m-p/1943150#M227800</link>
      <description>&lt;P&gt;I am using the i.MX8M Plus LPDDR4 EVK. I built the i.MX, Linux LF6.6.23_2.0.0 BSP version of Yocto.&lt;/P&gt;&lt;P&gt;I built the imx-image-full and, after that, I needed the SDK for imx-image-full. So, I used the command bitbake imx-image-full -c populate_sdk.&lt;/P&gt;&lt;P&gt;However, when I ran the populate_sdk command, it threw the following error:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-- Could NOT find Gn: Found unsuitable version "2118 (811d332bd905)", but the required version is exact "6.7.0" (found /home/deevia-pc001/camera_porting/imx-yocto-bsp/build/tmp/work/armv8a-poky-linux/qtpdf/6.7.0/recipe-sysroot-native/usr/bin/gn)&lt;/P&gt;&lt;P&gt;nxp forum link :link:&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Encounter-error-when-bitbake-qtwebengine-cconfigure-in-imx8-bsp/m-p/1490894?profile.language=en" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Encounter-error-when-bitbake-qtwebengine-cconfigure-in-imx8-bsp/m-p/1490894?profile.language=en&lt;/A&gt;&lt;/P&gt;&lt;P&gt;In one of the forums on NXP, they suggested adding the following line to local.conf:&lt;/P&gt;&lt;P&gt;BBMASK += "/meta-browser/meta-chromium/recipes-browser/chromium/gn-native_.*\.bb"&lt;/P&gt;&lt;P&gt;I added that line to the local.conf file. However, when I ran populate_sdk again, it threw a qtpdf compile error. I have attached logs of&amp;nbsp; errors. Can anyone help me resolve this issue?&lt;/P&gt;&lt;P&gt;thanks&amp;amp;Regards&lt;/P&gt;&lt;P&gt;srinivas&lt;/P&gt;</description>
      <pubDate>Thu, 29 Aug 2024 07:08:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/qtpdf-throws-continously-compile-time-errors/m-p/1943150#M227800</guid>
      <dc:creator>srinivas_123</dc:creator>
      <dc:date>2024-08-29T07:08:10Z</dc:date>
    </item>
    <item>
      <title>Re: qtpdf throws continously compile time errors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/qtpdf-throws-continously-compile-time-errors/m-p/1945276#M227901</link>
      <description>&lt;P&gt;Try to&lt;SPAN&gt;&amp;nbsp;comment out the meta-chromium layer in the bblayers.conf&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Mon, 02 Sep 2024 07:59:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/qtpdf-throws-continously-compile-time-errors/m-p/1945276#M227901</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-09-02T07:59:08Z</dc:date>
    </item>
  </channel>
</rss>