<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: V4L2 error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/V4L2-error/m-p/1945164#M227893</link>
    <description>Hi@pengyong_zhang&lt;BR /&gt;yes ,is there any specific reason for showing like this. am i missed any configurations.&lt;BR /&gt;Thanks&amp;amp;Regards&lt;BR /&gt;srinivas</description>
    <pubDate>Mon, 02 Sep 2024 06:24:08 GMT</pubDate>
    <dc:creator>srinivas_123</dc:creator>
    <dc:date>2024-09-02T06:24:08Z</dc:date>
    <item>
      <title>V4L2 error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/V4L2-error/m-p/1916024#M226557</link>
      <description>&lt;P&gt;I am using an i.MX 8M Plus custom board and have connected an OV5640 camera to it. After building the imx-image-full image and booting it on the custom board, I confirm the camera's presence using the command v4l2-ctl --list-devices. However, sometimes the camera does not appear when I run this command. Does anyone know why this is happening? Are there any modifications needed?&lt;/P&gt;&lt;P&gt;root@imx8mp-lpddr4-evk:/usr/bin/application# v4l2-ctl --list-devices&lt;BR /&gt;mxc-isi-m2m_v1 (platform:32e00000.isi:m2m_devic):&lt;BR /&gt;/dev/video2&lt;/P&gt;&lt;P&gt;vsi_v4l2dec (platform:vsi_v4l2dec):&lt;BR /&gt;/dev/video1&lt;/P&gt;&lt;P&gt;vsi_v4l2enc (platform:vsi_v4l2enc):&lt;BR /&gt;/dev/video0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;root@imx8mp-lpddr4-evk:/usr/bin/application# v4l2-ctl --list-devices&lt;BR /&gt;():&lt;BR /&gt;/dev/v4l-subdev0&lt;/P&gt;&lt;P&gt;FSL Capture Media Device (platform:32c00000.bus:camera):&lt;BR /&gt;/dev/media0&lt;/P&gt;&lt;P&gt;mxc-isi-cap_v1 (platform:32e00000.isi:cap_devic):&lt;BR /&gt;/dev/video3&lt;/P&gt;&lt;P&gt;mxc-isi-m2m_v1 (platform:32e00000.isi:m2m_devic):&lt;BR /&gt;/dev/video2&lt;/P&gt;&lt;P&gt;vsi_v4l2dec (platform:vsi_v4l2dec):&lt;BR /&gt;/dev/video1&lt;/P&gt;&lt;P&gt;vsi_v4l2enc (platform:vsi_v4l2enc):&lt;BR /&gt;/dev/video0&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;srinivas&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jul 2024 09:39:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/V4L2-error/m-p/1916024#M226557</guid>
      <dc:creator>srinivas_123</dc:creator>
      <dc:date>2024-07-24T09:39:37Z</dc:date>
    </item>
    <item>
      <title>Re: V4L2 error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/V4L2-error/m-p/1916897#M226588</link>
      <description>&lt;P&gt;hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231093"&gt;@srinivas_123&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sometimes you can see the camera device but sometimes can't,right?&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jul 2024 06:41:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/V4L2-error/m-p/1916897#M226588</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2024-07-25T06:41:29Z</dc:date>
    </item>
    <item>
      <title>Re: V4L2 error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/V4L2-error/m-p/1945164#M227893</link>
      <description>Hi@pengyong_zhang&lt;BR /&gt;yes ,is there any specific reason for showing like this. am i missed any configurations.&lt;BR /&gt;Thanks&amp;amp;Regards&lt;BR /&gt;srinivas</description>
      <pubDate>Mon, 02 Sep 2024 06:24:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/V4L2-error/m-p/1945164#M227893</guid>
      <dc:creator>srinivas_123</dc:creator>
      <dc:date>2024-09-02T06:24:08Z</dc:date>
    </item>
  </channel>
</rss>