<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic end Kernel panic - not syncing: Oops: Fatal exception in interrupt in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/end-Kernel-panic-not-syncing-Oops-Fatal-exception-in-interrupt/m-p/1945097#M227886</link>
    <description>&lt;P&gt;hello&lt;/P&gt;&lt;P&gt;We are using the IMX8MP core and encountered the following error while continuously recording DP video. I would like to inquire about the cause of the problem or the direction of the investigation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;[93531.847359] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000000&lt;BR /&gt;[93531.856193] Mem abort info:&lt;BR /&gt;[93531.858988] ESR = 0x96000004&lt;BR /&gt;[93531.862044] EC = 0x25: DABT (current EL), IL = 32 bits&lt;BR /&gt;[93531.867355] SET = 0, FnV = 0&lt;BR /&gt;[93531.870409] EA = 0, S1PTW = 0&lt;BR /&gt;[93531.873547] Data abort info:&lt;BR /&gt;[93531.876426] ISV = 0, ISS = 0x00000004&lt;BR /&gt;[93531.880260] CM = 0, WnR = 0&lt;BR /&gt;[93531.883230] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000048bf9000&lt;BR /&gt;[93531.889669] [0000000000000000] pgd=0000000000000000, p4d=0000000000000000&lt;BR /&gt;[93531.896464] Internal error: Oops: 96000004 [#1] PREEMPT SMP&lt;BR /&gt;[93531.902036] Modules linked in: tiger_ledctr(O) crct10dif_ce imx8_media_dev(C) flexcan can_dev&lt;BR /&gt;[93531.910584] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G WC O 5.10.9-1.0.0+g68232600d8b7 #194&lt;BR /&gt;[93531.919801] Hardware name: MYIR i.MX8MP BASE (DT)&lt;BR /&gt;[93531.924506] pstate: 60000085 (nZCv daIf -PAN -UAO -TCO BTYPE=--)&lt;BR /&gt;[93531.930524] pc : mxc_isi_channel_set_outbuf+0x194/0x200&lt;BR /&gt;[93531.935751] lr : mxc_isi_channel_set_outbuf+0x18c/0x200&lt;BR /&gt;[93531.940974] sp : ffff800011cabe20&lt;BR /&gt;[93531.944287] x29: ffff800011cabe20 x28: ffff800011ab2340&lt;BR /&gt;[93531.949602] x27: 0000000000000000 x26: ffff800011575ff8&lt;BR /&gt;[93531.954916] x25: ffff0000057a7738 x24: ffff0000057a7748&lt;BR /&gt;[93531.960231] x23: ffff000004430810 x22: 0000000000000008&lt;BR /&gt;[93531.965545] x21: ffff0000057a7768 x20: ffff000005788680&lt;BR /&gt;[93531.970859] x19: ffff0000057a73b0 x18: 0000000000000000&lt;BR /&gt;[93531.976172] x17: 0000000000000000 x16: 0000000000000000&lt;BR /&gt;[93531.981486] x15: 00006d54d4246770 x14: 000000000000013f&lt;BR /&gt;[93531.986800] x13: 0000000000000001 x12: 0000000000000040&lt;BR /&gt;[93531.992115] x11: ffff00000606eb58 x10: ffff00000606eb5a&lt;BR /&gt;[93531.997431] x9 : ffff800011b31700 x8 : ffff000006000270&lt;BR /&gt;[93532.002745] x7 : 0000000000000000 x6 : ffff000006000400&lt;BR /&gt;[93532.008059] x5 : ffff000006000248 x4 : 00000000000016c8&lt;BR /&gt;[93532.013373] x3 : ffff0000057a6f88 x2 : ffff0000057a73b0&lt;BR /&gt;[93532.018686] x1 : 0000000000000000 x0 : 0000000000000000&lt;BR /&gt;[93532.024000] Call trace:&lt;BR /&gt;[93532.026450] mxc_isi_channel_set_outbuf+0x194/0x200&lt;BR /&gt;[93532.031331] mxc_isi_cap_frame_write_done+0xf0/0x1fc&lt;BR /&gt;[93532.036296] mxc_isi_irq_handler+0x84/0x90&lt;BR /&gt;[93532.040396] __handle_irq_event_percpu+0x54/0x170&lt;BR /&gt;[93532.045100] handle_irq_event+0x68/0x150&lt;BR /&gt;[93532.049024] handle_fasteoi_irq+0xa4/0x1f4&lt;BR /&gt;[93532.053122] __handle_domain_irq+0x7c/0xe0&lt;BR /&gt;[93532.057221] gic_handle_irq+0xc0/0x140&lt;BR /&gt;[93532.060972] el1_irq+0xc4/0x180&lt;BR /&gt;[93532.064118] cpuidle_enter_state+0x12c/0x2f0&lt;BR /&gt;[93532.068388] cpuidle_enter+0x38/0x50&lt;BR /&gt;[93532.071967] do_idle+0x218/0x2a0&lt;BR /&gt;[93532.075196] cpu_startup_entry+0x28/0x70&lt;BR /&gt;[93532.079121] rest_init+0xd8/0xe8&lt;BR /&gt;[93532.082353] arch_call_rest_init+0x10/0x1c&lt;BR /&gt;[93532.086450] start_kernel+0x4bc/0x4f4&lt;BR /&gt;[93532.090117] Code: aa1303e0 97fcc3ae 910ee275 b9401661 (f9400000)&lt;BR /&gt;[93532.096213] ---[ end trace 425f6fdbc9117ec8 ]---&lt;BR /&gt;[93532.100832] Kernel panic - not syncing: Oops: Fatal exception in interrupt&lt;BR /&gt;[93532.107706] SMP: stopping secondary CPUs&lt;BR /&gt;[93532.111935] Kernel Offset: disabled&lt;BR /&gt;[93532.115424] CPU features: 0x0240002,2000200c&lt;BR /&gt;[93532.119691] Memory Limit: none&lt;BR /&gt;[93532.122754] ---[ end Kernel panic - not syncing: Oops: Fatal exception in interrupt ]---&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 02 Sep 2024 04:10:35 GMT</pubDate>
    <dc:creator>FanS2023</dc:creator>
    <dc:date>2024-09-02T04:10:35Z</dc:date>
    <item>
      <title>end Kernel panic - not syncing: Oops: Fatal exception in interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/end-Kernel-panic-not-syncing-Oops-Fatal-exception-in-interrupt/m-p/1945097#M227886</link>
      <description>&lt;P&gt;hello&lt;/P&gt;&lt;P&gt;We are using the IMX8MP core and encountered the following error while continuously recording DP video. I would like to inquire about the cause of the problem or the direction of the investigation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;[93531.847359] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000000&lt;BR /&gt;[93531.856193] Mem abort info:&lt;BR /&gt;[93531.858988] ESR = 0x96000004&lt;BR /&gt;[93531.862044] EC = 0x25: DABT (current EL), IL = 32 bits&lt;BR /&gt;[93531.867355] SET = 0, FnV = 0&lt;BR /&gt;[93531.870409] EA = 0, S1PTW = 0&lt;BR /&gt;[93531.873547] Data abort info:&lt;BR /&gt;[93531.876426] ISV = 0, ISS = 0x00000004&lt;BR /&gt;[93531.880260] CM = 0, WnR = 0&lt;BR /&gt;[93531.883230] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000048bf9000&lt;BR /&gt;[93531.889669] [0000000000000000] pgd=0000000000000000, p4d=0000000000000000&lt;BR /&gt;[93531.896464] Internal error: Oops: 96000004 [#1] PREEMPT SMP&lt;BR /&gt;[93531.902036] Modules linked in: tiger_ledctr(O) crct10dif_ce imx8_media_dev(C) flexcan can_dev&lt;BR /&gt;[93531.910584] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G WC O 5.10.9-1.0.0+g68232600d8b7 #194&lt;BR /&gt;[93531.919801] Hardware name: MYIR i.MX8MP BASE (DT)&lt;BR /&gt;[93531.924506] pstate: 60000085 (nZCv daIf -PAN -UAO -TCO BTYPE=--)&lt;BR /&gt;[93531.930524] pc : mxc_isi_channel_set_outbuf+0x194/0x200&lt;BR /&gt;[93531.935751] lr : mxc_isi_channel_set_outbuf+0x18c/0x200&lt;BR /&gt;[93531.940974] sp : ffff800011cabe20&lt;BR /&gt;[93531.944287] x29: ffff800011cabe20 x28: ffff800011ab2340&lt;BR /&gt;[93531.949602] x27: 0000000000000000 x26: ffff800011575ff8&lt;BR /&gt;[93531.954916] x25: ffff0000057a7738 x24: ffff0000057a7748&lt;BR /&gt;[93531.960231] x23: ffff000004430810 x22: 0000000000000008&lt;BR /&gt;[93531.965545] x21: ffff0000057a7768 x20: ffff000005788680&lt;BR /&gt;[93531.970859] x19: ffff0000057a73b0 x18: 0000000000000000&lt;BR /&gt;[93531.976172] x17: 0000000000000000 x16: 0000000000000000&lt;BR /&gt;[93531.981486] x15: 00006d54d4246770 x14: 000000000000013f&lt;BR /&gt;[93531.986800] x13: 0000000000000001 x12: 0000000000000040&lt;BR /&gt;[93531.992115] x11: ffff00000606eb58 x10: ffff00000606eb5a&lt;BR /&gt;[93531.997431] x9 : ffff800011b31700 x8 : ffff000006000270&lt;BR /&gt;[93532.002745] x7 : 0000000000000000 x6 : ffff000006000400&lt;BR /&gt;[93532.008059] x5 : ffff000006000248 x4 : 00000000000016c8&lt;BR /&gt;[93532.013373] x3 : ffff0000057a6f88 x2 : ffff0000057a73b0&lt;BR /&gt;[93532.018686] x1 : 0000000000000000 x0 : 0000000000000000&lt;BR /&gt;[93532.024000] Call trace:&lt;BR /&gt;[93532.026450] mxc_isi_channel_set_outbuf+0x194/0x200&lt;BR /&gt;[93532.031331] mxc_isi_cap_frame_write_done+0xf0/0x1fc&lt;BR /&gt;[93532.036296] mxc_isi_irq_handler+0x84/0x90&lt;BR /&gt;[93532.040396] __handle_irq_event_percpu+0x54/0x170&lt;BR /&gt;[93532.045100] handle_irq_event+0x68/0x150&lt;BR /&gt;[93532.049024] handle_fasteoi_irq+0xa4/0x1f4&lt;BR /&gt;[93532.053122] __handle_domain_irq+0x7c/0xe0&lt;BR /&gt;[93532.057221] gic_handle_irq+0xc0/0x140&lt;BR /&gt;[93532.060972] el1_irq+0xc4/0x180&lt;BR /&gt;[93532.064118] cpuidle_enter_state+0x12c/0x2f0&lt;BR /&gt;[93532.068388] cpuidle_enter+0x38/0x50&lt;BR /&gt;[93532.071967] do_idle+0x218/0x2a0&lt;BR /&gt;[93532.075196] cpu_startup_entry+0x28/0x70&lt;BR /&gt;[93532.079121] rest_init+0xd8/0xe8&lt;BR /&gt;[93532.082353] arch_call_rest_init+0x10/0x1c&lt;BR /&gt;[93532.086450] start_kernel+0x4bc/0x4f4&lt;BR /&gt;[93532.090117] Code: aa1303e0 97fcc3ae 910ee275 b9401661 (f9400000)&lt;BR /&gt;[93532.096213] ---[ end trace 425f6fdbc9117ec8 ]---&lt;BR /&gt;[93532.100832] Kernel panic - not syncing: Oops: Fatal exception in interrupt&lt;BR /&gt;[93532.107706] SMP: stopping secondary CPUs&lt;BR /&gt;[93532.111935] Kernel Offset: disabled&lt;BR /&gt;[93532.115424] CPU features: 0x0240002,2000200c&lt;BR /&gt;[93532.119691] Memory Limit: none&lt;BR /&gt;[93532.122754] ---[ end Kernel panic - not syncing: Oops: Fatal exception in interrupt ]---&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Sep 2024 04:10:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/end-Kernel-panic-not-syncing-Oops-Fatal-exception-in-interrupt/m-p/1945097#M227886</guid>
      <dc:creator>FanS2023</dc:creator>
      <dc:date>2024-09-02T04:10:35Z</dc:date>
    </item>
    <item>
      <title>Re: end Kernel panic - not syncing: Oops: Fatal exception in interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/end-Kernel-panic-not-syncing-Oops-Fatal-exception-in-interrupt/m-p/1945741#M227943</link>
      <description>&lt;P&gt;Hi &lt;/P&gt;
&lt;P&gt;Referring the crash log, the buffer address used in&amp;nbsp;&lt;SPAN&gt;mxc_isi_channel_set_outbuf is NULL. Which version you are using? Can you try it with latest kernel?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Tue, 03 Sep 2024 01:37:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/end-Kernel-panic-not-syncing-Oops-Fatal-exception-in-interrupt/m-p/1945741#M227943</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-09-03T01:37:56Z</dc:date>
    </item>
    <item>
      <title>Re: end Kernel panic - not syncing: Oops: Fatal exception in interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/end-Kernel-panic-not-syncing-Oops-Fatal-exception-in-interrupt/m-p/1945795#M227947</link>
      <description>你好&lt;BR /&gt;&lt;BR /&gt;内核版本为5.10.9-1.0.0+g68232600d8b7，可以尝试升级。但&lt;BR /&gt;内核崩溃并不会每次都发生，更换最新内核即使没发生，也不确认是否真的解决问题。&lt;BR /&gt;很疑惑为什么发生the buffer address used in mxc_isi_channel_set_outbuf is NULL，与我多次操作isi chanel有关系么？&lt;BR /&gt;</description>
      <pubDate>Tue, 03 Sep 2024 02:42:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/end-Kernel-panic-not-syncing-Oops-Fatal-exception-in-interrupt/m-p/1945795#M227947</guid>
      <dc:creator>FanS2023</dc:creator>
      <dc:date>2024-09-03T02:42:27Z</dc:date>
    </item>
    <item>
      <title>Re: end Kernel panic - not syncing: Oops: Fatal exception in interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/end-Kernel-panic-not-syncing-Oops-Fatal-exception-in-interrupt/m-p/1946749#M227996</link>
      <description>&lt;P&gt;可能是这个版本的驱动问题，也可能是操作问题，你先试试升级内核。&lt;/P&gt;</description>
      <pubDate>Wed, 04 Sep 2024 02:07:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/end-Kernel-panic-not-syncing-Oops-Fatal-exception-in-interrupt/m-p/1946749#M227996</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-09-04T02:07:07Z</dc:date>
    </item>
  </channel>
</rss>