<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using I.MX8QuadMax for deep learning in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-I-MX8QuadMax-for-deep-learning/m-p/1945002#M227885</link>
    <description>&lt;P&gt;There is no in-built WiFi, interface&amp;nbsp;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;M.2 KEY E available though.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
    <pubDate>Mon, 02 Sep 2024 02:34:01 GMT</pubDate>
    <dc:creator>Harvey021</dc:creator>
    <dc:date>2024-09-02T02:34:01Z</dc:date>
    <item>
      <title>Using I.MX8QuadMax for deep learning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-I-MX8QuadMax-for-deep-learning/m-p/1943112#M227797</link>
      <description>&lt;P&gt;I want to install Tensorflow and other required libraries like mediapipe, opencv and tensorflow hub in I.MX8QuadMax for a deep learning based application which utilizes camera. How can i install my these requirements easily on the linux image of I.MX8QuadMax.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Aug 2024 06:40:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-I-MX8QuadMax-for-deep-learning/m-p/1943112#M227797</guid>
      <dc:creator>Param21</dc:creator>
      <dc:date>2024-08-29T06:40:03Z</dc:date>
    </item>
    <item>
      <title>Re: Using I.MX8QuadMax for deep learning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-I-MX8QuadMax-for-deep-learning/m-p/1944030#M227834</link>
      <description>&lt;P&gt;OpenCV, Tensorflow lite should be already integrated with BSP, and you can pip install for mediapipe.&lt;/P&gt;
&lt;P&gt;More details, please refer to&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX-MACHINE-LEARNING-UG.pdf" target="_self"&gt;IMX-MACHINE-LEARNING-UG.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Fri, 30 Aug 2024 04:07:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-I-MX8QuadMax-for-deep-learning/m-p/1944030#M227834</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-08-30T04:07:05Z</dc:date>
    </item>
    <item>
      <title>Re: Using I.MX8QuadMax for deep learning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-I-MX8QuadMax-for-deep-learning/m-p/1944108#M227839</link>
      <description>&lt;P&gt;Thank you so much for your response and can you please answer the following questions:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;which version of linux image to be downloaded from the NXP website which includes all these libraries and it is ready to use for the application for I.MX8QuadMax?&lt;/P&gt;&lt;P&gt;How to include tensorflow Hub since my project uses tensorflow hub APIs as well?&lt;/P&gt;&lt;P&gt;Does I.MX8QuadMax kit comes with inbuilt Wi-Fi support?&lt;/P&gt;</description>
      <pubDate>Fri, 30 Aug 2024 05:13:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-I-MX8QuadMax-for-deep-learning/m-p/1944108#M227839</guid>
      <dc:creator>Param21</dc:creator>
      <dc:date>2024-08-30T05:13:19Z</dc:date>
    </item>
    <item>
      <title>Re: Using I.MX8QuadMax for deep learning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-I-MX8QuadMax-for-deep-learning/m-p/1944113#M227840</link>
      <description>which version of linux image to be downloaded from the NXP website which includes all these libraries and it is ready to use for the application for I.MX8QuadMax?&lt;BR /&gt;this query is solved. please reply for the remaining two questions.</description>
      <pubDate>Fri, 30 Aug 2024 05:20:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-I-MX8QuadMax-for-deep-learning/m-p/1944113#M227840</guid>
      <dc:creator>Param21</dc:creator>
      <dc:date>2024-08-30T05:20:25Z</dc:date>
    </item>
    <item>
      <title>Re: Using I.MX8QuadMax for deep learning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-I-MX8QuadMax-for-deep-learning/m-p/1945002#M227885</link>
      <description>&lt;P&gt;There is no in-built WiFi, interface&amp;nbsp;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;M.2 KEY E available though.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Mon, 02 Sep 2024 02:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-I-MX8QuadMax-for-deep-learning/m-p/1945002#M227885</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-09-02T02:34:01Z</dc:date>
    </item>
  </channel>
</rss>