<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX 8M Mini: USBx_VBUS pin functions when used as a USB host in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-USBx-VBUS-pin-functions-when-used-as-a-USB-host/m-p/1943039#M227791</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on a board design with i.MX 8M Mini and want to use it as a fixed USB host.&lt;BR /&gt;In this case, what function does the USBx_VBUS pin have?&lt;BR /&gt;I want to understand the USBx_VBUS pin when using a USB host and design it appropriately.&lt;/P&gt;</description>
    <pubDate>Thu, 29 Aug 2024 04:48:03 GMT</pubDate>
    <dc:creator>Y_Kanda</dc:creator>
    <dc:date>2024-08-29T04:48:03Z</dc:date>
    <item>
      <title>i.MX 8M Mini: USBx_VBUS pin functions when used as a USB host</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-USBx-VBUS-pin-functions-when-used-as-a-USB-host/m-p/1943039#M227791</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on a board design with i.MX 8M Mini and want to use it as a fixed USB host.&lt;BR /&gt;In this case, what function does the USBx_VBUS pin have?&lt;BR /&gt;I want to understand the USBx_VBUS pin when using a USB host and design it appropriately.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Aug 2024 04:48:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-USBx-VBUS-pin-functions-when-used-as-a-USB-host/m-p/1943039#M227791</guid>
      <dc:creator>Y_Kanda</dc:creator>
      <dc:date>2024-08-29T04:48:03Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini: USBx_VBUS pin functions when used as a USB host</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-USBx-VBUS-pin-functions-when-used-as-a-USB-host/m-p/1945881#M227953</link>
      <description>&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;USB_VBUS1 pin is used to detect USB device, it can't be used 5V directly. The usage is &amp;nbsp;: &amp;nbsp;(1) 5V--&amp;gt;Series 1k -- series 30k---&amp;gt;USB_VBUS1 &amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Sep 2024 04:44:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-USBx-VBUS-pin-functions-when-used-as-a-USB-host/m-p/1945881#M227953</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2024-09-03T04:44:37Z</dc:date>
    </item>
  </channel>
</rss>