<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8 watchdog timer in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-watchdog-timer/m-p/1941494#M227731</link>
    <description>Thank you. I'm using a TQMa8MPxL. The kernel configuration menu options for the Watchdog Timer Support include "IMX2+ Watchdog" and "IMX7ULP Watchdog" but the option for "IMX8 Watchdog" is not available. I'm guessing I might be working with an older version of the kernel where that particular config wasn't available. Does that seem a likely explanation. Is "IMX8 Watchdog" an option that is critical to using WDOG1 from the A53 and WDOG3 from the M7?</description>
    <pubDate>Tue, 27 Aug 2024 18:33:50 GMT</pubDate>
    <dc:creator>kturner</dc:creator>
    <dc:date>2024-08-27T18:33:50Z</dc:date>
    <item>
      <title>IMX8 watchdog timer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-watchdog-timer/m-p/1940661#M227690</link>
      <description>&lt;P&gt;&lt;STRONG&gt;I've successfully executed the demo evkmimx8mp_wdog01.&amp;nbsp; The readme.md states "Please note this application can't support running with Linux BSP!".&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Can you explain why the application on the M7 cannot run with Linux running on the A53?&amp;nbsp; Can the constraint be removed so that I can use WDOG1 through systemd on the Linux A53 and use WDOG3 on the M7 with an application started through remoteproc facility?&lt;/STRONG&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Aug 2024 20:25:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-watchdog-timer/m-p/1940661#M227690</guid>
      <dc:creator>kturner</dc:creator>
      <dc:date>2024-08-26T20:25:09Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8 watchdog timer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-watchdog-timer/m-p/1941364#M227724</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can check:&lt;/P&gt;
&lt;P&gt;For enabling wdog in linux one can refer to sect.2.11.7 Menu Configuration Options i.Mx linux reference manual&lt;A style="box-sizing: border-box; background-color: transparent; color: #215bd6; text-decoration: none; cursor: pointer;" href="https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf" target="_blank" rel="noopener nofollow noreferrer"&gt;​&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;regarding uboot, wdog can be configured in scfw codes (board.c file)&amp;nbsp; SCFW porting&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 27 Aug 2024 14:32:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-watchdog-timer/m-p/1941364#M227724</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-08-27T14:32:42Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8 watchdog timer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-watchdog-timer/m-p/1941494#M227731</link>
      <description>Thank you. I'm using a TQMa8MPxL. The kernel configuration menu options for the Watchdog Timer Support include "IMX2+ Watchdog" and "IMX7ULP Watchdog" but the option for "IMX8 Watchdog" is not available. I'm guessing I might be working with an older version of the kernel where that particular config wasn't available. Does that seem a likely explanation. Is "IMX8 Watchdog" an option that is critical to using WDOG1 from the A53 and WDOG3 from the M7?</description>
      <pubDate>Tue, 27 Aug 2024 18:33:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-watchdog-timer/m-p/1941494#M227731</guid>
      <dc:creator>kturner</dc:creator>
      <dc:date>2024-08-27T18:33:50Z</dc:date>
    </item>
  </channel>
</rss>